Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
SAM4C/4E/V71/V70/S70/E70 Advanced Encryption Standard (AES) Driver

This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Advanced Encryption Standard functionality.

The Advanced Encryption Standard module supports all five confidentiality modes of operation for symmetrical key block cipher algorithms (as specified in the NIST Special Publication 800-38A Recommendation):

Devices from the following series can use this module:

The outline of this documentation is as follows:

Prerequisites

There are no prerequisites for this module.

Module Overview

The Advanced Encryption Standard (AES) module is compliant with the American FIPS (Federal Information Processing Standard) Publication 197 specification.

The AES supports all five confidentiality modes of operation for symmetrical key block cipher algorithms (as specified in the NIST Special Publication 800-38A Recommendation) :

Data transfers both to and from the AES module can occur using the Peripheral DMA Controller (PDC) channels (thus minimizing processor intervention for large data buffer transfers).

As soon as the initialization vector, the input data, and the key are configured, the encryption/decryption process may be started. Once the process has completed the encrypted/decrypted data can be read out via registers or through DMA channels.

Special Considerations

Power Management

The AES module may be clocked through the Power Management Controller (PMC), in which case the user application must first configure the PMC to enable the AES clock.

Interrupt

When using the AES module's interrupt, the configuration of the device's Nested Vectored Interrupt Controller (NVIC) needs to be carried out before the AES module is configured.

Extra Information

For extra information, see Extra Information for Advanced Encryption Standard. This includes:

Examples

For a list of examples related to this driver, see Examples for Advanced Encryption Standard.

API Overview

Modules

 
 Quick Start Guide(s)
 In this section you can find a list of all Quick Start guides related to the SAM4C/4E/V71/V70/S70/E70 Advanced Encryption Standard (AES) Driver.
 

Data Structures

struct  aes_config
 AES Configuration structure. More...
 

Macros

#define AES_DMA_RX_IDX   12
 AES DMAC RX channel interface number. More...
 
#define AES_DMA_TX_IDX   11
 AES DMAC TX channel interface number. More...
 

Typedefs

typedef void(* aes_callback_t )(void)
 AES interrupt callback function type. More...
 
typedef enum aes_interrupt_source aes_interrupt_source_t
 AES interrupt source type. More...
 

Enumerations

enum  aes_cfb_size {
  AES_CFB_SIZE_128 = 0,
  AES_CFB_SIZE_64,
  AES_CFB_SIZE_32,
  AES_CFB_SIZE_16,
  AES_CFB_SIZE_8
}
 AES Cipher FeedBack (CFB) size. More...
 
enum  aes_encrypt_mode {
  AES_DECRYPTION = 0,
  AES_ENCRYPTION
}
 AES processing mode. More...
 
enum  aes_interrupt_source {
  AES_INTERRUPT_DATA_READY = AES_IER_DATRDY,
  AES_INTERRUPT_UNSPECIFIED_REGISTER_ACCESS = AES_IER_URAD,
  AES_INTERRUPT_END_OF_RECEIVE_BUFFER = AES_IER_ENDRX,
  AES_INTERRUPT_END_OF_TRANSMIT_BUFFER = AES_IER_ENDTX,
  AES_INTERRUPT_RECEIVE_BUFFER_FULL = AES_IER_RXBUFF,
  AES_INTERRUPT_TRANSMIT_BUFFER_FULL = AES_IER_TXBUFE
}
 AES interrupt source type. More...
 
enum  aes_key_size {
  AES_KEY_SIZE_128 = 0,
  AES_KEY_SIZE_192,
  AES_KEY_SIZE_256
}
 AES cryptographic key size. More...
 
enum  aes_opmode {
  AES_ECB_MODE = 0,
  AES_CBC_MODE,
  AES_OFB_MODE,
  AES_CFB_MODE,
  AES_CTR_MODE,
  AES_GCM_MODE
}
 AES cipher block mode. More...
 
enum  aes_start_mode {
  AES_MANUAL_START = 0,
  AES_AUTO_START,
  AES_IDATAR0_START
}
 AES start mode. More...
 

Functions

void aes_disable (void)
 Disable the AES module. More...
 
static void aes_disable_interrupt (Aes *const p_aes, aes_interrupt_source_t source)
 Disable an AES interrupt. More...
 
void aes_enable (void)
 Enable the AES module. More...
 
static void aes_enable_interrupt (Aes *const p_aes, aes_interrupt_source_t source)
 Enable an AES interrupt. More...
 
void aes_get_config_defaults (struct aes_config *const p_cfg)
 Initializes an AES configuration structure to defaults. More...
 
Pdc * aes_get_pdc_base (Aes *p_aes)
 Get AES PDC base address. More...
 
void aes_init (Aes *const p_aes, struct aes_config *const p_cfg)
 Initialize the AES module. More...
 
static uint32_t aes_read_authen_datalength (Aes *const p_aes)
 Get the AES Additional Authenticated Data (AAD) length in bytes. More...
 
static uint32_t aes_read_gcm_counter (Aes *const p_aes)
 Get the AES GCM Encryption Counter. More...
 
static uint32_t aes_read_gcmh (Aes *const p_aes, uint32_t id)
 Get AES GCM Hash subkey word. More...
 
static uint32_t aes_read_ghash (Aes *const p_aes, uint32_t id)
 Get the AES GCM Intermediate Hash Word. More...
 
static uint32_t aes_read_interrupt_mask (Aes *const p_aes)
 Get the AES interrupt mask status. More...
 
static uint32_t aes_read_interrupt_status (Aes *const p_aes)
 Get the AES interrupt status. More...
 
void aes_read_output_data (Aes *const p_aes, uint32_t *p_output_data_buffer)
 Read the output data. More...
 
static uint32_t aes_read_pctext_length (Aes *const p_aes)
 Get the AES plaintext/ciphertext length in bytes. More...
 
static uint32_t aes_read_tag (Aes *const p_aes, uint32_t id)
 Get AES GCM Authentication Tag Word. More...
 
static void aes_reset (Aes *const p_aes)
 Perform an AES software reset. More...
 
void aes_set_callback (Aes *const p_aes, aes_interrupt_source_t source, aes_callback_t callback, uint8_t irq_level)
 Set the AES interrupt callback. More...
 
void aes_set_config (Aes *const p_aes, struct aes_config *const p_cfg)
 Configure the AES module. More...
 
static void aes_start (Aes *const p_aes)
 Start a manual encryption/decryption process. More...
 
static void aes_write_authen_datalength (Aes *const p_aes, uint32_t length)
 Set the AES Additional Authenticated Data (AAD) length in bytes. More...
 
static void aes_write_gcmh (Aes *const p_aes, uint32_t id, uint32_t hword)
 Set the AES GCM Hash subkey word. More...
 
static void aes_write_ghash (Aes *const p_aes, uint32_t id, uint32_t ghash)
 Set the AES GCM Intermediate Hash Word. More...
 
void aes_write_initvector (Aes *const p_aes, const uint32_t *p_vector)
 Write the initialization vector (for the CBC, CFB, OFB, CTR & GCM cipher modes). More...
 
void aes_write_input_data (Aes *const p_aes, const uint32_t *p_input_data_buffer)
 Write the input data (four consecutive 32-bit words). More...
 
void aes_write_key (Aes *const p_aes, const uint32_t *p_key)
 Write the 128/192/256-bit cryptographic key. More...
 
static void aes_write_pctext_length (Aes *const p_aes, uint32_t length)
 Set the AES plaintext/ciphertext length in bytes. More...
 

#define AES_DMA_RX_IDX   12

AES DMAC RX channel interface number.

#define AES_DMA_TX_IDX   11

AES DMAC TX channel interface number.

typedef void(* aes_callback_t)(void)

AES interrupt callback function type.

AES interrupt source type.

AES Cipher FeedBack (CFB) size.

Enumerator
AES_CFB_SIZE_128 

Cipher feedback data size is 128-bit.

AES_CFB_SIZE_64 

Cipher feedback data size is 64-bit.

AES_CFB_SIZE_32 

Cipher feedback data size is 32-bit.

AES_CFB_SIZE_16 

Cipher feedback data size is 16-bit.

AES_CFB_SIZE_8 

Cipher feedback data size is 8-bit.

AES processing mode.

Enumerator
AES_DECRYPTION 

Decryption of data will be performed.

AES_ENCRYPTION 

Encryption of data will be performed.

AES interrupt source type.

Enumerator
AES_INTERRUPT_DATA_READY 

Data ready interrupt.

AES_INTERRUPT_UNSPECIFIED_REGISTER_ACCESS 

Unspecified register access detection interrupt.

AES_INTERRUPT_END_OF_RECEIVE_BUFFER 

End of receive buffer interrupt (SAM4C devices only).

AES_INTERRUPT_END_OF_TRANSMIT_BUFFER 

End of transmit buffer interrupt (SAM4C devices only).

AES_INTERRUPT_RECEIVE_BUFFER_FULL 

Receive buffer full interrupt (SAM4C devices only).

AES_INTERRUPT_TRANSMIT_BUFFER_FULL 

Transmit buffer empty interrupt (SAM4C devices only).

AES cryptographic key size.

Enumerator
AES_KEY_SIZE_128 

AES key size is 128 bits.

AES_KEY_SIZE_192 

AES key size is 192 bits.

AES_KEY_SIZE_256 

AES key size is 256 bits.

enum aes_opmode

AES cipher block mode.

Enumerator
AES_ECB_MODE 

Electronic Codebook (ECB).

AES_CBC_MODE 

Cipher Block Chaining (CBC).

AES_OFB_MODE 

Output Feedback (OFB).

AES_CFB_MODE 

Cipher Feedback (CFB).

AES_CTR_MODE 

Counter (CTR).

AES_GCM_MODE 

Galois Counter Mode (GCM).

AES start mode.

Enumerator
AES_MANUAL_START 

Manual start mode.

AES_AUTO_START 

Auto start mode.

AES_IDATAR0_START 

AES_IDATAR0 access only Auto Mode.

void aes_disable ( void  )
static void aes_disable_interrupt ( Aes *const  p_aes,
aes_interrupt_source_t  source 
)
inlinestatic

Disable an AES interrupt.

Parameters
[out]p_aesModule hardware register base address pointer
[in]sourceInterrupt source
void aes_enable ( void  )

Enable the AES module.

References sleepmgr_lock_mode(), SLEEPMGR_SLEEP_WFI, and sysclk_enable_peripheral_clock().

Referenced by main().

static void aes_enable_interrupt ( Aes *const  p_aes,
aes_interrupt_source_t  source 
)
inlinestatic

Enable an AES interrupt.

Parameters
[out]p_aesModule hardware register base address pointer
[in]sourceInterrupt source

Referenced by aes_set_callback().

void aes_get_config_defaults ( struct aes_config *const  p_cfg)

Initializes an AES configuration structure to defaults.

Initializes the specified AES configuration structure to a set of known default values.

Note
This function should be called to initialize all new instances of AES configuration structures before they are further modified by the user application.

The default configuration is as follows:

  • Data encryption
  • 128-bit AES key size
  • 128-bit cipher feedback size
  • Manual start mode
  • Electronic Codebook (ECB) mode
  • Last output data mode is disabled
  • No extra delay
Parameters
[out]p_cfgPointer to an AES configuration structure

References AES_CFB_SIZE_128, AES_ECB_MODE, AES_ENCRYPTION, AES_KEY_SIZE_128, AES_MANUAL_START, Assert, aes_config::cfb_size, aes_config::encrypt_mode, aes_config::gtag_en, aes_config::key_size, aes_config::lod, aes_config::opmode, aes_config::processing_delay, and aes_config::start_mode.

Referenced by main().

Pdc* aes_get_pdc_base ( Aes *  p_aes)

Get AES PDC base address.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
Returns
The PDC registers base address for the AES module.

References Assert, and NULL.

void aes_init ( Aes *const  p_aes,
struct aes_config *const  p_cfg 
)

Initialize the AES module.

Parameters
[out]p_aesModule hardware register base address pointer
[in]p_cfgPointer to an AES configuration structure

References aes_reset(), aes_set_config(), Assert, sysclk_disable_peripheral_clock(), and sysclk_enable_peripheral_clock().

Referenced by main().

static uint32_t aes_read_authen_datalength ( Aes *const  p_aes)
inlinestatic

Get the AES Additional Authenticated Data (AAD) length in bytes.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
Returns
The Additional Authenticated Data (AAD) length in bytes.
static uint32_t aes_read_gcm_counter ( Aes *const  p_aes)
inlinestatic

Get the AES GCM Encryption Counter.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
Returns
The AES GCM encryption counter.
static uint32_t aes_read_gcmh ( Aes *const  p_aes,
uint32_t  id 
)
inlinestatic

Get AES GCM Hash subkey word.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
[in]idIndex into the GCMHR array (range 0 to 3)
Returns
The contents of the AES_GCMHRx[x = 0...3] register specified.
static uint32_t aes_read_ghash ( Aes *const  p_aes,
uint32_t  id 
)
inlinestatic

Get the AES GCM Intermediate Hash Word.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
[in]idIndex into the GHASH array (range 0 to 3)
Returns
The content of the AES_GHASHRx[x = 0...3] register.
static uint32_t aes_read_interrupt_mask ( Aes *const  p_aes)
inlinestatic

Get the AES interrupt mask status.

Parameters
[in]p_aesModule hardware register base address pointer
Returns
The AES interrupt mask contents.

Referenced by AES_Handler().

static uint32_t aes_read_interrupt_status ( Aes *const  p_aes)
inlinestatic

Get the AES interrupt status.

Parameters
[in]p_aesModule hardware register base address pointer
Returns
The AES interrupt status register contents.

Referenced by AES_Handler().

void aes_read_output_data ( Aes *const  p_aes,
uint32_t *  p_output_data_buffer 
)

Read the output data.

Note
The data buffer that holds the processed data must be large enough to hold four consecutive 32-bit words.
Parameters
[in]p_aesModule hardware register base address pointer
[in]*p_output_data_bufferPointer to an output buffer

References Assert.

Referenced by aes_callback().

static uint32_t aes_read_pctext_length ( Aes *const  p_aes)
inlinestatic

Get the AES plaintext/ciphertext length in bytes.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
Returns
The plaintext/ciphertext length in bytes.
static uint32_t aes_read_tag ( Aes *const  p_aes,
uint32_t  id 
)
inlinestatic

Get AES GCM Authentication Tag Word.

Note
This function is only available on SAM4C devices.
Parameters
[in]p_aesModule hardware register base address pointer
[in]idIndex into the TAGR array (range 0 to 3)
Returns
The contents of the AES_TAGRx[x = 0...3] register specified.
static void aes_reset ( Aes *const  p_aes)
inlinestatic

Perform an AES software reset.

Parameters
[out]p_aesModule hardware register base address pointer

Referenced by aes_init().

void aes_set_callback ( Aes *const  p_aes,
aes_interrupt_source_t  source,
aes_callback_t  callback,
uint8_t  irq_level 
)

Set the AES interrupt callback.

Parameters
[out]p_aesModule hardware register base address pointer
[in]sourceInterrupt source
[in]callbackInterrupt callback function pointer
[in]irq_levelInterrupt priority level

References aes_callback_pointer, aes_enable_interrupt(), AES_INTERRUPT_DATA_READY, AES_INTERRUPT_END_OF_RECEIVE_BUFFER, AES_INTERRUPT_END_OF_TRANSMIT_BUFFER, AES_INTERRUPT_RECEIVE_BUFFER_FULL, AES_INTERRUPT_TRANSMIT_BUFFER_FULL, AES_INTERRUPT_UNSPECIFIED_REGISTER_ACCESS, Assert, callback, and irq_register_handler.

Referenced by main().

void aes_set_config ( Aes *const  p_aes,
struct aes_config *const  p_cfg 
)
static void aes_start ( Aes *const  p_aes)
inlinestatic

Start a manual encryption/decryption process.

Parameters
[out]p_aesModule hardware register base address pointer
static void aes_write_authen_datalength ( Aes *const  p_aes,
uint32_t  length 
)
inlinestatic

Set the AES Additional Authenticated Data (AAD) length in bytes.

Note
This function is only available on SAM4C devices.
Parameters
[out]p_aesModule hardware register base address pointer
[in]lengthLength in bytes of the AAD data to be processed
static void aes_write_gcmh ( Aes *const  p_aes,
uint32_t  id,
uint32_t  hword 
)
inlinestatic

Set the AES GCM Hash subkey word.

Note
This function is only available on SAM4C devices.
Parameters
[out]p_aesModule hardware register base address pointer
[in]idIndex into the GCMHR array (range 0 to 3)
[in]hwordGCM H Word
static void aes_write_ghash ( Aes *const  p_aes,
uint32_t  id,
uint32_t  ghash 
)
inlinestatic

Set the AES GCM Intermediate Hash Word.

Note
This function is only available on SAM4C devices.
Parameters
[out]p_aesModule hardware register base address pointer
[in]idIndex into the GHASHx array (range 0 to 3)
[in]ghashIntermediate GCM Hash Word x
void aes_write_initvector ( Aes *const  p_aes,
const uint32_t *  p_vector 
)

Write the initialization vector (for the CBC, CFB, OFB, CTR & GCM cipher modes).

Parameters
[out]p_aesModule hardware register base address pointer
[in]p_vectorPointer to four contiguous 32-bit words

References Assert.

Referenced by cbc_mode_test(), cfb128_mode_test(), ctr_mode_test(), ofb_mode_test(), run_cbc_mode_test(), run_cfb128_mode_test(), run_ctr_mode_test(), and run_ofb_mode_test().

void aes_write_input_data ( Aes *const  p_aes,
const uint32_t *  p_input_data_buffer 
)

Write the input data (four consecutive 32-bit words).

Parameters
[out]p_aesModule hardware register base address pointer
[in]p_input_data_bufferPointer to an input data buffer

References Assert.

Referenced by cbc_mode_test(), cfb128_mode_test(), ctr_mode_test(), ecb_mode_test(), ofb_mode_test(), run_cbc_mode_test(), run_cfb128_mode_test(), run_ctr_mode_test(), run_ecb_mode_test(), and run_ofb_mode_test().

void aes_write_key ( Aes *const  p_aes,
const uint32_t *  p_key 
)

Write the 128/192/256-bit cryptographic key.

Parameters
[out]p_aesModule hardware register base address pointer
[in]p_keyPointer to 4/6/8 contiguous 32-bit words
Note
The key size depends on the current AES configuration.

References Assert.

Referenced by cbc_mode_test(), cfb128_mode_test(), ctr_mode_test(), ecb_mode_test(), ofb_mode_test(), run_cbc_mode_test(), run_cfb128_mode_test(), run_ctr_mode_test(), run_ecb_mode_test(), and run_ofb_mode_test().

static void aes_write_pctext_length ( Aes *const  p_aes,
uint32_t  length 
)
inlinestatic

Set the AES plaintext/ciphertext length in bytes.

Note
This function is only available on SAM4C devices.
Parameters
[out]p_aesModule hardware register base address pointer
[in]lengthLength in bytes of the plaintext/ciphertext data