Performs the functionalities of Range measurement mode, Evaluate the Communication coverage of the transceiver.
Macros | |
#define | APP_SEND_TEST_PKT_INTERVAL_IN_MICRO_SEC (250000) |
#define | DATA_PKT (0x00) |
Functions | |
void | app_print_statistics (void) |
Print the statistics for Range Measurement on the UART Terminal. More... | |
static int | range_test_frame_tx (void) |
Send Range Measurement mode test frames to the peer device. More... | |
void | range_test_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx when the node is in Range Measurement mode i.e RANGE_TEST_TX_ON or RANGE_TEST_TX_OFF. More... | |
void | range_test_tx_off_task (void) |
Application task handling Range Measurement when the node is in RANGE_TEST_TX_OFF state, where no TX is enabled and only RX is ON. More... | |
void | range_test_tx_on_exit (void) |
To exit the Application task from RANGE_TEST_TX_ON state, where both TX and RX is enabled. More... | |
void | range_test_tx_on_init (void *arg) |
Initialization of Range Measurement mode in RANGE_TX_ON State. More... | |
void | range_test_tx_on_task (void) |
Application task handling Range Measurement when the node is in RANGE_TEST_TX_ON state, where both TX and RX is enabled. More... | |
static void | range_test_tx_timer_handler_cb (void *parameter) |
Callback function that handles timer in Range Measurement Mode. More... | |
Variables | |
static uint32_t | num_of_frames_rec |
static uint32_t | num_of_frames_send |
static uint8_t | seq_num |
#define APP_SEND_TEST_PKT_INTERVAL_IN_MICRO_SEC (250000) |
Referenced by range_test_tx_on_init(), and range_test_tx_timer_handler_cb().
#define DATA_PKT (0x00) |
Referenced by range_test_frame_tx(), and range_test_rx_cb().
void app_print_statistics | ( | void | ) |
Print the statistics for Range Measurement on the UART Terminal.
References num_of_frames_rec, and num_of_frames_send.
|
static |
Send Range Measurement mode test frames to the peer device.
This is a unicast with source address and destination addresses which were set during peer search process
References app_payload_t::cmd_id, data, DATA_PKT, FCF_SHORT_ADDR, node_info, num_of_frames_send, app_payload_t::payload, node_ib_t::peer_short_addr, data_pkt_range_test_t::pkt_count, seq_num, app_payload_t::seq_num, and transmit_frame().
Referenced by range_test_tx_timer_handler_cb().
void range_test_rx_cb | ( | frame_info_t * | frame | ) |
Callback that is called if data has been received by trx when the node is in Range Measurement mode i.e RANGE_TEST_TX_ON or RANGE_TEST_TX_OFF.
frame | Pointer to received frame |
References app_led_event(), app_payload_t::cmd_id, DATA_PKT, FCS_LEN, FRAME_OVERHEAD, LED_EVENT_RX_FRAME, LENGTH_FIELD_LEN, frame_info_tag::mpdu, and num_of_frames_rec.
void range_test_tx_off_task | ( | void | ) |
Application task handling Range Measurement when the node is in RANGE_TEST_TX_OFF state, where no TX is enabled and only RX is ON.
References app_debounce_button(), print_event(), PRINT_RANGE_MEASURE_STATSTICS, RANGE_TEST_TX_ON, set_main_state(), and sio2host_getchar_nowait().
void range_test_tx_on_exit | ( | void | ) |
To exit the Application task from RANGE_TEST_TX_ON state, where both TX and RX is enabled.
References APP_TIMER_TO_TX, print_event(), and PRINT_RANGE_MEASURE_TX_STOP.
void range_test_tx_on_init | ( | void * | arg | ) |
Initialization of Range Measurement mode in RANGE_TX_ON State.
arg | arguments to init RANGE_TX_ON state |
References APP_SEND_TEST_PKT_INTERVAL_IN_MICRO_SEC, APP_TIMER_TO_TX, FUNC_PTR, NULL, print_event(), PRINT_RANGE_MEASURE_TX_START, range_test_tx_timer_handler_cb(), and seq_num.
void range_test_tx_on_task | ( | void | ) |
Application task handling Range Measurement when the node is in RANGE_TEST_TX_ON state, where both TX and RX is enabled.
References app_debounce_button(), NULL, print_event(), PRINT_RANGE_MEASURE_STATSTICS, RANGE_TEST_TX_OFF, set_main_state(), and sio2host_getchar_nowait().
|
static |
Callback function that handles timer in Range Measurement Mode.
parameter | pass parameters to timer handler |
References app_led_event(), APP_SEND_TEST_PKT_INTERVAL_IN_MICRO_SEC, APP_TIMER_TO_TX, FUNC_PTR, LED_EVENT_TX_FRAME, NULL, num_of_frames_send, and range_test_frame_tx().
Referenced by range_test_tx_on_init().
|
static |
Referenced by app_print_statistics(), and range_test_rx_cb().
|
static |
Referenced by app_print_statistics(), range_test_frame_tx(), and range_test_tx_timer_handler_cb().
|
static |
Referenced by range_test_frame_tx(), and range_test_tx_on_init().