Declaration of main function used by HID generic example.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_generic_disable (void) |
Called by HID interface Callback running when USB Host disable generic interface. More... | |
bool | main_generic_enable (void) |
Called by HID interface Callback running when USB Host enable generic interface. More... | |
void | main_hid_set_feature (uint8_t *report) |
Called by UDI HID generic when USB Host send a feature request. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void main_generic_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable generic interface.
References main_b_generic_enable.
bool main_generic_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable generic interface.
true | if generic startup is ok |
References main_b_generic_enable.
void main_hid_set_feature | ( | uint8_t * | report | ) |
Called by UDI HID generic when USB Host send a feature request.
References udc_stop(), and ui_powerdown().
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
References ui_wakeup_enable().
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
References main_b_suspend_event, and ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
References main_b_cdc_enable, main_b_generic_enable, main_b_kbd_enable, main_b_keyboard_enable, main_b_mouse_enable, main_b_msc_enable, main_b_phdc_enable, main_b_sof_event, main_b_vendor_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
References main_b_resume_event, and ui_powerdown().