#include "lwip/opt.h"
#include "lwip/err.h"
#include "lwip/ip_addr.h"
#include "lwip/ip6_addr.h"
#include "lwip/def.h"
#include "lwip/pbuf.h"
Data Structures | |
struct | netif |
Generic data structure used for all lwIP network interfaces. More... | |
Macros | |
#define | ENABLE_LOOPBACK (LWIP_NETIF_LOOPBACK || LWIP_HAVE_LOOPIF) |
#define | NETIF_FLAG_BROADCAST 0x02U |
If set, the netif has broadcast capability. More... | |
#define | NETIF_FLAG_DHCP 0x08U |
If set, the interface is configured using DHCP. More... | |
#define | NETIF_FLAG_ETHARP 0x20U |
If set, the netif is an ethernet device using ARP. More... | |
#define | NETIF_FLAG_ETHERNET 0x40U |
If set, the netif is an ethernet device. More... | |
#define | NETIF_FLAG_IGMP 0x80U |
If set, the netif has IGMP capability. More... | |
#define | NETIF_FLAG_LINK_UP 0x10U |
If set, the interface has an active link (set by the network interface driver). More... | |
#define | NETIF_FLAG_POINTTOPOINT 0x04U |
If set, the netif is one end of a point-to-point connection. More... | |
#define | NETIF_FLAG_UP 0x01U |
Whether the network interface is 'up'. More... | |
#define | NETIF_INIT_SNMP(netif, type, speed) |
#define | netif_is_link_up(netif) (((netif)->flags & NETIF_FLAG_LINK_UP) ? (u8_t)1 : (u8_t)0) |
Ask if a link is up. More... | |
#define | netif_is_up(netif) (((netif)->flags & NETIF_FLAG_UP) ? (u8_t)1 : (u8_t)0) |
Ask if an interface is up. More... | |
#define | NETIF_MAX_HWADDR_LEN 6U |
Must be the maximum of all used hardware address lengths across all types of interfaces in use. More... | |
#define | NETIF_SET_HWADDRHINT(netif, hint) |
Typedefs | |
typedef err_t(* | netif_igmp_mac_filter_fn )(struct netif *netif, ip_addr_t *group, u8_t action) |
Function prototype for netif igmp_mac_filter functions. More... | |
typedef err_t(* | netif_init_fn )(struct netif *netif) |
Function prototype for netif init functions. More... | |
typedef err_t(* | netif_input_fn )(struct pbuf *p, struct netif *inp) |
Function prototype for netif->input functions. More... | |
typedef err_t(* | netif_linkoutput_fn )(struct netif *netif, struct pbuf *p) |
Function prototype for netif->linkoutput functions. More... | |
typedef err_t(* | netif_output_fn )(struct netif *netif, struct pbuf *p, ip_addr_t *ipaddr) |
Function prototype for netif->output functions. More... | |
typedef void(* | netif_status_callback_fn )(struct netif *netif) |
Function prototype for netif status- or link-callback functions. More... | |
Functions | |
struct netif * | netif_add (struct netif *netif, ip_addr_t *ipaddr, ip_addr_t *netmask, ip_addr_t *gw, void *state, netif_init_fn init, netif_input_fn input) |
Add a network interface to the list of lwIP netifs. More... | |
struct netif * | netif_find (char *name) |
Find a network interface by searching for its name. More... | |
void | netif_init (void) |
void | netif_remove (struct netif *netif) |
Remove a network interface from the list of lwIP netifs. More... | |
void | netif_set_addr (struct netif *netif, ip_addr_t *ipaddr, ip_addr_t *netmask, ip_addr_t *gw) |
Change IP address configuration for a network interface (including netmask and default gateway). More... | |
void | netif_set_default (struct netif *netif) |
Set a network interface as the default network interface (used to output all packets for which no specific route is found) More... | |
void | netif_set_down (struct netif *netif) |
Bring an interface down, disabling any traffic processing. More... | |
void | netif_set_gw (struct netif *netif, ip_addr_t *gw) |
Change the default gateway for a network interface. More... | |
void | netif_set_ipaddr (struct netif *netif, ip_addr_t *ipaddr) |
Change the IP address of a network interface. More... | |
void | netif_set_link_down (struct netif *netif) |
Called by a driver when its link goes down. More... | |
void | netif_set_link_up (struct netif *netif) |
Called by a driver when its link goes up. More... | |
void | netif_set_netmask (struct netif *netif, ip_addr_t *netmask) |
Change the netmask of a network interface. More... | |
void | netif_set_up (struct netif *netif) |
Bring an interface up, available for processing traffic. More... | |
Variables | |
struct netif * | netif_default |
The default network interface. More... | |
struct netif * | netif_list |
The list of network interfaces. More... | |
#define ENABLE_LOOPBACK (LWIP_NETIF_LOOPBACK || LWIP_HAVE_LOOPIF) |
#define NETIF_FLAG_BROADCAST 0x02U |
If set, the netif has broadcast capability.
Set by the netif driver in its init function.
#define NETIF_FLAG_DHCP 0x08U |
If set, the interface is configured using DHCP.
Set by the DHCP code when starting or stopping DHCP.
#define NETIF_FLAG_ETHARP 0x20U |
If set, the netif is an ethernet device using ARP.
Set by the netif driver in its init function. Used to check input packet types and use of DHCP.
#define NETIF_FLAG_ETHERNET 0x40U |
If set, the netif is an ethernet device.
It might not use ARP or TCP/IP if it is used for PPPoE only.
#define NETIF_FLAG_IGMP 0x80U |
If set, the netif has IGMP capability.
Set by the netif driver in its init function.
#define NETIF_FLAG_LINK_UP 0x10U |
If set, the interface has an active link (set by the network interface driver).
Either set by the netif driver in its init function (if the link is up at that time) or at a later point once the link comes up (if link detection is supported by the hardware).
#define NETIF_FLAG_POINTTOPOINT 0x04U |
If set, the netif is one end of a point-to-point connection.
Set by the netif driver in its init function.
#define NETIF_FLAG_UP 0x01U |
Whether the network interface is 'up'.
This is a software flag used to control whether this network interface is enabled and processes traffic. It is set by the startup code (for static IP configuration) or by dhcp/autoip when an address has been assigned.
#define NETIF_INIT_SNMP | ( | netif, | |
type, | |||
speed | |||
) |
#define netif_is_link_up | ( | netif | ) | (((netif)->flags & NETIF_FLAG_LINK_UP) ? (u8_t)1 : (u8_t)0) |
Ask if a link is up.
#define netif_is_up | ( | netif | ) | (((netif)->flags & NETIF_FLAG_UP) ? (u8_t)1 : (u8_t)0) |
Ask if an interface is up.
#define NETIF_MAX_HWADDR_LEN 6U |
Must be the maximum of all used hardware address lengths across all types of interfaces in use.
This does not have to be changed, normally.
#define NETIF_SET_HWADDRHINT | ( | netif, | |
hint | |||
) |
Function prototype for netif igmp_mac_filter functions.
Function prototype for netif init functions.
Set up flags and output/linkoutput callback functions in this function.
netif | The netif to initialize |
Function prototype for netif->input functions.
This function is saved as 'input' callback function in the netif struct. Call it when a packet has been received.
p | The received packet, copied into a pbuf |
inp | The netif which received the packet |
Function prototype for netif->linkoutput functions.
Only used for ethernet netifs. This function is called by ARP when a packet shall be sent.
netif | The netif which shall send a packet |
p | The packet to send (raw ethernet packet) |
Function prototype for netif->output functions.
Called by lwIP when a packet shall be sent. For ethernet netif, set this to 'etharp_output' and set 'linkoutput'.
netif | The netif which shall send a packet |
p | The packet to send (p->payload points to IP header) |
ipaddr | The IP address to which the packet shall be sent |
Function prototype for netif status- or link-callback functions.
struct netif* netif_add | ( | struct netif * | netif, |
ip_addr_t * | ipaddr, | ||
ip_addr_t * | netmask, | ||
ip_addr_t * | gw, | ||
void * | state, | ||
netif_init_fn | init, | ||
netif_input_fn | input | ||
) |
Add a network interface to the list of lwIP netifs.
netif | a pre-allocated netif structure |
ipaddr | IP address for the new netif |
netmask | network mask for the new netif |
gw | default gateway IP address for the new netif |
state | opaque data passed to the new netif |
init | callback function that initializes the interface |
input | callback function that is called to pass ingress packets up in the protocol layer stack. |
struct netif* netif_find | ( | char * | name | ) |
Find a network interface by searching for its name.
name | the name of the netif (like netif->name) plus concatenated number in ascii representation (e.g. 'en0') |
void netif_init | ( | void | ) |
void netif_remove | ( | struct netif * | netif | ) |
Remove a network interface from the list of lwIP netifs.
netif | the network interface to remove |
void netif_set_addr | ( | struct netif * | netif, |
ip_addr_t * | ipaddr, | ||
ip_addr_t * | netmask, | ||
ip_addr_t * | gw | ||
) |
Change IP address configuration for a network interface (including netmask and default gateway).
netif | the network interface to change |
ipaddr | the new IP address |
netmask | the new netmask |
gw | the new default gateway |
void netif_set_default | ( | struct netif * | netif | ) |
Set a network interface as the default network interface (used to output all packets for which no specific route is found)
netif | the default network interface |
void netif_set_down | ( | struct netif * | netif | ) |
Bring an interface down, disabling any traffic processing.
Change the default gateway for a network interface.
netif | the network interface to change |
gw | the new default gateway |
Change the IP address of a network interface.
netif | the network interface to change |
ipaddr | the new IP address |
void netif_set_link_down | ( | struct netif * | netif | ) |
Called by a driver when its link goes down.
void netif_set_link_up | ( | struct netif * | netif | ) |
Called by a driver when its link goes up.
Change the netmask of a network interface.
netif | the network interface to change |
netmask | the new netmask |
void netif_set_up | ( | struct netif * | netif | ) |
Bring an interface up, available for processing traffic.
struct netif* netif_default |
The default network interface.
struct netif* netif_list |
The list of network interfaces.