Microchip® Advanced Software Framework

lwip/lwip-1.3.2/src/include/lwip/sys.h File Reference
#include "lwip/opt.h"
#include "lwip/err.h"
#include "arch/sys_arch.h"

Data Structures

struct  sys_timeo
 
struct  sys_timeouts
 

Macros

#define SYS_ARCH_DEC(var, val)
 
#define SYS_ARCH_DECL_PROTECT(lev)
 SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for certain critical regions during buffer allocation, deallocation and memory allocation and deallocation. More...
 
#define SYS_ARCH_GET(var, ret)
 
#define SYS_ARCH_INC(var, val)
 
#define SYS_ARCH_PROTECT(lev)
 
#define SYS_ARCH_SET(var, val)
 
#define SYS_ARCH_TIMEOUT   0xffffffffUL
 Return code for timeouts from sys_arch_mbox_fetch and sys_arch_sem_wait. More...
 
#define SYS_ARCH_UNPROTECT(lev)
 
#define SYS_MBOX_EMPTY   SYS_ARCH_TIMEOUT
 
#define sys_mbox_tryfetch(mbox, msg)   sys_arch_mbox_tryfetch(mbox, msg)
 

Typedefs

typedef void(* sys_timeout_handler )(void *arg)
 

Functions

u32_t sys_arch_mbox_fetch (sys_mbox_t mbox, void **msg, u32_t timeout)
 Blocks the thread until a message arrives in the mailbox, but does not block the thread longer than "timeout" milliseconds (similar to the sys_arch_sem_wait() function). More...
 
u32_t sys_arch_mbox_tryfetch (sys_mbox_t mbox, void **msg)
 This is similar to sys_arch_mbox_fetch, however if a message is not present in the mailbox, it immediately returns with the code SYS_MBOX_EMPTY. More...
 
u32_t sys_arch_sem_wait (sys_sem_t sem, u32_t timeout)
 Blocks the thread while waiting for the semaphore to be signaled. More...
 
struct sys_timeoutssys_arch_timeouts (void)
 Get a pointer to the per-thread sys_timeouts structure. More...
 
void sys_init (void)
 Initialize the sys_arch layer. More...
 
u32_t sys_jiffies (void)
 
void sys_mbox_fetch (sys_mbox_t mbox, void **msg)
 Wait (forever) for a message to arrive in an mbox. More...
 
void sys_mbox_free (sys_mbox_t mbox)
 Deallocates a mailbox. More...
 
sys_mbox_t sys_mbox_new (int size)
 Creates an empty mailbox for maximum "size" elements. More...
 
void sys_mbox_post (sys_mbox_t mbox, void *msg)
 Posts the "msg" to the mailbox. More...
 
err_t sys_mbox_trypost (sys_mbox_t mbox, void *msg)
 Try to posts the "msg" to the mailbox. More...
 
void sys_msleep (u32_t ms)
 Sleep for some ms. More...
 
u32_t sys_now (void)
 Returns the current time in milliseconds. More...
 
void sys_sem_free (sys_sem_t sem)
 Frees a semaphore created by sys_sem_new. More...
 
sys_sem_t sys_sem_new (u8_t count)
 Creates and returns a new semaphore. More...
 
void sys_sem_signal (sys_sem_t sem)
 Signals (or releases) a semaphore. More...
 
void sys_sem_wait (sys_sem_t sem)
 Wait (forever) for a semaphore to become available. More...
 
int sys_sem_wait_timeout (sys_sem_t sem, u32_t timeout)
 Wait for a semaphore with timeout (specified in ms) More...
 
sys_thread_t sys_thread_new (char *name, void(*thread)(void *arg), void *arg, int stacksize, int prio)
 Instantiate a thread for lwIP. More...
 
void sys_timeout (u32_t msecs, sys_timeout_handler h, void *arg)
 Create a one-shot timer (aka timeout). More...
 
void sys_untimeout (sys_timeout_handler h, void *arg)
 Go through timeout list (for this task only) and remove the first matching entry, even though the timeout has not triggered yet. More...
 

#define SYS_ARCH_DEC (   var,
  val 
)
Value:
do { \
SYS_ARCH_PROTECT(old_level); \
var -= val; \
SYS_ARCH_UNPROTECT(old_level); \
} while(0)
#define SYS_ARCH_DECL_PROTECT(lev)
SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for ...
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:284
#define SYS_ARCH_PROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:285
float32_t var
Definition: arm_class_marks_example_f32.c:150
#define SYS_ARCH_UNPROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:286
#define SYS_ARCH_DECL_PROTECT (   lev)

SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for certain critical regions during buffer allocation, deallocation and memory allocation and deallocation.

#define SYS_ARCH_GET (   var,
  ret 
)
Value:
do { \
SYS_ARCH_PROTECT(old_level); \
ret = var; \
SYS_ARCH_UNPROTECT(old_level); \
} while(0)
#define SYS_ARCH_DECL_PROTECT(lev)
SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for ...
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:284
#define SYS_ARCH_PROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:285
float32_t var
Definition: arm_class_marks_example_f32.c:150
#define SYS_ARCH_UNPROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:286
#define SYS_ARCH_INC (   var,
  val 
)
Value:
do { \
SYS_ARCH_PROTECT(old_level); \
var += val; \
SYS_ARCH_UNPROTECT(old_level); \
} while(0)
#define SYS_ARCH_DECL_PROTECT(lev)
SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for ...
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:284
#define SYS_ARCH_PROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:285
float32_t var
Definition: arm_class_marks_example_f32.c:150
#define SYS_ARCH_UNPROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:286
#define SYS_ARCH_PROTECT (   lev)
#define SYS_ARCH_SET (   var,
  val 
)
Value:
do { \
SYS_ARCH_PROTECT(old_level); \
var = val; \
SYS_ARCH_UNPROTECT(old_level); \
} while(0)
#define SYS_ARCH_DECL_PROTECT(lev)
SYS_LIGHTWEIGHT_PROT define SYS_LIGHTWEIGHT_PROT in lwipopts.h if you want inter-task protection for ...
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:284
#define SYS_ARCH_PROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:285
float32_t var
Definition: arm_class_marks_example_f32.c:150
#define SYS_ARCH_UNPROTECT(lev)
Definition: lwip/lwip-1.4.1/src/include/lwip/sys.h:286
#define SYS_ARCH_TIMEOUT   0xffffffffUL

Return code for timeouts from sys_arch_mbox_fetch and sys_arch_sem_wait.

#define SYS_ARCH_UNPROTECT (   lev)
#define SYS_MBOX_EMPTY   SYS_ARCH_TIMEOUT
#define sys_mbox_tryfetch (   mbox,
  msg 
)    sys_arch_mbox_tryfetch(mbox, msg)

typedef void(* sys_timeout_handler)(void *arg)

u32_t sys_arch_mbox_fetch ( sys_mbox_t  mbox,
void **  msg,
u32_t  timeout 
)

Blocks the thread until a message arrives in the mailbox, but does not block the thread longer than "timeout" milliseconds (similar to the sys_arch_sem_wait() function).

Parameters
mboxMailbox used.
msgA result parameter that is set by the function (i.e., by doing "*msg = ptr"). The "msg" parameter maybe NULL to indicate that the message should be dropped. 0 indicates the thread should be blocked until a message arrives.
Returns
Number of milliseconds spent waiting or SYS_ARCH_TIMEOUT if there was a timeout. Or ERR_MEM if invalid pointer to message box.

References NULL, pdFALSE, portTICK_RATE_MS, portTickType, SYS_ARCH_BLOCKING_TICKTIMEOUT, SYS_ARCH_TIMEOUT, xQueueReceive, and xTaskGetTickCount().

Referenced by sys_mbox_fetch().

u32_t sys_arch_mbox_tryfetch ( sys_mbox_t  mbox,
void **  msg 
)

This is similar to sys_arch_mbox_fetch, however if a message is not present in the mailbox, it immediately returns with the code SYS_MBOX_EMPTY.

On success 0 is returned.

Parameters
mboxMailbox used.
msgA result parameter that is set by the function (i.e., by doing "*msg = ptr"). The "msg" parameter maybe NULL to indicate that the message should be dropped.
Returns
Number of milliseconds spent waiting or SYS_ARCH_TIMEOUT if there was a timeout. Or ERR_MEM if invalid pointer to message box.

References NULL, pdFALSE, SYS_MBOX_EMPTY, and xQueueReceive.

u32_t sys_arch_sem_wait ( sys_sem_t  sem,
u32_t  timeout 
)

Blocks the thread while waiting for the semaphore to be signaled.

Note that there is another function sys_sem_wait in sys.c, but it is a wrapper for the sys_arch_sem_wait function. Please note that it is important for the semaphores to return an accurate count of elapsed milliseconds, since they are used to schedule timers in lwIP.

Parameters
semSemphore number.
timeoutThe timeout parameter specifies how many milliseconds the function should block before returning; if the function times out, it should return SYS_ARCH_TIMEOUT. If timeout=0, then the function should block indefinitely. If the function acquires the semaphore, it should return how many milliseconds expired while waiting for the semaphore.
Returns
SYS_ARCH_TIMEOUT if times out, otherwise return the milliseconds expired while waiting for the semaphore.

References pdFALSE, portTICK_RATE_MS, portTickType, SYS_ARCH_BLOCKING_TICKTIMEOUT, SYS_ARCH_TIMEOUT, xSemaphoreTake, and xTaskGetTickCount().

Referenced by cgi_chipInfo(), cgi_status(), gmac_task(), ksz8851snl_task(), mem_malloc(), sys_msleep(), and sys_sem_wait().

struct sys_timeouts* sys_arch_timeouts ( void  )

Get a pointer to the per-thread sys_timeouts structure.

In lwIP, each thread has a list of timeouts which is repressented as a linked list of sys_timeout structures. The sys_timeouts structure holds a pointer to a linked list of timeouts. This function is called by the lwIP timeout scheduler and must not return a NULL value.

Returns
Pointer to the per-thread sys_timeouts structure.

References NbActiveThreads, TimeoutlistPerThread::pid, Threads_TimeoutsList, TimeoutlistPerThread::timeouts, and xTaskGetCurrentTaskHandle().

Referenced by sys_mbox_fetch(), sys_sem_wait(), sys_timeout(), and sys_untimeout().

void sys_init ( void  )
u32_t sys_jiffies ( void  )
void sys_mbox_fetch ( sys_mbox_t  mbox,
void **  msg 
)

Wait (forever) for a message to arrive in an mbox.

While waiting, timeouts (for this thread) are processed.

Parameters
mboxthe mbox to fetch the message from
msgthe place to store the message

References sys_timeo::arg, sys_timeo::h, LOCK_TCPIP_CORE, LWIP_DEBUGF, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_mbox_fetch(), SYS_ARCH_TIMEOUT, sys_arch_timeouts(), SYS_DEBUG, sys_timeo::time, and UNLOCK_TCPIP_CORE.

void sys_mbox_free ( sys_mbox_t  mbox)

Deallocates a mailbox.

If there are messages still present in the mailbox when the mailbox is deallocated, it is an indication of a programming error in lwIP and the developer should be notified.

Parameters
mboxMailbox to be used.

References SYS_MBOX_NULL, and vQueueDelete().

sys_mbox_t sys_mbox_new ( int  size)

Creates an empty mailbox for maximum "size" elements.

Elements stored in mailboxes are pointers.

Parameters
sizeMaximum "size" elements.
Returns
Mailbox created.

References SYS_MBOX_NULL, and xQueueCreate.

Referenced by tcpip_init().

void sys_mbox_post ( sys_mbox_t  mbox,
void *  msg 
)

Posts the "msg" to the mailbox.

This function have to block until the "msg" is really posted.

Parameters
mboxMailbox used.
msgPointer to the message to be post.

References pdTRUE, SYS_ARCH_BLOCKING_TICKTIMEOUT, and xQueueSend.

Referenced by tcpip_callback_with_block(), tcpip_timeout(), and tcpip_untimeout().

err_t sys_mbox_trypost ( sys_mbox_t  mbox,
void *  msg 
)

Try to posts the "msg" to the mailbox.

Parameters
mboxMailbox used.
msgPointer to the message to be post.
Returns
ERR_MEM if the mailbox is full otherwise ERR_OK if the "msg" is posted.

References ERR_MEM, ERR_OK, errQUEUE_FULL, and xQueueSend.

Referenced by tcpip_callback_with_block(), tcpip_input(), and tcpip_trycallback().

void sys_msleep ( u32_t  ms)

Sleep for some ms.

Timeouts are NOT processed while sleeping.

Parameters
msnumber of milliseconds to sleep

Timeouts are processed while sleeping.

Parameters
msnumber of milliseconds to sleep

References ERR_OK, sys_arch_sem_wait(), sys_sem_free(), sys_sem_new(), and sys_sem_wait_timeout().

u32_t sys_now ( void  )

Returns the current time in milliseconds.

Returns the current time in milliseconds.

Returns the current time in milliseconds, may be the same as sys_jiffies or at least based on it.

References sys_get_ms(), and xTaskGetTickCount().

void sys_sem_free ( sys_sem_t  sem)

Frees a semaphore created by sys_sem_new.

Parameters
semSemaphore number.

References SYS_SEM_NULL, and vQueueDelete().

Referenced by sys_msleep().

sys_sem_t sys_sem_new ( u8_t  count)

Creates and returns a new semaphore.

Parameters
countInitial state of the semaphore.
Returns
ERR_OK for OK, other value indicates error.

References SYS_SEM_NULL, vSemaphoreCreateBinary, and xSemaphoreTake.

Referenced by cgi_search(), ethernetif_init(), mem_init(), sys_msleep(), and tcpip_init().

void sys_sem_signal ( sys_sem_t  sem)

Signals (or releases) a semaphore.

Parameters
semSemphore number.

References xSemaphoreGive.

Referenced by cgi_chipInfo(), cgi_status(), mem_malloc(), and sswt_handler().

void sys_sem_wait ( sys_sem_t  sem)

Wait (forever) for a semaphore to become available.

While waiting, timeouts (for this thread) are processed.

Parameters
semsemaphore to wait for

References sys_timeo::arg, sys_timeo::h, LWIP_DEBUGF, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_sem_wait(), SYS_ARCH_TIMEOUT, sys_arch_timeouts(), SYS_DEBUG, and sys_timeo::time.

int sys_sem_wait_timeout ( sys_sem_t  sem,
u32_t  timeout 
)

Wait for a semaphore with timeout (specified in ms)

Parameters
semsemaphore to wait
timeouttimeout in ms (0: wait forever)
Returns
0 on timeout, 1 otherwise

References sswt_cb::psem, sswt_handler(), sys_sem_wait, sys_timeout(), sys_untimeout(), and sswt_cb::timeflag.

Referenced by sys_msleep().

sys_thread_t sys_thread_new ( char *  name,
void(*)(void *arg)  thread,
void *  arg,
int  stacksize,
int  prio 
)

Instantiate a thread for lwIP.

Both the id and the priority are system dependent.

Parameters
namePointer to the thread name.
threadPointer to the thread function.
argArgument will be passed into the thread().
stacksizeStack size of the thread.
prioThread priority.
Returns
The id of the new thread.

References NbActiveThreads, NULL, pdPASS, TimeoutlistPerThread::pid, SYS_ARCH_DECL_PROTECT, SYS_ARCH_PROTECT, SYS_ARCH_UNPROTECT, Threads_TimeoutsList, and xTaskCreate.

Referenced by ethernetif_init(), http_task(), low_level_init(), and tcpip_init().

void sys_timeout ( u32_t  msecs,
sys_timeout_handler  h,
void *  arg 
)

Create a one-shot timer (aka timeout).

Timeouts are processed in the following cases:

Parameters
msecstime in milliseconds after that the timer should expire
hcallback function to call when msecs have elapsed
argargument to pass to the callback function

References sys_timeo::arg, sys_timeo::h, LWIP_ASSERT, LWIP_DEBUGF, memp_malloc(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_timeouts(), SYS_DEBUG, sys_timeo::time, and U32_F.

void sys_untimeout ( sys_timeout_handler  h,
void *  arg 
)

Go through timeout list (for this task only) and remove the first matching entry, even though the timeout has not triggered yet.

Note
This function only works as expected if there is only one timeout calling 'h' in the list of timeouts.
Parameters
hcallback function that would be called by the timeout
argcallback argument that would be passed to h

References sys_timeo::arg, sys_timeo::h, LWIP_ASSERT, memp_free(), sys_timeo::next, sys_timeouts::next, NULL, sys_arch_timeouts(), and sys_timeo::time.