Microchip® Advanced Software Framework

nand_flash_raw_smc.c File Reference

Raw flash operation.

This file contains definitions and functions for raw NAND Flash operation.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include "nand_flash_raw.h"
#include "conf_board.h"
#include "conf_nf.h"
#include "gpio.h"
#include "smc.h"
#include "sysclk.h"
#include "conf_ebi.h"
#include "delay.h"

Macros

#define BOARD_NAND_CS   0
 
#define CONF_NF_BUSWIDTH   0
 
#define CONF_NF_CYCLE_TIMING   0
 
#define CONF_NF_PULSE_TIMING   0
 
#define CONF_NF_SETUP_TIMING   0
 
#define DISABLE_CE(raw)   gpio_set_pin_high(PIN_NF_CE_IDX)
 
#define ENABLE_CE(raw)   gpio_set_pin_low(PIN_NF_CE_IDX)
 
#define MODEL(raw)   ((struct nand_flash_model *)raw)
 
#define NF_WP_PIN   0
 
#define PIN_NF_CE_IDX   0
 
#define PIN_NF_RB_IDX   0
 
#define READ_DATA16(raw)   (*((volatile uint16_t *)raw->data_address))
 
#define READ_DATA8(raw)   (*((volatile uint8_t *)raw->data_address))
 
#define WRITE_ADDRESS(raw, address)   {*((volatile uint8_t *)raw->address_address) = (uint8_t)address;}
 
#define WRITE_ADDRESS16(raw, address)   {*((volatile uint16_t *)raw->address_address) = (uint16_t)address;}
 
#define WRITE_COMMAND(raw, command)   {*((volatile uint8_t *)raw->command_address) = (uint8_t)command;}
 
#define WRITE_COMMAND16(raw, command)   {*((volatile uint16_t *)raw->command_address) = (uint16_t)command;}
 
#define WRITE_DATA16(raw, data)   {*((volatile uint16_t *)raw->data_address) = (uint16_t)data;}
 
#define WRITE_DATA8(raw, data)   {*((volatile uint8_t *)raw->data_address) = (uint8_t)data;}
 

Functions

static uint32_t check_status (const struct nand_flash_raw *raw)
 Check for program or erase operation is completed. More...
 
static uint32_t copy_page (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t source_page, uint16_t dest_block, uint16_t dest_page)
 Copy the data in a page of the NAND Flash device to an other page on that same chip. More...
 
static uint32_t erase_block (const struct nand_flash_raw *raw, uint16_t block)
 Erase the specified block of the device. More...
 
uint32_t nand_flash_raw_copy_block (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t dest_block)
 Copies the data of one whole block of a NAND Flash device to another block. More...
 
uint32_t nand_flash_raw_copy_page (const struct nand_flash_raw *raw, uint16_t source_block, uint16_t source_page, uint16_t dest_block, uint16_t dest_page)
 Copy the data in a page of the NAND Flash device to an other page on that same chip. More...
 
uint32_t nand_flash_raw_erase_block (const struct nand_flash_raw *raw, uint16_t block)
 Erase the specified block of the device, retrying several time if it fails. More...
 
uint32_t nand_flash_raw_initialize (struct nand_flash_raw *raw, const struct nand_flash_model *model, uint32_t command_address, uint32_t address_address, uint32_t data_address)
 Initializes a nand_flash_raw instance based on the given model and physical interface. More...
 
uint32_t nand_flash_raw_read_id (const struct nand_flash_raw *raw)
 Read and return the identifiers of a NAND Flash chip. More...
 
void nand_flash_raw_read_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, uint8_t *data, uint8_t *spare)
 Read the data and/or the spare areas of a page of a NAND Flash into the provided buffers. More...
 
void nand_flash_raw_reset (const struct nand_flash_raw *raw)
 Reset a NAND Flash device. More...
 
uint32_t nand_flash_raw_write_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, uint8_t *data, uint8_t *spare)
 Write the data and/or the spare areas of a page into a NAND Flash. More...
 
static void read_data (const struct nand_flash_raw *raw, uint8_t *buffer, uint32_t size)
 Read data from the NAND Flash chip into the provided buffer. More...
 
static void wait_ready (void)
 Wait for the completion of a page program, erase and random read completion. More...
 
static void write_column_address (const struct nand_flash_raw *raw, uint16_t column_address)
 Send the column address to the NAND Flash chip. More...
 
static void write_data (const struct nand_flash_raw *raw, uint8_t *buffer, uint32_t size)
 Send data to the NAND Flash chip from the provided buffer. More...
 
static uint32_t write_page (const struct nand_flash_raw *raw, uint16_t block, uint16_t page, void *data, void *spare)
 Write the data and/or the spare area of a page on a NAND Flash chip. More...
 
static void write_row_address (const struct nand_flash_raw *raw, uint32_t row_address)
 Send the row address to the NAND Flash chip. More...
 

#define BOARD_NAND_CS   0
#define CONF_NF_BUSWIDTH   0
#define CONF_NF_CYCLE_TIMING   0
#define CONF_NF_PULSE_TIMING   0
#define CONF_NF_SETUP_TIMING   0
#define NF_WP_PIN   0
#define PIN_NF_CE_IDX   0
#define PIN_NF_RB_IDX   0
#define READ_DATA16 (   raw)    (*((volatile uint16_t *)raw->data_address))

Referenced by read_data().

#define READ_DATA8 (   raw)    (*((volatile uint8_t *)raw->data_address))
#define WRITE_ADDRESS (   raw,
  address 
)    {*((volatile uint8_t *)raw->address_address) = (uint8_t)address;}
#define WRITE_ADDRESS16 (   raw,
  address 
)    {*((volatile uint16_t *)raw->address_address) = (uint16_t)address;}
#define WRITE_COMMAND (   raw,
  command 
)    {*((volatile uint8_t *)raw->command_address) = (uint8_t)command;}
#define WRITE_COMMAND16 (   raw,
  command 
)    {*((volatile uint16_t *)raw->command_address) = (uint16_t)command;}
#define WRITE_DATA16 (   raw,
  data 
)    {*((volatile uint16_t *)raw->data_address) = (uint16_t)data;}

Referenced by write_data().

#define WRITE_DATA8 (   raw,
  data 
)    {*((volatile uint8_t *)raw->data_address) = (uint8_t)data;}

Referenced by write_data().

static uint32_t check_status ( const struct nand_flash_raw raw)
static

Check for program or erase operation is completed.

Parameters
rawPointer to a nand_flash_raw instance.
Returns
1 operation is completed; otherwise, return 0.

References NAND_COMMAND_STATUS, NAND_STATUS_ERROR, NAND_STATUS_READY, READ_DATA8, status, and WRITE_COMMAND.

Referenced by copy_page(), erase_block(), and write_page().

static uint32_t copy_page ( const struct nand_flash_raw raw,
uint16_t  source_block,
uint16_t  source_page,
uint16_t  dest_block,
uint16_t  dest_page 
)
static

Copy the data in a page of the NAND Flash device to an other page on that same chip.

Parameters
rawPointer to a nand_flash_raw instance.
source_blockSource block number.
source_pageSource page number inside the source block.
dest_blockDestination block number.
dest_pageDestination page number inside the destination block.
Returns
0 if successful; otherwise return the error code.

References check_status(), data, DISABLE_CE, ENABLE_CE, MODEL, NAND_COMMAND_COPYBACK_PROGRAM_1, NAND_COMMAND_COPYBACK_PROGRAM_2, NAND_COMMAND_COPYBACK_READ_1, NAND_COMMAND_COPYBACK_READ_2, NAND_COMMON_ERROR_CANNOTCOPY, NAND_COMMON_ERROR_CANNOTWRITE, NAND_COMMON_MAX_PAGE_SIZE, NAND_COMMON_MAX_PAGE_SPARE_SIZE, nand_flash_model_copy_back(), nand_flash_model_get_block_size_in_pages(), nand_flash_raw_read_page(), nand_flash_raw_write_page(), wait_ready(), write_column_address(), WRITE_COMMAND, and write_row_address().

Referenced by nand_flash_raw_copy_page().

static uint32_t erase_block ( const struct nand_flash_raw raw,
uint16_t  block 
)
static

Erase the specified block of the device.

Parameters
rawPointer to a nand_flash_raw instance.
blockNumber of the physical block to erase.
Returns
0 if successful; otherwise return the error code.

References check_status(), delay_ms, DISABLE_CE, ENABLE_CE, MODEL, NAND_COMMAND_ERASE_1, NAND_COMMAND_ERASE_2, NAND_COMMON_ERROR_CANNOTERASE, nand_flash_model_get_block_size_in_pages(), wait_ready(), WRITE_COMMAND, and write_row_address().

Referenced by nand_flash_raw_erase_block().

uint32_t nand_flash_raw_copy_block ( const struct nand_flash_raw raw,
uint16_t  source_block,
uint16_t  dest_block 
)

Copies the data of one whole block of a NAND Flash device to another block.

Parameters
rawPointer to a nand_flash_raw instance.
source_blockSource block number.
dest_blockDestination block number.
Returns
0 if successful; otherwise returns an NAND_COMMON_ERROR_BADBLOCK.
Note
Reference the Flash datasheet for the block address restriction.

References Assert, MODEL, NAND_COMMON_ERROR_BADBLOCK, nand_flash_model_get_block_size_in_pages(), and nand_flash_raw_copy_page().

uint32_t nand_flash_raw_copy_page ( const struct nand_flash_raw raw,
uint16_t  source_block,
uint16_t  source_page,
uint16_t  dest_block,
uint16_t  dest_page 
)

Copy the data in a page of the NAND Flash device to an other page on that same chip.

Parameters
rawPointer to a nand_flash_raw instance.
source_blockSource block number.
source_pageSource page number inside the source block.
dest_blockDestination block number.
dest_pageDestination page number inside the destination block.
Returns
0 if successful; otherwise returns an NAND_COMMON_ERROR_BADBLOCK.
Note
Reference the Flash datasheet for the block and page address restriction.

References copy_page(), and NAND_COMMON_ERROR_BADBLOCK.

Referenced by nand_flash_raw_copy_block().

uint32_t nand_flash_raw_erase_block ( const struct nand_flash_raw raw,
uint16_t  block 
)

Erase the specified block of the device, retrying several time if it fails.

Parameters
rawPointer to a nand_flash_raw instance.
blockNumber of the physical block to erase.
Returns
0 if successful; otherwise returns NAND_COMMON_ERROR_BADBLOCK.

References erase_block(), and NAND_COMMON_ERROR_BADBLOCK.

Referenced by main(), run_test_raw_read_write(), and run_test_software_ecc().

uint32_t nand_flash_raw_initialize ( struct nand_flash_raw raw,
const struct nand_flash_model model,
uint32_t  command_address,
uint32_t  address_address,
uint32_t  data_address 
)

Initializes a nand_flash_raw instance based on the given model and physical interface.

Parameters
rawPointer to a nand_flash_raw instance.
modelPointer to the underlying NAND chip model. Can be 0.
command_addressAddress at which commands are sent.
address_addressAddress at which addresses are sent.
data_addressAddress at which data is sent.
Returns
0 if successful; otherwise returns NAND_COMMON_ERROR_UNKNOWNMODEL.

References nand_flash_raw::address_address, ATPASTE2, BOARD_NAND_CS, nand_flash_raw::command_address, CONF_NF_BUSWIDTH, CONF_NF_CYCLE_TIMING, CONF_NF_PULSE_TIMING, CONF_NF_SETUP_TIMING, nand_flash_raw::data_address, data_address, delay_ms, gpio_configure_pin, IOPORT_DIR_INPUT, IOPORT_MODE_PULLUP, ioport_set_pin_dir(), ioport_set_pin_mode(), nand_flash_raw::model, NAND_COMMON_ERROR_UNKNOWNMODEL, nand_flash_model_find(), nand_flash_model_list, NAND_FLASH_MODEL_LIST_SIZE, nand_flash_raw_read_id(), nand_flash_raw_reset(), NF_WP_PIN, PIN_NF_CE_IDX, PIN_NF_RB_IDX, pmc_enable_periph_clk(), smc_set_cycle_timing(), smc_set_mode(), smc_set_pulse_timing(), smc_set_setup_timing(), and sysclk_get_cpu_hz().

Referenced by main(), nand_flash_ecc_initialize(), and run_test_initialization().

uint32_t nand_flash_raw_read_id ( const struct nand_flash_raw raw)

Read and return the identifiers of a NAND Flash chip.

Parameters
rawPointer to a nand_flash_raw instance.
Returns
id1|(id2<<8)|(id3<<16)|(id4<<24)

References delay_us, DISABLE_CE, ENABLE_CE, NAND_COMMAND_READID, READ_DATA8, WRITE_ADDRESS, and WRITE_COMMAND.

Referenced by nand_flash_raw_initialize(), and run_test_initialization().

void nand_flash_raw_read_page ( const struct nand_flash_raw raw,
uint16_t  block,
uint16_t  page,
uint8_t *  data,
uint8_t *  spare 
)

Read the data and/or the spare areas of a page of a NAND Flash into the provided buffers.

Parameters
rawPointer to a nand_flash_raw instance.
blockNumber of the physical block to read.
pageNumber of the page to read inside the given block.
dataBuffer where the data area will be read.
spareBuffer where the spare area will be read.
Note
If one of the buffer pointer is 0, the corresponding area is not read.

References delay_us, DISABLE_CE, ENABLE_CE, MODEL, NAND_COMMAND_READ_1, NAND_COMMAND_READ_2, NAND_COMMAND_READ_A, NAND_COMMAND_READ_C, nand_flash_model_get_block_size_in_pages(), nand_flash_model_get_page_data_size(), nand_flash_model_get_page_spare_size(), nand_flash_model_small_block(), read_data(), wait_ready(), write_column_address(), WRITE_COMMAND, and write_row_address().

Referenced by copy_page(), main(), nand_flash_ecc_read_page(), run_test_raw_read_write(), and run_test_software_ecc().

void nand_flash_raw_reset ( const struct nand_flash_raw raw)

Reset a NAND Flash device.

Parameters
rawPointer to a nand_flash_raw instance.

References DISABLE_CE, ENABLE_CE, NAND_COMMAND_RESET, wait_ready(), and WRITE_COMMAND.

Referenced by nand_flash_raw_initialize().

uint32_t nand_flash_raw_write_page ( const struct nand_flash_raw raw,
uint16_t  block,
uint16_t  page,
uint8_t *  data,
uint8_t *  spare 
)

Write the data and/or the spare areas of a page into a NAND Flash.

Parameters
rawPointer to a nand_flash_raw instance.
blockNumber of the physical block to write resides.
pageNumber of the page to write inside the given block.
dataBuffer where the data area will be stored.
spareBuffer where the spare area will be stored.
Returns
0 if successful; otherwise returns NAND_COMMON_ERROR_BADBLOCK.
Note
If one of the buffer pointer is 0, the corresponding area is not written.

References NAND_COMMON_ERROR_BADBLOCK, and write_page().

Referenced by copy_page(), main(), nand_flash_ecc_write_page(), and run_test_raw_read_write().

static void read_data ( const struct nand_flash_raw raw,
uint8_t *  buffer,
uint32_t  size 
)
static

Read data from the NAND Flash chip into the provided buffer.

Parameters
rawPointer to a nand_flash_raw instance.
bufferPointer to data buffer.
sizeNumber of bytes that will be written.

References MODEL, nand_flash_model_get_data_bus_width(), READ_DATA16, and READ_DATA8.

Referenced by nand_flash_raw_read_page(), and write_page().

static void wait_ready ( void  )
static

Wait for the completion of a page program, erase and random read completion.

References gpio_pin_is_low, and PIN_NF_RB_IDX.

Referenced by copy_page(), erase_block(), nand_flash_raw_read_page(), nand_flash_raw_reset(), and write_page().

static void write_column_address ( const struct nand_flash_raw raw,
uint16_t  column_address 
)
static

Send the column address to the NAND Flash chip.

Parameters
rawPointer to a nand_flash_raw instance.
column_addressColumn address to send.

References MODEL, nand_flash_model_get_data_bus_width(), nand_flash_model_get_page_data_size(), WRITE_ADDRESS, and WRITE_ADDRESS16.

Referenced by copy_page(), nand_flash_raw_read_page(), and write_page().

static void write_data ( const struct nand_flash_raw raw,
uint8_t *  buffer,
uint32_t  size 
)
static

Send data to the NAND Flash chip from the provided buffer.

Parameters
rawPointer to a nand_flash_raw instance.
bufferPointer to data buffer.
sizeNumber of bytes that will be written.

References MODEL, nand_flash_model_get_data_bus_width(), WRITE_DATA16, and WRITE_DATA8.

Referenced by write_page().

static uint32_t write_page ( const struct nand_flash_raw raw,
uint16_t  block,
uint16_t  page,
void *  data,
void *  spare 
)
static

Write the data and/or the spare area of a page on a NAND Flash chip.

Parameters
rawPointer to a nand_flash_raw instance.
blockNumber of the physical block to erase.
pageNumber of the page to write inside the given block.
dataBuffer containing the data area.
spareBuffer containing the spare area.
Returns
0 if successful; otherwise return the error code.
Note
If one of the buffer pointer is 0, the corresponding area is not written.

References check_status(), DISABLE_CE, ENABLE_CE, MODEL, NAND_COMMAND_WRITE_1, NAND_COMMAND_WRITE_2, NAND_COMMON_ERROR_CANNOTWRITE, nand_flash_model_get_block_size_in_pages(), nand_flash_model_get_page_data_size(), nand_flash_model_get_page_spare_size(), read_data(), wait_ready(), write_column_address(), WRITE_COMMAND, write_data(), and write_row_address().

Referenced by nand_flash_raw_write_page().

static void write_row_address ( const struct nand_flash_raw raw,
uint32_t  row_address 
)
static

Send the row address to the NAND Flash chip.

Parameters
rawPointer to a nand_flash_raw instance.
row_addressRow address to send.

References MODEL, nand_flash_model_get_data_bus_width(), nand_flash_model_get_device_size_in_pages(), WRITE_ADDRESS, and WRITE_ADDRESS16.

Referenced by copy_page(), erase_block(), nand_flash_raw_read_page(), and write_page().