Microchip® Advanced Software Framework

nand_flash_spare_scheme.h File Reference

Flash spare area scheme.

This file contains definitions and functions to do NAND Flash device's spare area operations.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

Data Structures

struct  nand_flash_spare_scheme
 

Functions

void nand_flash_spare_scheme_read_bad_block_marker (const struct nand_flash_spare_scheme *scheme, const uint8_t *spare, uint8_t *marker)
 Read the bad block marker inside a spare area buffer using the given scheme. More...
 
void nand_flash_spare_scheme_read_ecc (const struct nand_flash_spare_scheme *scheme, const uint8_t *spare, uint8_t *ecc)
 Read ECC information from a spare area using the given scheme. More...
 
void nand_flash_spare_scheme_read_extra (const struct nand_flash_spare_scheme *scheme, const uint8_t *spare, void *extra, uint8_t size, uint8_t offset)
 Read extra bytes of information from a spare area, using the given scheme. More...
 
void nand_flash_spare_scheme_write_bad_block_marker (const struct nand_flash_spare_scheme *scheme, uint8_t *spare, uint8_t marker)
 Modify the bad block marker inside a spare area, using the given scheme. More...
 
void nand_flash_spare_scheme_write_ecc (const struct nand_flash_spare_scheme *scheme, uint8_t *spare, const uint8_t *ecc)
 Write ECC information in a spare area, using the given scheme. More...
 
void nand_flash_spare_scheme_write_extra (const struct nand_flash_spare_scheme *scheme, uint8_t *spare, const void *extra, uint8_t size, uint8_t offset)
 Write extra bytes of information from a spare area, using the given scheme. More...
 

Variables

struct nand_flash_spare_scheme nand_flash_spare_scheme_2048
 
struct nand_flash_spare_scheme nand_flash_spare_scheme_256
 
struct nand_flash_spare_scheme nand_flash_spare_scheme_4096
 
struct nand_flash_spare_scheme nand_flash_spare_scheme_512
 

void nand_flash_spare_scheme_read_bad_block_marker ( const struct nand_flash_spare_scheme scheme,
const uint8_t *  spare,
uint8_t *  marker 
)

Read the bad block marker inside a spare area buffer using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
markerPointer to the variable to store the bad block marker.

References nand_flash_spare_scheme::bad_block_marker_position.

void nand_flash_spare_scheme_read_ecc ( const struct nand_flash_spare_scheme scheme,
const uint8_t *  spare,
uint8_t *  ecc 
)

Read ECC information from a spare area using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
eccECC buffer.

References nand_flash_spare_scheme::ecc_byte_number, and nand_flash_spare_scheme::ecc_bytes_positions.

Referenced by nand_flash_ecc_read_page().

void nand_flash_spare_scheme_read_extra ( const struct nand_flash_spare_scheme scheme,
const uint8_t *  spare,
void *  extra,
uint8_t  size,
uint8_t  offset 
)

Read extra bytes of information from a spare area, using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
extraExtra bytes buffer.
sizeNumber of extra bytes to read.
offsetIndex where to read the first extra byte.

References Assert, nand_flash_spare_scheme::extra_byte_number, nand_flash_spare_scheme::extra_bytes_positions, and offset.

void nand_flash_spare_scheme_write_bad_block_marker ( const struct nand_flash_spare_scheme scheme,
uint8_t *  spare,
uint8_t  marker 
)

Modify the bad block marker inside a spare area, using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
markerBad block marker to write.

References nand_flash_spare_scheme::bad_block_marker_position.

void nand_flash_spare_scheme_write_ecc ( const struct nand_flash_spare_scheme scheme,
uint8_t *  spare,
const uint8_t *  ecc 
)

Write ECC information in a spare area, using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
eccECC buffer.

References nand_flash_spare_scheme::ecc_byte_number, and nand_flash_spare_scheme::ecc_bytes_positions.

Referenced by nand_flash_ecc_write_page().

void nand_flash_spare_scheme_write_extra ( const struct nand_flash_spare_scheme scheme,
uint8_t *  spare,
const void *  extra,
uint8_t  size,
uint8_t  offset 
)

Write extra bytes of information from a spare area, using the given scheme.

Parameters
schemePointer to a nand_flash_spare_scheme instance.
spareSpare area buffer.
extraExtra bytes buffer to write.
sizeNumber of extra bytes to write.
offsetIndex where to read the first extra byte.

References Assert, nand_flash_spare_scheme::extra_byte_number, nand_flash_spare_scheme::extra_bytes_positions, and offset.

struct nand_flash_spare_scheme nand_flash_spare_scheme_2048
struct nand_flash_spare_scheme nand_flash_spare_scheme_256
struct nand_flash_spare_scheme nand_flash_spare_scheme_4096
struct nand_flash_spare_scheme nand_flash_spare_scheme_512