Microchip® Advanced Software Framework

usb/sio2host.c File Reference
#include "conf_sio2host.h"
#include "sio2host.h"
#include "stdio_usb.h"

Functions

void dtr_cb (bool set)
 This function is callled with the value set as true whenever a device is connected to the terminal. More...
 
void main_cdc_disable (uint8_t port)
 Closes the communication port This is called by CDC interface when USB Host disable it. More...
 
bool main_cdc_enable (uint8_t port)
 Opens the communication port This is called by CDC interface when USB Host enable it. More...
 
uint8_t sio2host_getchar (void)
 This function performs a blocking character receive functionality. More...
 
int sio2host_getchar_nowait (void)
 This function performs a non-blocking character receive functionality. More...
 
void sio2host_init (void)
 Initializes the Serial IO Module. More...
 
void sio2host_putchar (uint8_t ch)
 This function prints the character to the host. More...
 
uint8_t sio2host_rx (uint8_t *data, uint8_t max_length)
 Receives data from UART. More...
 
uint8_t sio2host_tx (uint8_t *data, uint8_t length)
 Transmits data via UART. More...
 
void usb_rx_notify (void)
 This function is called by the USB data receive Interrupt The Receive buffer is filled in this function. More...
 

Variables

static volatile bool main_b_cdc_enable = false
 
static uint8_t serial_rx_buf [SERIAL_RX_BUF_SIZE_HOST]
 Receive buffer The buffer size is defined in sio2host.h. More...
 
static uint8_t serial_rx_buf_head
 Receive buffer head. More...
 
static uint8_t serial_rx_buf_tail
 Receive buffer tail. More...
 
static uint8_t serial_rx_count
 Number of bytes in receive buffer. More...
 
static volatile bool usb_rx_byte_rcvd = false
 

void main_cdc_disable ( uint8_t  port)

Closes the communication port This is called by CDC interface when USB Host disable it.

References main_b_cdc_enable.

bool main_cdc_enable ( uint8_t  port)

Opens the communication port This is called by CDC interface when USB Host enable it.

Called by CDC interface Callback running when USB Host enable CDC interface.

Return values
trueif cdc startup is successfully done

References main_b_cdc_enable.

volatile bool main_b_cdc_enable = false
static
uint8_t serial_rx_buf[SERIAL_RX_BUF_SIZE_HOST]
static

Receive buffer The buffer size is defined in sio2host.h.

Referenced by sio2host_rx(), and usb_rx_notify().

uint8_t serial_rx_buf_head
static

Receive buffer head.

Referenced by sio2host_rx().

uint8_t serial_rx_buf_tail
static

Receive buffer tail.

Referenced by sio2host_rx(), and usb_rx_notify().

uint8_t serial_rx_count
static

Number of bytes in receive buffer.

Referenced by sio2host_rx(), and usb_rx_notify().

volatile bool usb_rx_byte_rcvd = false
static