Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
xEventGroupWaitBits

event_groups.h

    EventBits_t xEventGroupWaitBits(    EventGroupHandle_t xEventGroup,
                                        const EventBits_t uxBitsToWaitFor,
                                        const BaseType_t xClearOnExit,
                                        const BaseType_t xWaitForAllBits,
                                        const TickType_t xTicksToWait );
 

[Potentially] block to wait for one or more bits to be set within a previously created event group.

This function cannot be called from an interrupt.

Parameters
xEventGroupThe event group in which the bits are being tested. The event group must have previously been created using a call to xEventGroupCreate().
uxBitsToWaitForA bitwise value that indicates the bit or bits to test inside the event group. For example, to wait for bit 0 and/or bit 2 set uxBitsToWaitFor to 0x05. To wait for bits 0 and/or bit 1 and/or bit 2 set uxBitsToWaitFor to 0x07. Etc.
xClearOnExitIf xClearOnExit is set to pdTRUE then any bits within uxBitsToWaitFor that are set within the event group will be cleared before xEventGroupWaitBits() returns if the wait condition was met (if the function returns for a reason other than a timeout). If xClearOnExit is set to pdFALSE then the bits set in the event group are not altered when the call to xEventGroupWaitBits() returns.
xWaitForAllBitsIf xWaitForAllBits is set to pdTRUE then xEventGroupWaitBits() will return when either all the bits in uxBitsToWaitFor are set or the specified block time expires. If xWaitForAllBits is set to pdFALSE then xEventGroupWaitBits() will return when any one of the bits set in uxBitsToWaitFor is set or the specified block time expires. The block time is specified by the xTicksToWait parameter.
xTicksToWaitThe maximum amount of time (specified in 'ticks') to wait for one/all (depending on the xWaitForAllBits value) of the bits specified by uxBitsToWaitFor to become set.
Returns
The value of the event group at the time either the bits being waited for became set, or the block time expired. Test the return value to know which bits were set. If xEventGroupWaitBits() returned because its timeout expired then not all the bits being waited for will be set. If xEventGroupWaitBits() returned because the bits it was waiting for were set then the returned value is the event group value before any bits were automatically cleared in the case that xClearOnExit parameter was set to pdTRUE.

Example usage:

   #define BIT_0    ( 1 << 0 )
   #define BIT_4    ( 1 << 4 )
   void aFunction( EventGroupHandle_t xEventGroup )
   {
   EventBits_t uxBits;
   const TickType_t xTicksToWait = 100 / portTICK_PERIOD_MS;
Wait a maximum of 100ms for either bit 0 or bit 4 to be set within
the event group.  Clear the bits before exiting.
        uxBits = xEventGroupWaitBits(
                    xEventGroup,    // The event group being tested.
                    BIT_0 | BIT_4,  // The bits within the event group to wait for.
                    pdTRUE,         // BIT_0 and BIT_4 should be cleared before returning.
                    pdFALSE,        // Don't wait for both bits, either bit will do.
                    xTicksToWait ); // Wait a maximum of 100ms for either bit to be set.
        if( ( uxBits & ( BIT_0 | BIT_4 ) ) == ( BIT_0 | BIT_4 ) )
        {
xEventGroupWaitBits() returned because both bits were set.
        }
        else if( ( uxBits & BIT_0 ) != 0 )
        {
xEventGroupWaitBits() returned because just BIT_0 was set.
        }
        else if( ( uxBits & BIT_4 ) != 0 )
        {
xEventGroupWaitBits() returned because just BIT_4 was set.
        }
        else
        {
xEventGroupWaitBits() returned because xTicksToWait ticks passed
without either BIT_0 or BIT_4 becoming set.
        }
   }
   
 EventGroupHandle_t xEventGroupCreateStatic( EventGroupHandle_t * pxEventGroupBuffer );
 

Create a new event group.

Internally, within the FreeRTOS implementation, event groups use a [small] block of memory, in which the event group's structure is stored. If an event groups is created using xEventGropuCreate() then the required memory is automatically dynamically allocated inside the xEventGroupCreate() function. (see http://www.freertos.org/a00111.html). If an event group is created using xEventGropuCreateStatic() then the application writer must instead provide the memory that will get used by the event group. xEventGroupCreateStatic() therefore allows an event group to be created without using any dynamic memory allocation.

Although event groups are not related to ticks, for internal implementation reasons the number of bits available for use in an event group is dependent on the configUSE_16_BIT_TICKS setting in FreeRTOSConfig.h. If configUSE_16_BIT_TICKS is 1 then each event group contains 8 usable bits (bit 0 to bit 7). If configUSE_16_BIT_TICKS is set to 0 then each event group has 24 usable bits (bit 0 to bit 23). The EventBits_t type is used to store event bits within an event group.

Parameters
pxEventGroupBufferpxEventGroupBuffer must point to a variable of type StaticEventGroup_t, which will be then be used to hold the event group's data structures, removing the need for the memory to be allocated dynamically.
Returns
If the event group was created then a handle to the event group is returned. If pxEventGroupBuffer was NULL then NULL is returned.

Example usage:

StaticEventGroup_t is a publicly accessible structure that has the same
size and alignment requirements as the real event group structure.  It is
provided as a mechanism for applications to know the size of the event
group (which is dependent on the architecture and configuration file
settings) without breaking the strict data hiding policy by exposing the
real event group internals.  This StaticEventGroup_t variable is passed
into the xSemaphoreCreateEventGroupStatic() function and is used to store
the event group's data structures
    StaticEventGroup_t xEventGroupBuffer;
Create the event group without dynamically allocating any memory.
    xEventGroup = xEventGroupCreateStatic( &xEventGroupBuffer );
   

event_groups.h

    EventBits_t xEventGroupWaitBits(    EventGroupHandle_t xEventGroup,
                                        const EventBits_t uxBitsToWaitFor,
                                        const BaseType_t xClearOnExit,
                                        const BaseType_t xWaitForAllBits,
                                        const TickType_t xTicksToWait );
 

[Potentially] block to wait for one or more bits to be set within a previously created event group.

This function cannot be called from an interrupt.

Parameters
xEventGroupThe event group in which the bits are being tested. The event group must have previously been created using a call to xEventGroupCreate().
uxBitsToWaitForA bitwise value that indicates the bit or bits to test inside the event group. For example, to wait for bit 0 and/or bit 2 set uxBitsToWaitFor to 0x05. To wait for bits 0 and/or bit 1 and/or bit 2 set uxBitsToWaitFor to 0x07. Etc.
xClearOnExitIf xClearOnExit is set to pdTRUE then any bits within uxBitsToWaitFor that are set within the event group will be cleared before xEventGroupWaitBits() returns if the wait condition was met (if the function returns for a reason other than a timeout). If xClearOnExit is set to pdFALSE then the bits set in the event group are not altered when the call to xEventGroupWaitBits() returns.
xWaitForAllBitsIf xWaitForAllBits is set to pdTRUE then xEventGroupWaitBits() will return when either all the bits in uxBitsToWaitFor are set or the specified block time expires. If xWaitForAllBits is set to pdFALSE then xEventGroupWaitBits() will return when any one of the bits set in uxBitsToWaitFor is set or the specified block time expires. The block time is specified by the xTicksToWait parameter.
xTicksToWaitThe maximum amount of time (specified in 'ticks') to wait for one/all (depending on the xWaitForAllBits value) of the bits specified by uxBitsToWaitFor to become set.
Returns
The value of the event group at the time either the bits being waited for became set, or the block time expired. Test the return value to know which bits were set. If xEventGroupWaitBits() returned because its timeout expired then not all the bits being waited for will be set. If xEventGroupWaitBits() returned because the bits it was waiting for were set then the returned value is the event group value before any bits were automatically cleared in the case that xClearOnExit parameter was set to pdTRUE.

Example usage:

   #define BIT_0    ( 1 << 0 )
   #define BIT_4    ( 1 << 4 )
   void aFunction( EventGroupHandle_t xEventGroup )
   {
   EventBits_t uxBits;
   const TickType_t xTicksToWait = 100 / portTICK_PERIOD_MS;
Wait a maximum of 100ms for either bit 0 or bit 4 to be set within
the event group.  Clear the bits before exiting.
        uxBits = xEventGroupWaitBits(
                    xEventGroup,    // The event group being tested.
                    BIT_0 | BIT_4,  // The bits within the event group to wait for.
                    pdTRUE,         // BIT_0 and BIT_4 should be cleared before returning.
                    pdFALSE,        // Don't wait for both bits, either bit will do.
                    xTicksToWait ); // Wait a maximum of 100ms for either bit to be set.
        if( ( uxBits & ( BIT_0 | BIT_4 ) ) == ( BIT_0 | BIT_4 ) )
        {
xEventGroupWaitBits() returned because both bits were set.
        }
        else if( ( uxBits & BIT_0 ) != 0 )
        {
xEventGroupWaitBits() returned because just BIT_0 was set.
        }
        else if( ( uxBits & BIT_4 ) != 0 )
        {
xEventGroupWaitBits() returned because just BIT_4 was set.
        }
        else
        {
xEventGroupWaitBits() returned because xTicksToWait ticks passed
without either BIT_0 or BIT_4 becoming set.
        }
   }