License | Copyright (c) 2017-2018 Microchip Technology Inc |
Extra Information for Parallel Capture | |
Examples for Parallel Capture | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM4L Parallel Capture (PARC) Driver |
 Quick Start Guide for the PARC driver | This is the quick start guide for the SAM4L Parallel Capture (PARC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Parallel Capture (PARC) - Example Using GPIO as Stimuli | |
Document Revision History | |
License | Copyright (c) 2014-2018 Microchip Technology Inc |
Quick start guide for USB device mouse module (UDI mouse) | This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID mouse in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quickstart guide for SAM SPI driver | This is the quickstart guide for the SAM SPI driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the HMATRIX driver | This is the quick start guide for the HSB BUS Matrix (HMATRIX), with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the HMATRIX module |
Quick start guide for First-In-First-Out Buffer (FIFO) | This is the quick start guide for the First-In-First-Out Buffer (FIFO), with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Push and flush | In this use case, two elements will be pushed to the FIFO, and the FIFO will be flushed |
Quick Start Guide for the SPI Master Driver | This is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Basic setup for SPI master on XMEGA devices | |
Extra Information for Timer Counter Driver | |
Examples for Timer Counter | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver |
 Quick Start Guide for the TC driver | This is the quick start guide for the SAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Timer Counter Capture Waveform Example | |
Document Revision History | |
Extra Information for EIC | |
Quickstart guide for SAM EIC driver | This is the quickstart guide for the SAM4L External Interrupt Controller (EIC) Driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Document Revision History | |
Extra Information for GPIO | |
Examples for GPIO | This is a list of the available Quick Start guides (QSGs) and example applications for SAM4L General-Purpose Input/Output (GPIO) Driver |
Document Revision History | |
Quick Start Guide for the GPIO driver | This is the quick start guide for the group_sam_drivers_gpio, with step-by-step instructions on how to configure and use the driver for a specific use case |
Example | |
Quick Start Guide for the C42364A | LCD Glass component |
Quick start guide for USB device Mass Storage module (UDI MSC) | This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 MSC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Extra Information for Liquid Crystal Display Controller Driver | |
Examples for Liquid Crystal Display Controller | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM4L Liquid Crystal Display (LCDCA) Driver |
 Quick Start Guide for the LCDCA Driver | This is the quick start guide for the SAM4L Liquid Crystal Display (LCDCA) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Liquid Crystal Controller - Example Interfacing to a C42048A Display | |
Document Revision History | |
conf_clock.h examples with USB support | Content of XMEGA conf_clock.h: |
Quick start guide for USB device multi-touch module (UDI Multi-touch) | |
Quick start guide for USB Device Vendor module (UDI Vendor) | This is the quick start guide for the USB device interface Vendor module (UDI Vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Vendor in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quickstart guide for SAM PDCA driver | This is the quickstart guide for the SAM PDCA driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the ILI93XX | LCD Glass component |
Quick start guide for USB host mass-storage module (UHI MSC) | This is the quick start guide for the USB host mass-storage module (UHI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quickstart guide for SAM TWIS driver | This is the quickstart guide for the SAM TWIS driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for the SAM USART module | This is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 USART receive character and echo back | In this use case, the USART module is configured for: |
 USART receive character and echo back via interrupts | In this use case, the USART module is configured for: |
Quick Start Guide for the C42412A | LCD Glass component |
Quick start guide for Serial Interface service | This is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases |
 Advanced use case - Send a packet of serial data | In this use case, the USART module is configured for: |
Quickstart guide for SAM FLASHCALW driver | This is the quickstart guide for the SAM FLASHCALW driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the System Clock Management service (SAM4L) | This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases |
Quick start guide for the SAM BPM module | This is the quick start guide for the BPM Module, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Advanced use case - Switch Power Scaling Modes | In this use case, the BPM module can switch the power scaling modes of the system |
Quick start guide for the common IOPORT service | This is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases |
 Advanced use case doing port access | In this case we will read out the pins from one whole port and write the read value to another port |
Quickstart guide for SAM4L watchdog driver | This is the quickstart guide for the SAM4L watchdog driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the GLOC driver | This is the quick start guide for the Glue Logic Controller (GLOC), with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the GLOC module |
Quick start guide for USB host Communication Device Class module (UHI CDC) | This is the quick start guide for the USB host Communication Device Class module (UHI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Extra Information for Asynchronous Timer Driver | |
Examples for Asynchronous Timer Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM4L Asynchronous Timer (AST) Driver |
 Quick Start Guide for the AST driver | This is the quick start guide for the SAM4L Asynchronous Timer (AST) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into the main application loop or any other function that will need to control the AST module |
 Asynchronous Timer (AST) - Example 1 Calendar Mode | |
 Asynchronous Timer (AST) - Example 2 Alarm Wakeup | |
Document Revision History | |
Quick start guide for USB host mouse module (UHI mouse) | This is the quick start guide for the USB host mouse module (UHI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quick Start Guide for the SAM4L IIS driver | This is the quickstart guide for the SAM4L Inter-IC Sound Controller driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick start guide for USB device keyboard module (UDI keyboard) | This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID keyboard in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
uxQueueMessagesWaiting | Queue |
vQueueDelete | Queue |
vSemaphoreDelete | Semphr |
xTaskHandle | Task |
taskYIELD | Task |
taskENTER_CRITICAL | Task |
taskEXIT_CRITICAL | Task |
taskDISABLE_INTERRUPTS | Task |
taskENABLE_INTERRUPTS | Task |
xTaskGetTickCount | Task |
uxTaskGetNumberOfTasks | Task |
pcTaskGetTaskName | Task |
vTaskList | Task |
vTaskGetRunTimeStats | Task |
vTaskStartTrace | Task |
usTaskEndTrace | Task |
Quickstart guide for AT25DFx component. | This is the quickstart guide for the AT25DFx SerialFlash component, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the ABDAC driver | This is the quick start guide for the group_sam_drivers_abdac, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the ABDAC module |
Quick start guide for USB device Communication Class Device module (UDI CDC) | This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 CDC in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quick start guide for reset cause service | This is the quick start guide for the Reset Cause service, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Use case #1 | In this use case, the reset cause service is used to perform a software controlled reset |
death.c | Create a single persistent task which periodically dynamically creates another two tasks |
Quick Start Guide for the AES driver | This is the quick start guide for the group_sam_drivers_aes, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the AES module |
Quick Start Guide for the PICOUART driver | This is the quick start guide for the PICOUART - Picopower UART, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the PICOUART module |
Quick start guide for USB host vendor module (UHI vendor) | This is the quick start guide for the USB host vendor module (UHI vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 Enable USB high speed support | In this use case, the USB host is used to support USB high speed |
 Multiple classes support | In this use case, the USB host is used to support several USB classes |
 Dual roles support | In this use case, the USB host and USB device are enabled, it is the dual role |
Quick start guide for QTouch component | This is the quick start guide for the QTouch device driver for I2C interface, with step-by-step instructions on how to configure and use the driver for a specific use case |
Extra Information for Analog Comparator Interface Driver | |
Examples for Analog Comparator Interface | This is a list of the available Quick Start guides (QSGs) and example applications for SAM4L Analog Comparator Interface Controller (ACIFC) Driver |
 Quick Start Guide for SAM4L Analog Comparator Driver | This is the quick start guide for the SAM4L Analog Comparator Interface Controller (ACIFC) Driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
 Analog Comparator Interface Controller - Example Using Comparison Interrupt | |
Document Revision History | |
Quick start guide for USB device generic module (UDI generic) | This is the quick start guide for the USB device generic module (UDI generic) with step-by-step instructions on how to configure and use the modules in a selection of use cases |
 HID generic in a composite device | A USB Composite Device is a USB Device which uses more than one USB class |
 Change USB speed | In this use case, the USB device is used with different USB speeds |
 Use USB strings | In this use case, the usual USB strings is added in the USB device |
 Use USB remote wakeup feature | In this use case, the USB remote wakeup feature is enabled |
 Bus power application recommendations | In this use case, the USB device BUS power feature is enabled |
 USB dynamic serial number | In this use case, the USB serial strings is dynamic |
Quickstart guide for Common service TWI | This is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Quick Start Guide for the TWIM driver | This is the quick start guide for the TWIM - Two-Wire Master Interface, with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the TWIM module |
Quickstart guide for SAM ADCIFE driver | This is the quickstart guide for the SAM ADCIFE driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
conf_clock.h examples with USB support | Content of conf_clock.h for AT32UC3A0, AT32UC3A1, AT32UC3B devices (USBB): |
Extra Information for Peripheral Event Controller Driver | |
Examples for Peripheral Event Controller Driver | This is a list of the available Quick Start Guides (QSGs) and example applications for SAM4L Peripheral Event Controller (PEVC) Driver |
 Quick Start Guide for the Peripheral Event Controller Driver | This is the quick start guide for the SAM4L Peripheral Event Controller (PEVC) Driver, with step-by-step instructions on how to configure and use the driver for a specific use case |
 Example for the Peripheral Event System - AST/PDCA | |
 Example for the Peripheral Event System - GPIO/PDCA | |
Quickstart guide for SAM FREQM driver | This is the quickstart guide for the SAM FREQM driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases |
Todo List | |
Deprecated List | |