This is the quick start guide for the HSB BUS Matrix (HMATRIX), with step-by-step instructions on how to configure and use the driver for a specific use case.The code examples can be copied into e.g the main application loop or any other function that will need to control the HMATRIX module.
This use case will demonstrate how to configurate the HMATRIX module to set the slave with different default master type.
This module requires the following service
Add this to the main loop or a setup function:
We can set priority of each master for one slave by