#include <stdlib.h>
#include "tal.h"
#include "tal_constants.h"
#include "tal_helper.h"
#include "ieee_const.h"
#include "sio2host.h"
#include "app_frame_format.h"
#include "app_init.h"
#include "app_peer_search.h"
#include "perf_api.h"
Macros | |
#define | CONFIG_MODE_TX_PWR (0xB5) |
Lowest power -11 dBm. More... | |
#define | MAX_NUMBER_PEER_REQ_RETRY (0xFF) |
#define | PEER_REQUEST_SEND_INTERVAL_IN_MICRO_SEC (50000) |
Enumerations | |
enum | peer_search_initiator_state_t { PEER_REQ_SEND, PEER_RSP_RCVD, NUM_PEER_SEARCH_INITIATOR_STATES, PEER_REQ_SEND, PEER_RSP_RCVD, NUM_PEER_SEARCH_INITIATOR_STATES } |
Functions | |
static void | app_peer_req_tmr_handler_cb (void *parameter) |
Timer handler for supporting peer search. More... | |
static void | peer_req_send_exit () |
function to exit peer req send state More... | |
static void | peer_req_send_rx_cb (frame_info_t *mac_frame_info) |
Callback that is called if data has been received by trx in PEER_REQ_SEND State. More... | |
static void | peer_req_send_task () |
Application task handling peer request send. More... | |
static void | peer_rsp_rcvd_exit () |
Function to exit the peer rsp rcvd state. More... | |
static void | peer_rsp_rcvd_init (void *arg) |
Peer rsp received state init function. More... | |
static void | peer_rsp_rcvd_tx_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in peer rsp rcvd state. More... | |
void | peer_search_initiator_exit () |
Function to exit peer search initiator exit state. More... | |
void | peer_search_initiator_init (void *arg) |
Application task to start peer search. More... | |
void | peer_search_initiator_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx. More... | |
void | peer_search_initiator_set_sub_state (uint8_t state, void *arg) |
Function to set the sub state of state machine. More... | |
void | peer_search_initiator_task () |
Application task handling peer search. More... | |
void | peer_search_initiator_tx_done_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in peer search initiator state. More... | |
static retval_t | send_peer_conf (void) |
Send the peer confirmation confirming the node which has been connected This frame is sent as a unicast to peer node. More... | |
static retval_t | send_peer_req (void) |
Send peer search request. More... | |
Variables | |
static peer_state_function_t const | peer_search_initiator_state_table [NUM_PEER_SEARCH_INITIATOR_STATES] |
static uint8_t | seq_num |