Microchip® Advanced Software Framework

nlme_set_conf_tag Struct Reference

NLME-SET.confirm message structure.

#include <nwk_msg_types.h>

Data Fields

nwk_msg_code_t cmdcode ALIGN8BIT
 This identifies the message as NLME_SET_CONFIRM. More...
 
nwk_enum_t Status ALIGN8BIT
 The result of the request to write the MAC PIB attribute. More...
 
nib_attribute_t NIBAttribute ALIGN8BIT
 The identifier of the MAC PIB attribute that was written. More...
 
uint8_t NIBAttributeIndex ALIGN8BIT