NLME-SET.request message structure.
#include <nwk_msg_types.h>
Data Fields | |
nwk_msg_code_t cmdcode | ALIGN8BIT |
This identifies the message as NLME_SET_REQUEST. More... | |
nib_attribute_t NIBAttribute | ALIGN8BIT |
The identifier of the MAC PIB attribute to set. More... | |
uint8_t NIBAttributeIndex | ALIGN8BIT |
uint8_t value[1] | ALIGN8BIT |
The value to write to the indicated MAC PIB attribute. More... | |