API driver for component ADS7843.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "ads7843.h"
#include "conf_ads7843.h"
#include "board.h"
#include "ioport.h"
#include "pio_handler.h"
#include "pio.h"
#include "spi_master.h"
#include "conf_spi_master.h"
Macros | |
#define | ADS7843_BUFSIZE 3 |
#define | ADS7843_SPI_BAUDRATE 1000000 |
Frequence rate for sending one bit. More... | |
#define | ADS7843_TIMEOUT 5000000 |
#define | ADS_CTRL_DFR (1 << 2) |
SER/DFR. More... | |
#define | ADS_CTRL_EIGHT_BITS_MOD (1 << 3) |
Mode. More... | |
#define | ADS_CTRL_PD0 (1 << 0) |
PD0. More... | |
#define | ADS_CTRL_PD1 (1 << 1) |
PD1. More... | |
#define | ADS_CTRL_START (1 << 7) |
Start Bit. More... | |
#define | ADS_CTRL_SWITCH_SHIFT 4 |
Address setting. More... | |
#define | CMD_ENABLE_PENIRQ ((1 << ADS_CTRL_SWITCH_SHIFT) | ADS_CTRL_START) |
Enable penIRQ. More... | |
#define | CMD_X_POSITION |
Get Y position command. More... | |
#define | CMD_Y_POSITION |
Get X position command. More... | |
#define | DELAY_BEFORE_SPCK 200 |
2us min (tCSS) <=> 200/100 000 000 = 2us More... | |
#define | DELAY_BETWEEN_CONS_COM 0xf |
5us min (tCSH) <=> (32 * 15) / (100 000 000) = 5us More... | |
Functions | |
void | ads7843_disable_interrupt (void) |
Disable interrupts on touch event. More... | |
void | ads7843_enable_interrupt (void) |
Enable interrupts on touch event. More... | |
void | ads7843_get_raw_point (uint32_t *p_x, uint32_t *p_y) |
Get the touch raw coordinates. More... | |
uint32_t | ads7843_init (void) |
Initialize the SPI communication with the ADS7843 controller. More... | |
uint32_t | ads7843_is_pressed (void) |
Return the touch screen status, pressed or not. More... | |
static uint32_t | ads7843_send_cmd (uint8_t uc_cmd) |
Send a command to the ADS7843 touch controller. More... | |
void | ads7843_set_handler (void(*p_handler)(uint32_t, uint32_t)) |
Set the touch interrupt handler. More... | |
#define ADS7843_BUFSIZE 3 |
Referenced by ads7843_send_cmd().
#define ADS7843_SPI_BAUDRATE 1000000 |
Frequence rate for sending one bit.
Referenced by ads7843_init().
#define ADS7843_TIMEOUT 5000000 |
#define ADS_CTRL_DFR (1 << 2) |
SER/DFR.
#define ADS_CTRL_EIGHT_BITS_MOD (1 << 3) |
Mode.
#define ADS_CTRL_PD0 (1 << 0) |
PD0.
#define ADS_CTRL_PD1 (1 << 1) |
PD1.
#define ADS_CTRL_START (1 << 7) |
Start Bit.
#define ADS_CTRL_SWITCH_SHIFT 4 |
Address setting.
#define CMD_ENABLE_PENIRQ ((1 << ADS_CTRL_SWITCH_SHIFT) | ADS_CTRL_START) |
Enable penIRQ.
Referenced by ads7843_get_raw_point(), and ads7843_init().
#define CMD_X_POSITION |
Get Y position command.
Referenced by ads7843_get_raw_point().
#define CMD_Y_POSITION |
Get X position command.
Referenced by ads7843_get_raw_point().
#define DELAY_BEFORE_SPCK 200 |
2us min (tCSS) <=> 200/100 000 000 = 2us
#define DELAY_BETWEEN_CONS_COM 0xf |
5us min (tCSH) <=> (32 * 15) / (100 000 000) = 5us
|
static |
Send a command to the ADS7843 touch controller.
uc_cmd | command to send. |
(volatile declaration needed for code optimisation by compiler)
References ADS7843_BUFSIZE, data, SPI_ERROR_TIMEOUT, spi_is_rx_full(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, and spi_write_single().
Referenced by ads7843_get_raw_point(), and ads7843_init().