#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "tal_config.h"
#include "tal_internal.h"
#include "mac_build_config.h"
Macros | |
#define | LOWER_ED_LIMIT -100 |
#define | UPPER_ED_LIMIT -30 |
Values used for ED scaling in dBm. More... | |
Functions | |
void | handle_ed_end_irq (trx_id_t trx_id) |
The peak_ed_level is the maximum ED value received from the transceiver for the specified Scan Duration. More... | |
uint8_t | scale_ed_value (int8_t ed) |
Scale ED value. More... | |
void | set_ed_sample_duration (trx_id_t trx_id, uint16_t sample_duration_us) |
Sets the energy measurement duration. More... | |
#define LOWER_ED_LIMIT -100 |
Referenced by scale_ed_value().
#define UPPER_ED_LIMIT -30 |
Values used for ED scaling in dBm.
Referenced by scale_ed_value().
void handle_ed_end_irq | ( | trx_id_t | trx_id | ) |
The peak_ed_level is the maximum ED value received from the transceiver for the specified Scan Duration.
Starts ED Scan
This function starts an ED Scan for the scan duration specified by the MAC layer. The result is returned from the TAL by calling tal_ed_end_cb().
trx_id | Transceiver identifier |
scan_duration | Specifies the ED scan duration in superframe duration |
This function handles an ED done interrupt from the transceiver.
trx_id | Transceiver identifier |
References cca_done_handling(), RF_BASE_ADDR_OFFSET, RF_EDAUTO, RF_RX, RF_TRXOFF, RG_RF09_CMD, RG_RF09_EDV, set_ed_sample_duration(), SR_BBC0_PC_BBEN, SR_RF09_EDC_EDM, SR_RF09_IRQM_EDC, switch_to_rx(), tal_current_ed_val, tal_ed_end_cb(), TAL_ED_SCAN, TAL_IDLE, tal_pib, tal_state, trx_default_state, and tx_state.
Referenced by tal_task().
uint8_t scale_ed_value | ( | int8_t | ed | ) |
Scale ED value.
This function scales the trx ED value to the range 0x00 - 0xFF.
ed | RF215 register value EDV. |
References LOWER_ED_LIMIT, and UPPER_ED_LIMIT.
Referenced by process_incoming_frame().
void set_ed_sample_duration | ( | trx_id_t | trx_id, |
uint16_t | sample_duration_us | ||
) |
Sets the energy measurement duration.
trx_id | Transceiver identifier |
sample_duration_us | Sample duration in us |
References RF_BASE_ADDR_OFFSET, and RG_RF09_EDD.
Referenced by config_phy(), handle_ed_end_irq(), and tal_pib_set().