Declaration of main function used by CDC unit test.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_cdc_config (void) |
Called by UDI interface Callback running when USB Host send a port configuration. More... | |
void | main_cdc_disable (void) |
Called by UDI interface Callback running when USB Host disable CDC interface. More... | |
bool | main_cdc_enable (void) |
Called by UDI interface Callback running when USB Host enable CDC interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vbus_action (bool b_high) |
Called when Vbus line state change. More... | |
void main_cdc_config | ( | void | ) |
Called by UDI interface Callback running when USB Host send a port configuration.
References main_b_cdc_configurated.
void main_cdc_disable | ( | void | ) |
Called by UDI interface Callback running when USB Host disable CDC interface.
References main_b_cdc_enumerated.
bool main_cdc_enable | ( | void | ) |
Called by UDI interface Callback running when USB Host enable CDC interface.
true | if CDC startup is ok |
References main_b_cdc_enumerated.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
Called by UDC when USB Host request to disable remote wakeup.
This is called by the USB stack when the host requests remote wake-up to be disabled, and will request the user interface to disable wake-up.
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
Called by UDC when USB Host request to enable remote wakeup.
This is called by the USB stack when the host requests remote wake-up to be enabled, and will request the user interface to enable wake-up.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Called by UDD when the USB line exit of suspend state.
Called by USB stack when the bus resumes from suspend.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Called when a start of frame is received on USB line.
Called by USB stack when a start of frame is received, i.e., every millisecond during normal operation. This function triggers processing of the user interface if the HID interface has been enabled.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by USB stack when host suspends the bus.
void main_vbus_action | ( | bool | b_high | ) |
Called when Vbus line state change.