Main functions for CDC unit test.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdio.h>
#include <asf.h>
#include <unit_test/suite.h>
#include <stdio_serial.h>
#include <conf_test.h>
Functions | |
int | main (void) |
Run usb device cdc unit tests. More... | |
void | main_cdc_config (void) |
Called by UDI interface Callback running when USB Host send a port configuration. More... | |
void | main_cdc_disable (void) |
Called by UDI interface Callback running when USB Host disable CDC interface. More... | |
bool | main_cdc_enable (void) |
Called by UDI interface Callback running when USB Host enable CDC interface. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | main_vbus_action (bool b_high) |
Called when Vbus line state change. More... | |
static void | run_usb_cdc_config_test (const struct test_case *test) |
static void | run_usb_cdc_test (const struct test_case *test) |
static void | run_usb_resume_test (const struct test_case *test) |
static void | run_usb_sof_test (const struct test_case *test) |
static void | run_usb_suspend_test (const struct test_case *test) |
static void | run_usb_vbus_test (const struct test_case *test) |
Variables | |
static bool | main_b_cdc_configurated = false |
static bool | main_b_cdc_enumerated = false |
static bool | main_b_resume_event = false |
static bool | main_b_sof_event = false |
static bool | main_b_suspend_event = false |
static bool | main_b_vbus_event = false |
int main | ( | void | ) |
Run usb device cdc unit tests.
Initializes the clock system, board and serial output, then sets up the usb unit test suite and runs it.
References uart_rs232_options::baudrate, board_init(), cpu_irq_enable, DEFINE_TEST_ARRAY, DEFINE_TEST_CASE, DEFINE_TEST_SUITE, irq_initialize_vectors, NULL, run_usb_cdc_config_test(), run_usb_cdc_test(), run_usb_resume_test(), run_usb_sof_test(), run_usb_suspend_test(), run_usb_vbus_test(), SLEEPMGR_ACTIVE, sleepmgr_init(), sleepmgr_lock_mode(), stdio_serial_init(), sysclk_init(), test_suite_run(), and usart_serial_options.
void main_cdc_config | ( | void | ) |
Called by UDI interface Callback running when USB Host send a port configuration.
References main_b_cdc_configurated.
void main_cdc_disable | ( | void | ) |
Called by UDI interface Callback running when USB Host disable CDC interface.
References main_b_cdc_enumerated.
bool main_cdc_enable | ( | void | ) |
Called by UDI interface Callback running when USB Host enable CDC interface.
true | if CDC startup is ok |
References main_b_cdc_enumerated.
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
References main_b_suspend_event.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
References main_b_sof_event.
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
Turn off all leds Callback running when USB Host set USB line in suspend state.
References main_b_resume_event.
void main_vbus_action | ( | bool | b_high | ) |
Called when Vbus line state change.
References main_b_vbus_event.
|
static |
References main_b_cdc_configurated, and test_assert_true.
Referenced by main().
|
static |
References main_b_cdc_configurated, main_b_cdc_enumerated, main_vbus_action(), sleepmgr_enter_sleep(), udc_include_vbus_monitoring(), udc_start(), udc_stop(), and UNUSED.
Referenced by main().
|
static |
References main_b_resume_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_sof_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_suspend_event, and test_assert_true.
Referenced by main().
|
static |
References main_b_vbus_event, and test_assert_true.
Referenced by main().
Referenced by main_cdc_config(), run_usb_cdc_config_test(), and run_usb_cdc_test().
Referenced by main_cdc_disable(), main_cdc_enable(), and run_usb_cdc_test().
Referenced by main_suspend_action(), and run_usb_resume_test().
Referenced by main_sof_action(), and run_usb_sof_test().
Referenced by main_resume_action(), and run_usb_suspend_test().
Referenced by main_vbus_action(), and run_usb_vbus_test().