Eddystone Beacons Support.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
union | beacon_id_t |
Eddystone-UID beacon structure. More... | |
struct | eddystone_tlm_data_t |
Eddystone-TLM frame data. More... | |
struct | esurl_conf_gatt_service_t |
URL configuration service GATT characteristics. More... | |
Macros | |
#define | EDDYSTONE_16_BIT_UUID 0xFEAA |
16-bit Eddystone Service UUID More... | |
#define | EDDYSTONE_BEACON_INTERVAL_MS_MAX (10240) |
Maximum beacon interval in ms (10240ms or 10.24s) More... | |
#define | EDDYSTONE_BEACON_INTERVAL_MS_MIN (100) |
Minimum beacon interval in ms (100ms) More... | |
#define | EDDYSTONE_TLM_FRAME_VERSION (0x00) |
Version number of the supported TLM frame. More... | |
#define | EDDYSTONE_TOTAL_TLM_FRAME_LENGTH (22) |
Total number of bytes for the Eddystone TLM frame. More... | |
#define | EDDYSTONE_TOTAL_UID_FRAME_LENGTH (28) |
Total number of bytes for the Eddystone UID frame. More... | |
#define | EDDYSTONE_URI_DATA_MAX_SIZE (17 + 1) |
Maximum number of bytes in the encoded URL including the encoded scheme prefix. More... | |
#define | EDDYSTONE_URI_FLAG (0x10) |
Value of the URI flag characteristics. More... | |
#define | EDDYSTONE_URL_CONF_SERVICE_UUID ("\xd8\x81\xc9\x1a\xb9\x99\x96\xab\xba\x40\x86\x87\x80\x20\x0c\xee") |
Eddystone-URL configuration service defines. More... | |
#define | ESURL_CONF_ADV_INTERVAL (160) |
Advertisement interval between 0x0020 and 0x4000 in 0.625ms units [20ms to 10.24s]. More... | |
#define | ESURL_CONF_ADV_TIMEOUT (655) |
Advertisement timeout between 0x0001 and 0x3FFF in seconds, 0x0000 disables time-out. More... | |
#define | FIX88_2_FLOAT(a) ((float)(a/256.0)) |
#define | FIX88_2_INT(a) ((int16_t)((a) >> 8)) |
#define | FLOAT_2_FIX88(a) ((int16_t)((a)*256.0)) |
Conversion between float and 8:8 fixed point format. More... | |
#define | INT_2_FIX88(a) (((int16_t)(a)) << 8) |
Conversion between integer and 8:8 fixed point format. More... | |
Typedefs | |
typedef union beacon_id_t | beacon_id_t |
Eddystone-UID beacon structure. More... | |
typedef struct eddystone_tlm_data_t | eddystone_tlm_data_t |
Eddystone-TLM frame data. More... | |
typedef struct esurl_conf_gatt_service_t | esurl_conf_gatt_service_t |
URL configuration service GATT characteristics. More... | |
Enumerations | |
enum | eddystone_frame_t { EDDYSTONE_UID = 0x00, EDDYSTONE_URL = 0x10, EDDYSTONE_TLM = 0x20 } |
Three Types of Eddystone frames. More... | |
enum | eddystone_mode_t { EDDYSTONE_IDLE_MODE = 0x00, EDDYSTONE_BEACON_MODE, EDDYSTONE_URL_CONFIG_MODE_ADV, EDDYSTONE_URL_CONFIG_MODE_CONNECTED } |
Different modes present in Eddystone application. More... | |
enum | eddystone_tx_power_mode_t { TX_POWER_MODE_LOWEST = 0x00, TX_POWER_MODE_LOW, TX_POWER_MODE_MEDIUM, TX_POWER_MODE_HIGH } |
TX power modes supported. More... | |
enum | esurl_conf_serv_characteristic_t { CHAR_LOCK_STATE = 0x00, CHAR_LOCK, CHAR_UNLOCK, CHAR_URI_DATA, CHAR_URI_FLAGS, CHAR_ADV_TX_POWER_LEVELS, CHAR_TX_POWER_MODE, CHAR_BEACON_PERIOD, CHAR_RESET, ESURL_CONF_CHAR_NUM } |
Different characteristics present in Eddystone URL configuration service. More... | |
Functions | |
at_ble_status_t | eddystone_adv_stop (void) |
Stop transmitting Eddystone beacons. More... | |
eddystone_mode_t | eddystone_get_mode (void) |
Obtain the current mode of the Eddystone beacon. More... | |
at_ble_status_t | eddystone_init (void) |
Eddystone initialization; all UID and URL data are reset to default values. More... | |
at_ble_status_t | eddystone_set_beacon_id (beacon_id_t *uid) |
Update the Eddystone-UID (beacon ID). More... | |
at_ble_status_t | eddystone_set_beacon_interval (uint16_t beacon_interval_ms) |
Update the beacon interval. More... | |
at_ble_status_t | eddystone_set_encoded_url (uint8_t *url_val, uint8_t len) |
Update the Eddystone URL value. More... | |
at_ble_status_t | eddystone_set_power_mode (eddystone_tx_power_mode_t tx_power_mode) |
Update the TX power mode to be advertised. More... | |
at_ble_status_t | eddystone_set_uid_calib_tx_power (int8_t tx_power_0m, at_ble_tx_power_level_t radio_tx_power) |
Update the calibrated TX power value present in the Eddystone-UID frame. More... | |
at_ble_status_t | eddystone_tlm_frame_send (eddystone_tlm_data_t *tlm_data) |
Start sending Eddystone TLM beacons continuously The TLM frame is created out of battery voltage value, beacon temperature, advertisement PDU count and time since boot up. More... | |
at_ble_status_t | eddystone_uid_frame_send (void) |
Start sending Eddystone UID beacons continuously The UID frame is created out of parameters like Beacon ID and calibrated tx power at 0m. More... | |
at_ble_status_t | eddystone_url_frame_send (void) |
Start sending Eddystone URL beacons continuously The URL frame is created out of encoded URL and advertised tx power level at 0m. More... | |
at_ble_status_t | esurl_conf_adv_start (uint16_t adv_interval) |
Start the Eddystone-URL configuration service. More... | |
at_ble_status_t | esurl_conf_service_init (esurl_conf_gatt_service_t *serv) |
Eddystone URL Configuration Service and Characteristics initialization. More... | |
Variables | |
volatile uint32_t | eddystone_100ms_counter |
100ms counter value used in the creation of TLM frame. More... | |
const ble_gap_event_cb_t | esurl_conf_gap_cb |
Eddystone GAP events callback handler. More... | |
const ble_gatt_server_event_cb_t | esurl_conf_gatt_server_cb |
Eddystone GATT server events callback handler. More... | |
esurl_conf_gatt_service_t | esurl_conf_service |
Eddystone-URL configuration service information. More... | |
#define EDDYSTONE_16_BIT_UUID 0xFEAA |
16-bit Eddystone Service UUID
#define EDDYSTONE_BEACON_INTERVAL_MS_MAX (10240) |
Maximum beacon interval in ms (10240ms or 10.24s)
Referenced by esurl_write_authorize_event().
#define EDDYSTONE_BEACON_INTERVAL_MS_MIN (100) |
Minimum beacon interval in ms (100ms)
Referenced by esurl_write_authorize_event().
#define EDDYSTONE_TLM_FRAME_VERSION (0x00) |
Version number of the supported TLM frame.
Referenced by eddystone_create_tlm_frame().
#define EDDYSTONE_TOTAL_TLM_FRAME_LENGTH (22) |
Total number of bytes for the Eddystone TLM frame.
Referenced by eddystone_adv_start().
#define EDDYSTONE_TOTAL_UID_FRAME_LENGTH (28) |
Total number of bytes for the Eddystone UID frame.
Referenced by eddystone_adv_start().
#define EDDYSTONE_URI_DATA_MAX_SIZE (17 + 1) |
Maximum number of bytes in the encoded URL including the encoded scheme prefix.
Referenced by esurl_conf_service_init().
#define EDDYSTONE_URI_FLAG (0x10) |
Value of the URI flag characteristics.
Referenced by esurl_data_reset().
#define EDDYSTONE_URL_CONF_SERVICE_UUID ("\xd8\x81\xc9\x1a\xb9\x99\x96\xab\xba\x40\x86\x87\x80\x20\x0c\xee") |
Eddystone-URL configuration service defines.
128-bit UUID of the Eddystone-URL configuration service
Referenced by esurl_conf_adv_start(), and esurl_conf_service_init().
#define ESURL_CONF_ADV_INTERVAL (160) |
Advertisement interval between 0x0020 and 0x4000 in 0.625ms units [20ms to 10.24s].
Referenced by eddystone_custom_event().
#define ESURL_CONF_ADV_TIMEOUT (655) |
Advertisement timeout between 0x0001 and 0x3FFF in seconds, 0x0000 disables time-out.
Referenced by esurl_conf_adv_start().
#define FIX88_2_FLOAT | ( | a | ) | ((float)(a/256.0)) |
#define FIX88_2_INT | ( | a | ) | ((int16_t)((a) >> 8)) |
#define FLOAT_2_FIX88 | ( | a | ) | ((int16_t)((a)*256.0)) |
Conversion between float and 8:8 fixed point format.
Referenced by read_temperature_fix88().
#define INT_2_FIX88 | ( | a | ) | (((int16_t)(a)) << 8) |
Conversion between integer and 8:8 fixed point format.
typedef union beacon_id_t beacon_id_t |
Eddystone-UID beacon structure.
typedef struct eddystone_tlm_data_t eddystone_tlm_data_t |
Eddystone-TLM frame data.
typedef struct esurl_conf_gatt_service_t esurl_conf_gatt_service_t |
URL configuration service GATT characteristics.
enum eddystone_frame_t |
enum eddystone_mode_t |
at_ble_status_t eddystone_adv_stop | ( | void | ) |
Stop transmitting Eddystone beacons.
Stop transmitting Eddystone beacons.
References at_ble_adv_stop(), AT_BLE_FAILURE, AT_BLE_SUCCESS, eddystone_adv_enabled, EDDYSTONE_IDLE_MODE, es_mode, and status.
Referenced by eddystone_tlm_frame_send(), eddystone_uid_frame_send(), eddystone_url_frame_send(), and esurl_conf_adv_start().
eddystone_mode_t eddystone_get_mode | ( | void | ) |
Obtain the current mode of the Eddystone beacon.
Obtain the current mode of the Eddystone beacon.
References es_mode.
Referenced by eddystone_custom_event(), and main().
at_ble_status_t eddystone_init | ( | void | ) |
Eddystone initialization; all UID and URL data are reset to default values.
Eddystone initialization; all UID and URL data are reset to default values.
References AT_BLE_SUCCESS, esuid_data_reset(), and esurl_data_reset().
Referenced by eddystone_app_init().
at_ble_status_t eddystone_set_beacon_id | ( | beacon_id_t * | uid | ) |
Update the Eddystone-UID (beacon ID).
[in] | uid | The 16-byte UID value to be set; It must be in big endian format. UID consists of 10-byte Namespace ID and 6-byte Instance ID. |
Update the Eddystone-UID (beacon ID).
References AT_BLE_SUCCESS, esuid_data_t::beacon_id, beacon_id_t::instance_id, and beacon_id_t::namespace_id.
at_ble_status_t eddystone_set_beacon_interval | ( | uint16_t | beacon_interval_ms | ) |
Update the beacon interval.
This update requires a restart of the Eddystone frames to use this new beacon interval value.
[in] | beacon_interval_ms | Interval period in ms [100ms to 10240ms] |
Update the beacon interval.
Restart sending the Eddystone frames to use the updated beacon interval
References at_ble_characteristic_value_set(), AT_BLE_FAILURE, esurl_data_t::beacon_period, CHAR_BEACON_PERIOD, at_ble_characteristic_t::char_val_handle, esurl_conf_gatt_service_t::chars, esurl_conf_char_initialized, HIGH_BYTE, LOW_BYTE, and status.
at_ble_status_t eddystone_set_encoded_url | ( | uint8_t * | url_val, |
uint8_t | len | ||
) |
Update the Eddystone URL value.
[in] | url_val | Pointer to the encoded URL data. |
[in] | len | Number of bytes in the URL data. |
Update the Eddystone URL value.
References at_ble_characteristic_value_set(), AT_BLE_FAILURE, CHAR_URI_DATA, at_ble_characteristic_t::char_val_handle, esurl_conf_gatt_service_t::chars, EDDYSTONE_MAX_URL_ENC_LEN, esurl_conf_char_initialized, esurl_data_t::uri_data, and esurl_data_t::uri_len.
at_ble_status_t eddystone_set_power_mode | ( | eddystone_tx_power_mode_t | tx_power_mode | ) |
Update the TX power mode to be advertised.
This change in TX power mode will set the radio TX power accordingly.
[in] | tx_power_mode | One of the four power modes supported by Eddystone (eddystone_tx_power_mode_t) |
Update the TX power mode to be advertised.
References at_ble_characteristic_value_set(), AT_BLE_FAILURE, CHAR_TX_POWER_MODE, at_ble_characteristic_t::char_val_handle, esurl_conf_gatt_service_t::chars, esurl_conf_char_initialized, status, and esurl_data_t::tx_power_mode.
at_ble_status_t eddystone_set_uid_calib_tx_power | ( | int8_t | tx_power_0m, |
at_ble_tx_power_level_t | radio_tx_power | ||
) |
Update the calibrated TX power value present in the Eddystone-UID frame.
[in] | tx_power_0m | Calibrated TX power level at 0 meters which is advertised in the UID frame. |
[in] | radio_tx_power | Radio TX power to be set in the BLE device to achieve the advertised TX power at 0 meters. |
Update the calibrated TX power value present in the Eddystone-UID frame.
References AT_BLE_SUCCESS, esuid_data_t::radio_tx_power, and esuid_data_t::tx_power_0m.
at_ble_status_t eddystone_tlm_frame_send | ( | eddystone_tlm_data_t * | tlm_data | ) |
Start sending Eddystone TLM beacons continuously The TLM frame is created out of battery voltage value, beacon temperature, advertisement PDU count and time since boot up.
Start sending Eddystone TLM beacons continuously The TLM frame is created out of battery voltage value, beacon temperature, advertisement PDU count and time since boot up.
References AT_BLE_SUCCESS, eddystone_adv_start(), eddystone_adv_stop(), eddystone_create_tlm_frame(), EDDYSTONE_URL_CONFIG_MODE_ADV, es_adv_data, es_mode, and status.
Referenced by main().
at_ble_status_t eddystone_uid_frame_send | ( | void | ) |
Start sending Eddystone UID beacons continuously The UID frame is created out of parameters like Beacon ID and calibrated tx power at 0m.
Start sending Eddystone UID beacons continuously The UID frame is created out of parameters like Beacon ID and calibrated tx power at 0m.
References AT_BLE_SUCCESS, eddystone_adv_start(), eddystone_adv_stop(), eddystone_create_uid_frame(), EDDYSTONE_URL_CONFIG_MODE_ADV, es_adv_data, es_mode, and status.
Referenced by eddystone_app_init(), and main().
at_ble_status_t eddystone_url_frame_send | ( | void | ) |
Start sending Eddystone URL beacons continuously The URL frame is created out of encoded URL and advertised tx power level at 0m.
Start sending Eddystone URL beacons continuously The URL frame is created out of encoded URL and advertised tx power level at 0m.
References at_ble_disconnect(), AT_BLE_SUCCESS, AT_BLE_TERMINATED_BY_USER, eddystone_adv_start(), eddystone_adv_stop(), eddystone_create_url_frame(), EDDYSTONE_URL_CONFIG_MODE_ADV, EDDYSTONE_URL_CONFIG_MODE_CONNECTED, es_conf_conn_handle, es_mode, es_url_adv_data, and status.
Referenced by eddystone_app_init(), eddystone_custom_event(), esurl_dev_disconnected_event(), and main().
at_ble_status_t esurl_conf_adv_start | ( | uint16_t | adv_interval | ) |
Start the Eddystone-URL configuration service.
It starts the advertisement enabling any Central device to connect to the service.
[in] | adv_interval | Advertising interval between AT_BLE_ADV_INTERVAL_MIN and AT_BLE_ADV_INTERVAL_MAX in 0.625 ms units (20ms to 10.24s). |
Start the Eddystone-URL configuration service.
References esurl_data_t::adv_tx_power_level, ADV_TYPE_SIZE, at_ble_adv_data_set(), AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, at_ble_tx_power_set(), AT_BLE_UUID_128_LEN, COMPLETE_LIST_128BIT_SERV_UUIDS, COMPLETE_LOCAL_NAME, CONF_ES_CONF_ADV_DATA_COMPLETE_LOCAL_NAME, eddystone_adv_enabled, eddystone_adv_stop(), EDDYSTONE_URL_CONF_SERVICE_UUID, EDDYSTONE_URL_CONFIG_MODE_ADV, es_adv_data, es_mode, es_scan_data, ESURL_CONF_ADV_TIMEOUT, NULL, esurl_data_t::radio_tx_power_level, status, TX_POWER_LEVEL, TX_POWER_LEVEL_SIZE, and TX_POWER_MODE_MEDIUM.
Referenced by eddystone_custom_event().
at_ble_status_t esurl_conf_service_init | ( | esurl_conf_gatt_service_t * | serv | ) |
Eddystone URL Configuration Service and Characteristics initialization.
It initializes the given service structure with required default values and registers it with the BLE stack. This configuration service should be used only when Eddystone-URL beacons are used. (Must be called only once by the user.)
[in] | serv | Pointer to store Eddystone configuration service information. |
Eddystone URL Configuration Service and Characteristics initialization.
References esurl_data_t::adv_tx_power_level, AT_BLE_ATTR_NO_PERMISSIONS, AT_BLE_ATTR_READABLE_NO_AUTHN_NO_AUTHR, AT_BLE_ATTR_READABLE_REQ_AUTHN_NO_AUTHR, AT_BLE_ATTR_WRITABLE_NO_AUTHN_REQ_AUTHR, AT_BLE_ATTR_WRITABLE_REQ_AUTHN_REQ_AUTHR, AT_BLE_CHAR_READ, AT_BLE_CHAR_WRITE, at_ble_primary_service_define(), AT_BLE_SUCCESS, AT_BLE_UUID_128, AT_BLE_UUID_128_LEN, esurl_data_t::beacon_period, BLE_PAIR_ENABLE, CHAR_ADV_TX_POWER_LEVELS, CHAR_BEACON_PERIOD, CHAR_LOCK, CHAR_LOCK_STATE, CHAR_RESET, CHAR_TX_POWER_MODE, CHAR_UNLOCK, CHAR_URI_DATA, CHAR_URI_FLAGS, at_ble_characteristic_t::char_val_handle, esurl_conf_gatt_service_t::chars, at_ble_characteristic_t::client_config_handle, at_ble_characteristic_t::client_config_permissions, CONF_ES_DEFAULT_URL_SIZE, EDDYSTONE_TX_POWER_MODES_NUM, EDDYSTONE_URI_DATA_MAX_SIZE, EDDYSTONE_URL_CONF_SERVICE_UUID, esurl_conf_char_initialized, ESURL_CONF_CHAR_NUM, ESURL_CONF_CHAR_UUID_DIFF_OFFSET, esurl_data_reset(), ESURL_LOCK_CODE_MAX_SIZE, esurl_conf_gatt_service_t::handle, at_ble_characteristic_t::init_value, esurl_data_t::lock_code, esurl_data_t::lock_code_len, esurl_data_t::lock_state, NULL, at_ble_characteristic_t::presentation_format, at_ble_characteristic_t::properties, at_ble_characteristic_t::server_config_handle, at_ble_characteristic_t::server_config_permissions, status, esurl_data_t::tx_power_mode, at_ble_uuid_t::type, esurl_data_t::uri_data, esurl_data_t::uri_flags, at_ble_characteristic_t::user_desc, at_ble_characteristic_t::user_desc_handle, at_ble_characteristic_t::user_desc_len, at_ble_characteristic_t::user_desc_max_len, at_ble_characteristic_t::user_desc_permissions, esurl_conf_gatt_service_t::uuid, at_ble_uuid_t::uuid, at_ble_characteristic_t::uuid, UUID_CHAR_ADV_TX_POWER, UUID_CHAR_BEACON_PERIOD, UUID_CHAR_FLAGS, UUID_CHAR_LOCK, UUID_CHAR_LOCK_STATE, UUID_CHAR_RESET, UUID_CHAR_TX_POWER_MODE, UUID_CHAR_UNLOCK, UUID_CHAR_URI_DATA, at_ble_characteristic_t::value_init_len, at_ble_characteristic_t::value_max_len, and at_ble_characteristic_t::value_permissions.
Referenced by eddystone_app_init().
volatile uint32_t eddystone_100ms_counter |
100ms counter value used in the creation of TLM frame.
This counter variable needs to be updated by the application for every 100ms
Referenced by eddystone_create_tlm_frame(), and timer_callback_handler().
const ble_gap_event_cb_t esurl_conf_gap_cb |
Eddystone GAP events callback handler.
Eddystone GAP events callback handler.
Referenced by eddystone_app_init().
const ble_gatt_server_event_cb_t esurl_conf_gatt_server_cb |
Eddystone GATT server events callback handler.
Eddystone GATT server events callback handler.
Referenced by eddystone_app_init().
esurl_conf_gatt_service_t esurl_conf_service |
Eddystone-URL configuration service information.
Referenced by eddystone_app_init().