Receives data from a UDP Socket.
The asynchronous recvfrom function is used to retrieve data from a UDP socket. The socket must already be bound to a local port before a call to the recvfrom function is made (i.e message SOCKET_MSG_BIND is received with successful status in the socket callback).
Upon calling the recvfrom function with a successful return code, the application is expected to receive a notification in the socket callback whenever a message is received through the SOCKET_MSG_RECVFROM event.
Receiving the SOCKET_MSG_RECVFROM message in the callback with zero, indicates that the socket is closed. Whereby a negative buffer length indicates one of the socket error codes such as socket timeout error SOCK_ERR_TIMEOUT
The recvfrom callback can also be used to show the IP address of the remote host that sent the frame by using the "strRemoteAddr" element in the tstrSocketRecvMsg structure. (refer to the code example)
Functions | |
NMI_API sint16 | recvfrom (SOCKET sock, void *pvRecvBuf, uint16 u16BufLen, uint32 u32Timeoutmsec) |
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvRecvBuf | Pointer to a buffer that will hold the received data. The buffer shall be used in the recv callback to deliver the received data to the caller. The buffer must be resident in memory (heap or global buffer). |
[in] | u16BufLen | The buffer size in bytes. |
[in] | u32TimeoutSeconds | Timeout for the recv function in milli-seconds. If the value is set to ZERO, the timeout will be set to infinite (the recv function waits forever). |
The example demonstrates a code snippet for the calling of the recvfrom function in the socket callback upon notification of a successful bind event, and the parsing of the received data when the SOCKET_MSG_RECVFROM event is received.
Receives data from a UDP Socket. The asynchronous recvfrom function is used to retrieve data from a UDP socket. The socket must already be bound to a local port before a call to the recvfrom function is made (i.e message @ref SOCKET_MSG_BIND is received with successful status in the socket callback). Upon calling the recvfrom function with a successful return code, the application is expected to receive a notification in the socket callback whenever a message is received through the @ref SOCKET_MSG_RECVFROM event. Receiving the SOCKET_MSG_RECVFROM message in the callback with zero, indicates that the socket is closed. Whereby a negative buffer length indicates one of the socket error codes such as socket timeout error @ref SOCK_ERR_TIMEOUT The recvfrom callback can also be used to show the IP address of the remote host that sent the frame by using the "strRemoteAddr" element in the @ref tstrSocketRecvMsg structure. (refer to the code example)
[in] | sock | Socket ID, must hold a non negative value. A negative value will return a socket error SOCK_ERR_INVALID_ARG. Indicating that an invalid argument is passed in. |
[in] | pvRecvBuf | Pointer to a buffer that will hold the received data. The buffer shall be used in the recv callback to deliver the received data to the caller. The buffer must be resident in memory (heap or global buffer). |
[in] | u16BufLen | The buffer size in bytes. |
[in] | u32TimeoutSeconds | Timeout for the recv function in milli-seconds. If the value is set to ZERO, the timeout will be set to infinite (the recv function waits forever). |
The example demonstrates a code snippet for the calling of the recvfrom function in the socket callback upon notification of a successful bind event, and the parsing of the received data when the SOCKET_MSG_RECVFROM event is received.