Synchronous deinitialization function to the WILC1000 driver.
Dinitializes the host interface and frees resources used by the M2M_WIFI layer. Must be called in the application closing function, to ensure that all resources have been correctly released. No arguments are expected to be passed in.
Functions | |
NMI_API sint8 | m2m_wifi_deinit (void *arg) |
De-initialize the WINC driver and host interface. More... | |
De-initialize the WINC driver and host interface.
Synchronous API to de-initialize the WINC driver and host interface.
[in] | arg | Generic argument. Not used in current implementation. |
Synchronous de-initialization function for the WINC driver. De-initializes the host interface and frees any resources used by the M2M_WIFI layer. This function must be called in the application closing phase to ensure that all resources have been correctly released. No arguments are expected to be passed in.
[in] | arg | Opaque argument, not used in current implementation. Application should use null. |
De-initialization function for the WINC driver. De-initializes the host interface and frees any resources used by the M2M_WIFI layer. This function must be called in the application closing phase to ensure that all resources have been correctly released.
[in] | arg | Opaque argument, not used in current implementation. Application should use null. |