|
| m2m_wifi_init |
| Synchronous initialization functions for the WILC driver.
|
|
| m2m_wifi_deinit |
| Synchronous deinitialization function to the WILC1000 driver.
|
|
| m2m_wifi_handle_events |
| Synchronous M2M event handler function, responsible for handling interrupts received from the WILC firmware.
|
|
| m2m_wifi_connect |
| Asynchronous wi-fi connection function to a specific AP.
|
|
| m2m_wifi_disconnect |
| Synchronous wi-fi disconnection function, requesting a Wi-Fi disconnect from the currently connected AP.
|
|
| m2m_wifi_get_connection_info |
| Asynchronous connection status retrieval function, retrieves the status information of the currently connected AP.
|
|
| m2m_wifi_set_mac_address |
| Synchronous dual MAC address assigning to the WILC1500 .
|
|
| m2m_wifi_wps |
| Asynchronous WPS triggering function.
|
|
| m2m_wifi_wps_disable |
| Disable the NMC1500 WPS operation.
|
|
| m2m_wifi_p2p |
| Asynchronous Wi-Fi direct (P2P) enabling mode function.
|
|
| m2m_wifi_p2p_disconnect |
| Disable the NMC1500 device Wi-Fi direct mode (P2P).
|
|
| m2m_wifi_enable_ap |
| Asychronous wi-fi hotspot enabling function.
|
|
| m2m_wifi_disable_ap |
| Synchronous wi-fi hotspot disabling function.
|
|
| m2m_wifi_set_scan_options |
| Synchronous wi-fi scan settings function.
|
|
| m2m_wifi_set_scan_region |
| Synchronous wi-fi scan region setting function.
|
|
| m2m_wifi_request_scan |
| Asynchronous wi-fi scan request on the given channel.
|
|
| m2m_wifi_get_num_ap_found |
| Synchronous function to retrieve the number of AP's found in the last scan request, The function read the number of AP's from global variable which updated in the wi-fi callback fucntion through the M2M_WIFI_RESP_SCAN_DONE event.
|
|
| m2m_wifi_req_scan_result |
| Synchronous call to read the AP information from the SCAN Result list with the given index.
|
|
|
| m2m_wifi_get_otp_mac_address |
| Request the MAC address stored on the OTP (one time programmable) memory of the device.
|
|
| m2m_wifi_get_mac_address |
| Function to retrieve the current MAC address.
|
|
| m2m_wifi_set_sleep_mode |
| Synchronous power-save mode setting function for the NMC1500.
|
|
| m2m_wifi_get_sleep_mode |
| Synchronous power save mode retrieval function.
|
|
| m2m_wifi_set_lsn_int |
| Synchronous function for setting the wi-fi listen interval for power save operation.
|
|
| m2m_wifi_enable_monitoring_mode |
| Asynchronous wi-fi monitoring enable mode (Promiscuous mode) function.
|
|
| m2m_wifi_disable_monitoring_mode |
| Synchronous function to disable Wi-Fi monitoring mode (Promiscuous mode).
|
|
| m2m_wifi_send_wlan_pkt |
| Synchronous function to transmit a WIFI RAW packet while the implementation of this packet is left to the application developer.
|
|
| m2m_wifi_send_ethernet_pkt |
| Synchronous function to transmit an Ethernet packet.
|
|
| m2m_wifi_set_cust_InfoElement |
| Synchronous function to Add/Remove user-defined Information Element to the WIFIBeacon and Probe Response frames while chip mode is Access Point Mode.
|
|
| Initialization |
| Here are listed all the functions that implement the Wlan Initialization APIs.
|
|
| Wlan Events |
| Here are listed all the functions that implement the Wlan Events APIs.
|
|
| Connection |
| Here are listed all the functions that implement the Wifi Connection APIs.
|
|
| Scanning |
| Here are listed all the functions that implement the Wifi Scanning APIs.
|
|
| Hot-Spot (Access-Point) |
| Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs.
|
|
| Bypass Mode |
| Here are listed all the functions that implement the Bypass Mode APIs.
|
|
| Roaming |
| Here are listed all the functions that implement the Wifi Roaming APIs.
|
|
| Power Save |
| Here are listed all the functions that implement the Power-Save APIs.
|
|
| Configuration |
| Here are listed all the functions that implement the Wlan Configuration APIs.
|
|
| System Time |
| Here are listed all the functions that implement the System Time APIs.
|
|
| Provisioning |
| Here are listed all the functions that implement the Wifi Provisioning APIs.
|
|
| Crypto |
| Here are listed all the functions that implement the Wifi Crypto APIs.
|
|
| BLE |
| Here are listed all the functions that implement the BLE APIs.
|
|