Here are listed all the functions that implement the Power-Save APIs.
Functions | |
sint8 | m2m_wifi_enable_XO_during_sleep (uint8 bXOSleepEnable) |
Specifies whether the crystal oscillator is left on or off during deep sleep (defaults to off). More... | |
uint8 | m2m_wifi_get_sleep_mode (void) |
Get the current Power save mode. More... | |
sint8 | m2m_wifi_request_sleep (uint32 u32SlpReqTime) |
API to place the WINC IC into sleep mode for a specified period of time. More... | |
sint8 | m2m_wifi_set_lsn_int (tstrM2mLsnInt *pstrM2mLsnInt) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods. More... | |
sint8 | m2m_wifi_set_power_profile (uint8 u8PwrMode) |
Change the power profile mode. More... | |
sint8 | m2m_wifi_set_sleep_mode (uint8 PsTyp, uint8 BcastEn) |
Set the power saving mode for the WILC1000. More... | |
Specifies whether the crystal oscillator is left on or off during deep sleep (defaults to off).
m2m_wifi_enable_XO_during_sleep controls the state of the crystal oscillator during deep sleep.
[in] | bXOSleepEnable | 0 : The XO will be switched off during deep sleep 1 : The XO will be kept on during deep sleep |
References hif_send(), M2M_ERR_INVALID_ARG, M2M_REQ_GROUP_WIFI, M2M_WIFI_REQ_XO_SLEEP_ENABLE, NULL, and tstrM2mWiFiXOSleepEnable::u8EnableXODuringSleep.
Get the current Power save mode.
Synchronous API to retrieve the current power save mode of the WINC.
Synchronous power save mode retrieval function.
Referenced by os_m2m_wifi_get_sleep_mode().
API to place the WINC IC into sleep mode for a specified period of time.
Asynchronous API to place the WINC into sleep mode for a specified period of time.
Synchronous power-save sleep request function, which requests the WINC device to sleep in the currently configured power save mode, as set using @ref m2m_wifi_set_sleep_mode, for a specific time as defined by the passed in parameter. This function should be used in the @ref M2M_PS_MANUAL power save mode only. A wake up request is automatically performed by the WINC device when any host driver API function, e.g. Wi-Fi or socket operation is called.
[in] | u32SlpReqTime | Request sleep time in ms. The best recommended sleep duration is left to be determined by the application. Taking into account that if the application sends notifications very rarely, sleeping for a long time can be a power-efficient decision. In contrast, applications that are sensitive for long periods of absence can experience performance degradation in the connection if long sleeping times are used. |
Power-save sleep request function, which requests the WINC device to sleep in the currently configured power save mode, as set using @ref m2m_wifi_set_sleep_mode, for a specific time as defined by the parameter u32SlpReqTime (measured in milliseconds). This function should be used when the WINC is running in @ref M2M_PS_MANUAL power save mode only. A wake up request is automatically performed by the WINC device when any host driver API function, e.g. Wi-Fi or socket operation is called.
[in] | u32SlpReqTime | Request sleep time in ms. The best recommended sleep duration is left to be determined by the application. Taking into account that if the application sends notifications very rarely, sleeping for a long time can be a power-efficient decision. In contrast, applications that are sensitive for long periods of absence can experience performance degradation in the connection if long sleeping times are used. |
Referenced by os_m2m_wifi_request_sleep_imp().
NMI_API sint8 m2m_wifi_set_lsn_int | ( | tstrM2mLsnInt * | pstrM2mLsnInt | ) |
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods.
Asynchronous API to set Wi-Fi listen interval for power save operation.
API to set Wi-Fi listen interval for power save operation.
[in] | pstrM2mLsnInt | Structure holding the listen interval configurations. |
[in] | pstrM2mLsnInt | Structure holding the listen interval configurations. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done by modifying the Wi-Fi listen interval. The listen interval is how many beacon periods the station can sleep before it wakes up to receive data buffered in the AP. It is represented in units of AP beacon periods(100ms).
[in] | pstrM2mLsnInt | Structure holding the listen interval configuration. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done by modifying the Wi-Fi listen interval. The listen interval is how many beacon periods the station can sleep before it wakes up to receive data buffered in the AP. It is represented in units of AP beacon periods(100ms).
[in] | pstrM2mLsnInt | Structure holding the listen interval configuration. |
Referenced by app_wifi_init(), and os_m2m_wifi_set_lsn_int_imp().
Change the power profile mode.
Change the power profile mode
Not implemented in WINC3400 firmware.
[in] | u8PwrMode | Change the WINC power profile to different mode PWR_LOW1/PWR_LOW2/PWR_HIGH/PWR_AUTO (tenuM2mPwrMode) |
[in] | u8PwrMode | Change the WINC power profile to different mode based on the enumeration tenuM2mPwrMode. |
[in] | u8PwrMode | Change the WINC power profile to different mode PWR_LOW1/PWR_LOW2/PWR_HIGH/PWR_AUTO (tenuM2mPwrMode) |
[in] | u8PwrMode | Change the WINC power profile to different mode based on the enumeration tenuM2mPwrMode. Not implemented in WINC3400 firmware. |
Set the power saving mode for the WILC1000.
Synchronous API to set the power-save mode of the WINC.
Set the power saving mode for the WINC3400.
Synchronous API to set the power-save mode of the WINC IC.
Set the power saving mode for the WINC1500.
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM beacon for receiving broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM beacon, but its wakeup depends only on the the configured Listen Interval. |
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC1500 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WINC1500 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done through one of two ways: - 1) Changing the power save mode, to one of the allowed power save modes (see @ref tenuPowerSaveModes). This is done by setting the first parameter. - 2) Configuring DTIM monitoring: Configuring beacon monitoring parameters by enabling or disabling the reception of broadcast/multicast data. This is done by setting the second parameter.
[in] | PsTyp | Desired power saving mode. Supported types are enumerated in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC will be awake for each DTIM beacon in order to check for and receive broadcast traffic. If it is 0, the WINC will ignore broadcast traffic. Through this flag the WINC will not wakeup at the DTIM beacon, but instead it will wakeup only based on the configured Listen Interval. |
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC3400 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WINC3400 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
This is one of the two synchronous power-save setting functions that allow the host MCU application to tweak the system power consumption. Such tweaking can be done through one of two ways: - 1) Changing the power save mode, to one of the allowed power save modes (see @ref tenuPowerSaveModes). This is done by setting the first parameter. - 2) Configuring DTIM monitoring: Configuring beacon monitoring parameters by enabling or disabling the reception of broadcast/multicast data. This is done by setting the second parameter.
[in] | PsTyp | Desired power saving mode. Supported types are enumerated in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If set to 1, the WINC will wake for each DTIM beacon to ensure broadcast traffic can be received. If set to 0, the WINC will not wakeup at the DTIM beacon, ignoring broadcast traffic, instead it will wake every N beacon periods, as per the negotiated Listen Interval. |
Referenced by app_wifi_init(), atCmd_PsMode_Handler(), and os_m2m_wifi_set_sleep_mode_imp().