Synchronous dual MAC address assigning to the WILC1500 .
It is used for non-production SW.
Functions | |
NMI_API sint8 | m2m_wifi_set_mac_address (uint8 au8MacAddress0[6], uint8 au8MacAddress1[6]) |
Assign MAC addresses to the WILC device. More... | |
Assign MAC addresses to the WILC device.
[in] | au8MacAddress0 | MAC Address to be provisioned to the WILC for STA interface. |
[in] | au8MacAddress1 | MAC Address to be provisioned to the WILC for AP interface. |
References tstrM2mSetMacAddress::au8Mac0, tstrM2mSetMacAddress::au8Mac1, hif_send(), m2m_memcpy(), M2M_REQ_GRP_WIFI, M2M_WIFI_REQ_SET_MAC_ADDRESS, and NULL.
Referenced by app_wifi_init(), main(), and os_m2m_wifi_set_mac_address_imp().