Synchronous function to disable Wi-Fi monitoring mode (Promiscuous mode).
Synchronous function to change the Wi-Fi monitoring channel(Promiscuous mode).
Expected to be called, if the enable monitoring mode is set, but if it was called without enabling no negative impact will reside.
Functions | |
NMI_API sint8 | m2m_wifi_change_monitoring_channel (uint8 u8ChannelID) |
NMI_API sint8 | m2m_wifi_disable_monitoring_mode (void) |
[in] | u8ChannelID | New monitoring channel |
References hif_send(), M2M_REQ_DATA_PKT, M2M_REQ_GRP_WIFI, M2M_WIFI_CH_1, M2M_WIFI_CH_14, M2M_WIFI_REQ_CHG_MONITORING_CHNL, and NULL.
References hif_send(), M2M_REQ_GRP_WIFI, M2M_WIFI_REQ_DISABLE_MONITORING, and NULL.
Referenced by os_m2m_wifi_disable_monitoring_mode().