Synchronous function for setting the wi-fi listen interval for power save operation.
It is represented in units of AP Beacon periods. Function
Set the Wi-Fi listen interval for power save operation. It is represented in units of AP Beacon periods.
Asynchronous API to set Wi-Fi listen interval for power save operation.
API to set Wi-Fi listen interval for power save operation.
- Parameters
-
[in] | pstrM2mLsnInt | Structure holding the listen interval configurations. |
- Returns
- The function SHALL return 0 for success and a negative value otherwise.
- See Also
- tstrM2mLsnInt , m2m_wifi_set_sleep_mode
- Precondition
- m2m_wifi_set_sleep_mode shall be called first
- Warning
- The Function called once after initialization.
- Parameters
-
[in] | pstrM2mLsnInt | Structure holding the listen interval configurations. |
- Precondition
- Function m2m_wifi_set_sleep_mode shall be called first
- Warning
- The function should be called once after initialization.
- See Also
- tstrM2mLsnInt m2m_wifi_set_sleep_mode
- Returns
- The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
This is one of the two synchronous power-save setting functions that
allow the host MCU application to tweak the system power consumption. Such tweaking can be done by modifying the
Wi-Fi listen interval. The listen interval is how many beacon periods the station can sleep before it wakes up to receive data buffered in the AP.
It is represented in units of AP beacon periods(100ms).
- Warning
- The function should be called once after initialization.
- Parameters
-
[in] | pstrM2mLsnInt | Structure holding the listen interval configuration. |
- Precondition
- The function m2m_wifi_set_sleep_mode shall be called first, to set the power saving mode required.
- Returns
- The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
- See Also
- tstrM2mLsnInt m2m_wifi_set_sleep_mode
This is one of the two synchronous power-save setting functions that
allow the host MCU application to tweak the system power consumption. Such tweaking can be done by modifying the
Wi-Fi listen interval. The listen interval is how many beacon periods the station can sleep before it wakes up to receive data buffered in the AP.
It is represented in units of AP beacon periods(100ms).
- Warning
- The function should be called once after initialization.
- Parameters
-
[in] | pstrM2mLsnInt | Structure holding the listen interval configuration. |
- Precondition
- The function m2m_wifi_set_sleep_mode shall be called first, to set the power saving mode required.
- Returns
- The function returns M2M_SUCCESS if the command has been successfully queued to the WINC and a negative value otherwise.
- See Also
- tstrM2mLsnInt m2m_wifi_set_sleep_mode