Here are listed all the functions that implement the Wifi Hot-Spot (Access-Point) APIs.
Functions | |
sint8 | m2m_wifi_disable_ap (void) |
Synchronous API to disable access point mode on the WINC IC. More... | |
sint8 | m2m_wifi_enable_ap (CONST tstrM2MAPConfig *pstrM2MAPConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC. More... | |
sint8 | m2m_wifi_enable_ap_ext (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC with extended options. More... | |
Synchronous API to disable access point mode on the WINC IC.
Synchronous API to disable access point mode on the WINC.
Must be called only when the AP is enabled through the @ref m2m_wifi_enable_ap function. Otherwise the call to this function will not be useful.
Referenced by enable_disable_ap_mode(), m2m_wifi_disable_ap_ex(), os_m2m_wifi_disable_ap(), socket_cb(), and wifi_ap_provision().
NMI_API sint8 m2m_wifi_enable_ap | ( | CONST tstrM2MAPConfig * | pstrM2MAPConfig | ) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC.
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC.
[in] | pstrM2MAPConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function
The WINC IC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
The WINC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
Referenced by enable_disable_ap_mode(), m2m_wifi_enable_ap_ex(), main(), os_m2m_wifi_enable_ap_imp(), and wifi_ap_provision().
NMI_API sint8 m2m_wifi_enable_ap_ext | ( | CONST tstrM2MAPModeConfig * | pstrM2MAPModeConfig | ) |
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC IC with extended options.
Asynchronous API to enable access point (AKA "hot-spot") mode on the WINC with extended options.
The WINC IC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPModeConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
The WINC supports the ability to operate as an access point with the following limitations: - Only 1 station may be associated at any given time. - Open system and WEP are the only security suites supported.
[in] | pstrM2MAPModeConfig | A structure holding the AP configurations. |
The code snippet demonstrates how the AP mode is enabled after the driver is initialized in the application's main function and the handling of the event M2M_WIFI_REQ_DHCP_CONF, to indicate successful connection.
Referenced by m2m_wifi_enable_ap().