AP Configuration.
This structure holds the configuration parameters for the AP mode. It should be set by the application when it requests to enable the AP operation mode. The AP mode currently supports only OPEN and WEP security.
This structure holds the configuration parameters for the M2M AP mode. It should be set by the application when it requests to enable the M2M AP operation mode. The M2M AP mode currently supports only WEP security (with the NO Security option availabe of course).
This structure holds the configuration parameters for the M2M AP mode. It should be set by the application when it requests to enable the M2M AP operation mode. This mode supports either open, WEP or WPA/WPA2 mixed mode security types.
#include <m2m_types.h>
uint8 tstrM2MAPConfig::__PAD16__[2] |
Padding bytes for forcing alignment
uint8 tstrM2MAPConfig::__PAD24__[3] |
Padding bytes for forcing alignment
uint8 tstrM2MAPConfig::__PAD__[PAD_SZ(2+M2M_MAX_SSID_LEN+5+sizeof(tuniM2MWifiAuth))] |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2MAPConfig::au8DHCPServerIP |
Ap IP server address
AP DHCP server address
Referenced by enable_disable_ap_mode(), m2m_wifi_start_provision_mode(), main(), and wifi_ap_provision().
uint8 tstrM2MAPConfig::au8Key[M2M_MAX_PSK_LEN] |
WPA key
uint8 tstrM2MAPConfig::au8SSID |
AP SSID
< Configuration parameters for the WiFi AP.AP SSID
Referenced by atCmd_ApEnable_Handler(), enable_disable_ap_mode(), main(), sta_task(), and wifi_ap_provision().
uint8 tstrM2MAPConfig::au8WepKey |
uint16 tstrM2MAPConfig::u16BeaconInterval |
< Configuration parameters for the WiFi AP. Time between two consecutive beacons in TUs (1024 usec). A value of 0 would use the FW default
Referenced by sta_task().
uint8 tstrM2MAPConfig::u8IsPMKUsed |
set to true if the PMK is calculated on the host .
Referenced by m2m_wifi_enable_ap().
uint8 tstrM2MAPConfig::u8KeyIndx |
uint8 tstrM2MAPConfig::u8KeySz |
uint8 tstrM2MAPConfig::u8ListenChannel |
Wi-Fi RF Channel which the AP will operate on
Referenced by atCmd_ApEnable_Handler(), enable_disable_ap_mode(), main(), sta_task(), and wifi_ap_provision().
uint8 tstrM2MAPConfig::u8MaxSupportedSta |
Max supported stations for AP. Val 0 considered as default 8 stations Val > 8 are considered upto 8 stations
uint8 tstrM2MAPConfig::u8SecType |
Security type: Open, WEP and WPA2 modes supported as defined in tenuM2mSecType
Security type: Open, WEP or WPA/WPA2 mixed mode
Security type: OPEN or WEP
Referenced by atCmd_ApEnable_Handler(), enable_disable_ap_mode(), main(), sta_task(), and wifi_ap_provision().
uint8 tstrM2MAPConfig::u8SsidHide |
SSID Status "Hidden(1)/Visible(0)"
Referenced by atCmd_ApEnable_Handler().
tuniM2MWifiAuth tstrM2MAPConfig::uniAuth |
Union holding all possible authentication parameters corresponding the current security types.
Referenced by atCmd_ApEnable_Handler(), m2m_wifi_enable_ap(), and sta_task().