Synchronous power-save mode setting function for the NMC1500.
Set the power saving mode for the WILC1000.
Synchronous API to set the power-save mode of the WINC.
Set the power saving mode for the WINC3400.
Synchronous API to set the power-save mode of the WINC IC.
Set the power saving mode for the WINC1500.
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
- Returns
- The function SHALL return 0 for success and a negative value otherwise.
- See Also
- tenuPowerSaveModes
- Warning
- The function called once after initialization.
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WILC1000 must be awake each DTIM beacon for receiving broadcast traffic. If it is 0, the WILC1000 will not wakeup at the DTIM beacon, but its wakeup depends only on the the configured Listen Interval. |
- See Also
- tenuPowerSaveModes m2m_wifi_get_sleep_mode
- Returns
- The function returns M2M_SUCCESS for successful operations and a negative value otherwise.
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC1500 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WINC1500 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
- Returns
- The function SHALL return 0 for success and a negative value otherwise.
- See Also
- tenuPowerSaveModes
- Warning
- The function called once after initialization.
This is one of the two synchronous power-save setting functions that allow the host MCU application
to tweak the system power consumption. Such tweaking can be done through one of two ways:
- 1) Changing the power save mode, to one of the allowed power save modes (see @ref tenuPowerSaveModes). This is done by setting the first parameter.
- 2) Configuring DTIM monitoring: Configuring beacon monitoring parameters by enabling or disabling the reception of broadcast/multicast data.
This is done by setting the second parameter.
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are enumerated in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC will be awake for each DTIM beacon in order to check for and receive broadcast traffic. If it is 0, the WINC will ignore broadcast traffic. Through this flag the WINC will not wakeup at the DTIM beacon, but instead it will wakeup only based on the configured Listen Interval. |
- Warning
- The function called once after initialization.
- Returns
- The function returns M2M_SUCCESS for successful operation and a negative value otherwise.
- See Also
- tenuPowerSaveModes m2m_wifi_get_sleep_mode m2m_wifi_set_lsn_int
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are defined in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If it is 1, the WINC3400 must be awake each DTIM Beacon for receiving Broadcast traffic. If it is 0, the WINC3400 will not wakeup at the DTIM Beacon, but its wakeup depends only on the the configured Listen Interval. |
- Returns
- The function SHALL return 0 for success and a negative value otherwise.
- See Also
- tenuPowerSaveModes
- Warning
- The function called once after initialization.
This is one of the two synchronous power-save setting functions that allow the host MCU application
to tweak the system power consumption. Such tweaking can be done through one of two ways:
- 1) Changing the power save mode, to one of the allowed power save modes (see @ref tenuPowerSaveModes). This is done by setting the first parameter.
- 2) Configuring DTIM monitoring: Configuring beacon monitoring parameters by enabling or disabling the reception of broadcast/multicast data.
This is done by setting the second parameter.
- Parameters
-
[in] | PsTyp | Desired power saving mode. Supported types are enumerated in tenuPowerSaveModes. |
[in] | BcastEn | Broadcast reception enable flag. If set to 1, the WINC will wake for each DTIM beacon to ensure broadcast traffic can be received. If set to 0, the WINC will not wakeup at the DTIM beacon, ignoring broadcast traffic, instead it will wake every N beacon periods, as per the negotiated Listen Interval. |
- Warning
- The function called once after initialization.
- Returns
- The function returns M2M_SUCCESS for successful operation and a negative value otherwise.
- See Also
- tenuPowerSaveModes m2m_wifi_get_sleep_mode m2m_wifi_set_lsn_int