Synchronous wi-fi hotspot disabling function.
Synchronous wi-fi hotspot add/remove station from the black List.
Must be called only when the AP is enabled through the m2m_wifi_enable_ap function. Otherwise the call to this function will not be useful.
Functions | |
NMI_API sint8 | m2m_wifi_ap_add_black_list (uint8 bAddNewEntry, uint8 *mac_addr) |
NMI_API sint8 | m2m_wifi_disable_ap (void) |
Synchronous API to disable access point mode on the WINC IC. More... | |
[in] | bAddNewEntry | Boolean value if 1 then the given mac address would be added to the black list if zero the given mac address would be removed from the black list mac_addr MAC address of the station to be added/removed from the black list Note to remove all stations from the black list use all FF's in the mac address and set bAddNewEntry to zero |
References hif_send(), m2m_memcpy(), M2M_REQ_GRP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_AP_BLACK_LIST, and NULL.
Synchronous API to disable access point mode on the WINC IC.
Synchronous API to disable access point mode on the WINC.
Must be called only when the AP is enabled through the @ref m2m_wifi_enable_ap function. Otherwise the call to this function will not be useful.