This driver interfaces the HSMCI module.
It will add functions for SD/MMC card reading, writing and management.
|
bool | hsmci_adtc_start (sdmmc_cmd_def_t cmd, uint32_t arg, uint16_t block_size, uint16_t nb_block, bool access_block) |
| Send an ADTC command on the selected slot An ADTC (Addressed Data Transfer Commands) command is used for read/write access. More...
|
|
bool | hsmci_adtc_stop (sdmmc_cmd_def_t cmd, uint32_t arg) |
| Send a command to stop an ADTC command on the selected slot. More...
|
|
void | hsmci_deselect_device (uint8_t slot) |
| Deselect a slot. More...
|
|
uint8_t | hsmci_get_bus_width (uint8_t slot) |
| Return the maximum bus width of a slot. More...
|
|
uint32_t | hsmci_get_response (void) |
| Return the 32 bits response of the last command. More...
|
|
void | hsmci_get_response_128 (uint8_t *response) |
| Return the 128 bits response of the last command. More...
|
|
void | hsmci_init (void) |
| Initializes the low level driver. More...
|
|
bool | hsmci_is_high_speed_capable (void) |
| Return the high speed capability of the driver. More...
|
|
bool | hsmci_read_word (uint32_t *value) |
| Read a word on the line. More...
|
|
void | hsmci_select_device (uint8_t slot, uint32_t clock, uint8_t bus_width, bool high_speed) |
| Select a slot and initialize it. More...
|
|
void | hsmci_send_clock (void) |
| Send 74 clock cycles on the line of selected slot Note: It is required after card plug and before card install. More...
|
|
bool | hsmci_send_cmd (sdmmc_cmd_def_t cmd, uint32_t arg) |
| Send a command on the selected slot. More...
|
|
bool | hsmci_start_read_blocks (void *dest, uint16_t nb_block) |
| Start a read blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer. More...
|
|
bool | hsmci_start_write_blocks (const void *src, uint16_t nb_block) |
| Start a write blocks transfer on the line Note: The driver will use the DMA available to speed up the transfer. More...
|
|
bool | hsmci_wait_end_of_read_blocks (void) |
| Wait the end of transfer initiated by mci_start_read_blocks() More...
|
|
bool | hsmci_wait_end_of_write_blocks (void) |
| Wait the end of transfer initiated by mci_start_write_blocks() More...
|
|
bool | hsmci_write_word (uint32_t value) |
| Write a word on the line. More...
|
|
bool hsmci_adtc_start |
( |
sdmmc_cmd_def_t |
cmd, |
|
|
uint32_t |
arg, |
|
|
uint16_t |
block_size, |
|
|
uint16_t |
nb_block, |
|
|
bool |
access_block |
|
) |
| |
Send an ADTC command on the selected slot An ADTC (Addressed Data Transfer Commands) command is used for read/write access.
- Parameters
-
cmd | Command definition |
arg | Argument of the command |
block_size | Block size used for the transfer |
nb_block | Total number of block for this transfer |
access_block | if true, the x_read_blocks() and x_write_blocks() functions must be used after this function. If false, the mci_read_word() and mci_write_word() functions must be used after this function. |
- Returns
- true if success, otherwise false
References Assert, block_size, hsmci_block_size, hsmci_nb_block, hsmci_send_cmd_execute(), hsmci_transfert_pos, SDMMC_CMD_MULTI_BLOCK, SDMMC_CMD_SDIO_BLOCK, SDMMC_CMD_SDIO_BYTE, SDMMC_CMD_SINGLE_BLOCK, SDMMC_CMD_STREAM, and SDMMC_CMD_WRITE.