#include <atpl230.h>
Data Fields | |
uint16_t | model |
(r) Model number More... | |
char | prodId [10] |
(r) Product identifier More... | |
uint8_t | reserved0 |
Reserved. More... | |
uint8_t | reserved1 |
Reserved. More... | |
uint8_t | reserved2 |
Reserved. More... | |
uint16_t | reserved3 |
Reserved. More... | |
uint32_t | rxBadCrc |
(r) Bad CRC in received message (only in Prime v1.3) More... | |
uint32_t | rxBadLen |
(r) Bad len in message (too short - too long) More... | |
uint8_t | rxHdrRcv |
(r) Flag to indicate if header has already been received More... | |
uint8_t | rxIdBuff |
(r) Buffer identifier of received message More... | |
uint8_t | rxMode |
(w/r) Mode PRIME v1.3 or PRIME v1.4 More... | |
uint16_t | rxPayloadLen |
(r) RX: Payload length in bytes More... | |
uint16_t | rxPayloadLenSym |
(r) RX: Payload length in OFDM symbols More... | |
uint8_t | rxQRMode |
(w/r) Flag to enable / disable Rx Quality Report Mode More... | |
uint8_t | rxScheme |
(r) Modulation Scheme of last received message More... | |
uint32_t | rxTotal |
(r) Received correctly messages count More... | |
uint32_t | rxTotalBytes |
(r) Received bytes count More... | |
uint32_t | rxTotalErrors |
(r) Reception errors count More... | |
uint32_t | txBadBusyChannel |
(r) Transmission failure owing to busy channel More... | |
uint32_t | txBadBusyTx |
(r) Already in transmission More... | |
uint32_t | txBadFormat |
(r) Message to transmit in bad format More... | |
uint32_t | txBadLen |
(r) Bad len in message (too short - too long) More... | |
uint8_t | txDisableRx |
(w/r) Flag to enable / disable reception at transmission start More... | |
uint8_t | txIdBuff |
(w/r) Buffer identifier of transmitted message More... | |
uint8_t | txLevel |
(w/r) Level parameter of last transmitted message More... | |
uint8_t | txMode |
(w/r) Mode PRIME v1.3 or PRIME v1.4 More... | |
uint16_t | txPayloadLenSym |
(r) TX: Payload length in OFDM symbols More... | |
uint8_t | txQRMode |
(w/r) Flag to enable / disable Tx Quality Report Mode More... | |
uint8_t | txScheme |
(w/r) Modulation scheme of last transmitted message More... | |
uint32_t | txTdelay |
(w/r) Delay for transmission in 10's of us More... | |
uint32_t | txTimeout |
(r) Timeout error in transmission More... | |
uint32_t | txTotal |
(r) Transmitted correctly messages count More... | |
uint32_t | txTotalBytes |
(r) Transmitted bytes count More... | |
uint32_t | txTotalErrors |
(r) Transmission errors count More... | |
uint32_t | version |
(r) Version number More... | |
uint16_t atpl230_t::model |
(r) Model number
char atpl230_t::prodId[10] |
(r) Product identifier
Referenced by _init_phy_layer().
uint8_t atpl230_t::reserved0 |
Reserved.
uint8_t atpl230_t::reserved1 |
Reserved.
uint8_t atpl230_t::reserved2 |
Reserved.
uint16_t atpl230_t::reserved3 |
Reserved.
uint32_t atpl230_t::rxBadCrc |
(r) Bad CRC in received message (only in Prime v1.3)
uint32_t atpl230_t::rxBadLen |
(r) Bad len in message (too short - too long)
Referenced by phy_rx_frame_cb().
uint8_t atpl230_t::rxHdrRcv |
(r) Flag to indicate if header has already been received
Referenced by phy_rx_frame_cb().
uint8_t atpl230_t::rxIdBuff |
(r) Buffer identifier of received message
Referenced by _init_phy_layer(), and phy_rx_frame_cb().
uint8_t atpl230_t::rxMode |
(w/r) Mode PRIME v1.3 or PRIME v1.4
Referenced by phy_rx_frame_cb().
uint16_t atpl230_t::rxPayloadLen |
(r) RX: Payload length in bytes
Referenced by phy_rx_frame_cb().
uint16_t atpl230_t::rxPayloadLenSym |
(r) RX: Payload length in OFDM symbols
Referenced by phy_rx_frame_cb().
uint8_t atpl230_t::rxQRMode |
(w/r) Flag to enable / disable Rx Quality Report Mode
Referenced by _init_phy_layer(), and phy_rx_frame_cb().
uint8_t atpl230_t::rxScheme |
(r) Modulation Scheme of last received message
Referenced by phy_rx_frame_cb().
uint32_t atpl230_t::rxTotal |
(r) Received correctly messages count
Referenced by phy_rx_frame_cb().
uint32_t atpl230_t::rxTotalBytes |
(r) Received bytes count
Referenced by phy_rx_frame_cb().
uint32_t atpl230_t::rxTotalErrors |
(r) Reception errors count
Referenced by phy_rx_frame_cb().
uint32_t atpl230_t::txBadBusyChannel |
(r) Transmission failure owing to busy channel
Referenced by phy_tx_frame_result_cb().
uint32_t atpl230_t::txBadBusyTx |
(r) Already in transmission
Referenced by phy_tx_frame(), and phy_tx_frame_result_cb().
uint32_t atpl230_t::txBadFormat |
(r) Message to transmit in bad format
Referenced by phy_tx_frame(), and phy_tx_frame_result_cb().
uint32_t atpl230_t::txBadLen |
(r) Bad len in message (too short - too long)
Referenced by phy_tx_frame(), and phy_tx_frame_result_cb().
uint8_t atpl230_t::txDisableRx |
(w/r) Flag to enable / disable reception at transmission start
Referenced by phy_tx_frame().
uint8_t atpl230_t::txIdBuff |
(w/r) Buffer identifier of transmitted message
Referenced by _init_phy_layer(), and phy_tx_frame().
uint8_t atpl230_t::txLevel |
(w/r) Level parameter of last transmitted message
Referenced by phy_tx_frame().
uint8_t atpl230_t::txMode |
(w/r) Mode PRIME v1.3 or PRIME v1.4
Referenced by phy_tx_frame().
uint16_t atpl230_t::txPayloadLenSym |
(r) TX: Payload length in OFDM symbols
Referenced by phy_tx_frame().
uint8_t atpl230_t::txQRMode |
(w/r) Flag to enable / disable Tx Quality Report Mode
Referenced by _init_phy_layer(), and phy_tx_frame_result_cb().
uint8_t atpl230_t::txScheme |
(w/r) Modulation scheme of last transmitted message
Referenced by phy_tx_frame().
uint32_t atpl230_t::txTdelay |
(w/r) Delay for transmission in 10's of us
Referenced by phy_tx_frame().
uint32_t atpl230_t::txTimeout |
(r) Timeout error in transmission
Referenced by phy_tx_frame_result_cb().
uint32_t atpl230_t::txTotal |
(r) Transmitted correctly messages count
Referenced by phy_tx_frame_result_cb().
uint32_t atpl230_t::txTotalBytes |
(r) Transmitted bytes count
Referenced by phy_tx_frame_result_cb().
uint32_t atpl230_t::txTotalErrors |
(r) Transmission errors count
Referenced by phy_tx_frame_result_cb().
uint32_t atpl230_t::version |
(r) Version number
Referenced by _init_phy_layer().