Structure to hold ethernet interface parameters.
Structure to hold Ethernet interface parameters. Structure is to be defined and have its attributes set, based on the application's functionality before a call is made to initialize the wi-fi operations by calling the m2m_wifi_init function. Part of the wi-fi configuration structure tstrWifiInitParam. Applications shouldn't need to define this structure, if the bypass mode is not defined.
Structure is to be defined and have its attributes set,based on the application's functiality before a call is made to the initialize the wi-fi operations by calling the @ref m2m_wifi_init function. Part of the wi-fi configuration structure @ref tstrWifiInitParam.
#include <m2m_wifi.h>
Data Fields | |
uint8 | __PAD8__ |
uint8 * | au8ethRcvBuf |
tpfAppEthCb | pfAppEthCb |
tpfAppWifiCb | pfAppWifiCb |
uint16 | u16ethRcvBufSize |
uint8 | u8EthernetEnable |
uint8 tstrEthInitParam::__PAD8__ |
Padding
tpfAppWifiCb tstrEthInitParam::pfAppWifiCb |
Callback for wifi notifications.
Referenced by m2m_ble_wifi_init().
uint8 tstrEthInitParam::u8EthernetEnable |
Enable Ethernet mode flag
Referenced by m2m_wifi_init_start(), and winc_fill_callback_info().