#include <atpl230.h>
Data Fields | |
uint8_t | cinr_avg |
Average CNIR (Carrier to Interference + Noise ratio) (valid only when rxQRMode is enable) More... | |
uint8_t * | data_buf |
Pointer to data buffer. More... | |
uint16_t | data_len |
Length of the data buffer. More... | |
uint16_t | evm_header |
Error Vector Magnitude for header (valid only when rxQRMode is enable) More... | |
uint32_t | evm_header_acum |
Accumulated Error Vector Magnitude for header (valid only when rxQRMode is enable) More... | |
uint16_t | evm_payload |
Error Vector Magnitude for payload (valid only when rxQRMode is enable) More... | |
uint32_t | evm_payload_acum |
Accumulated Error Vector Magnitude for payload (valid only when rxQRMode is enable) More... | |
uint8_t | header_type |
Header Type of the last received message. More... | |
uint8_t | mode |
Mode PRIME v1.3, PRIME PLUS or Noise Capture. More... | |
uint8_t | noise_result |
Noise result in case of noise capture mode. More... | |
uint8_t | rssi_avg |
Average RSSI (Received Signal Strength Indication) (valid only when rxQRMode is enable) More... | |
uint32_t | rx_time |
Reception time in 10us. More... | |
uint8_t | scheme |
Modulation scheme of the last received message. More... | |
uint8_t | uc_buff_id |
Buffer identifier. More... | |
uint8_t xPhyMsgRx_t::cinr_avg |
Average CNIR (Carrier to Interference + Noise ratio) (valid only when rxQRMode is enable)
Referenced by _serial_if_get_rx_task(), phy_rx_frame_cb(), and sniffer_if_process().
uint8_t* xPhyMsgRx_t::data_buf |
Pointer to data buffer.
Referenced by _serial_if_get_rx_task(), pal_data_indication(), pal_get_rx(), phy_rx_frame_cb(), prvGetRxTask(), and sniffer_if_process().
uint16_t xPhyMsgRx_t::data_len |
Length of the data buffer.
Referenced by _serial_if_get_rx_task(), pal_data_indication(), pal_data_indication_ex(), pal_get_rx(), phy_rx_frame_cb(), prvGetRxTask(), and sniffer_if_process().
uint16_t xPhyMsgRx_t::evm_header |
Error Vector Magnitude for header (valid only when rxQRMode is enable)
Referenced by _serial_if_get_rx_task(), and phy_rx_frame_cb().
uint32_t xPhyMsgRx_t::evm_header_acum |
Accumulated Error Vector Magnitude for header (valid only when rxQRMode is enable)
Referenced by _serial_if_get_rx_task(), and phy_rx_frame_cb().
uint16_t xPhyMsgRx_t::evm_payload |
Error Vector Magnitude for payload (valid only when rxQRMode is enable)
Referenced by _serial_if_get_rx_task(), and phy_rx_frame_cb().
uint32_t xPhyMsgRx_t::evm_payload_acum |
Accumulated Error Vector Magnitude for payload (valid only when rxQRMode is enable)
Referenced by _pal_get_ex_snr(), _serial_if_get_rx_task(), and phy_rx_frame_cb().
uint8_t xPhyMsgRx_t::header_type |
Header Type of the last received message.
Referenced by _serial_if_get_rx_task(), pal_get_rx(), phy_rx_frame_cb(), and sniffer_if_process().
uint8_t xPhyMsgRx_t::mode |
Mode PRIME v1.3, PRIME PLUS or Noise Capture.
Referenced by _serial_if_get_rx_task(), phy_rx_frame_cb(), and sniffer_if_process().
uint8_t xPhyMsgRx_t::noise_result |
Noise result in case of noise capture mode.
Referenced by _serial_if_get_rx_task(), and phy_rx_frame_cb().
uint8_t xPhyMsgRx_t::rssi_avg |
Average RSSI (Received Signal Strength Indication) (valid only when rxQRMode is enable)
Referenced by _serial_if_get_rx_task(), pal_data_indication(), phy_rx_frame_cb(), and sniffer_if_process().
uint32_t xPhyMsgRx_t::rx_time |
Reception time in 10us.
Referenced by pal_data_indication(), and phy_rx_frame_cb().
uint8_t xPhyMsgRx_t::scheme |
Modulation scheme of the last received message.
Referenced by _serial_if_get_rx_task(), pal_data_indication(), phy_rx_frame_cb(), and sniffer_if_process().
uint8_t xPhyMsgRx_t::uc_buff_id |
Buffer identifier.
Referenced by _pal_get_qt(), _serial_if_get_rx_task(), phy_rx_frame_cb(), and sniffer_if_process().