Proximity Reporter Profile declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
#include "ble_manager.h"
Macros | |
#define | ADV_DATA_LEN (18) |
ADV_DATA_LEN. More... | |
#define | ADV_TYPE_LEN (0x1) |
ADV_TYPE_LEN. More... | |
#define | APP_PXP_ADV_TIMEOUT (655) |
APP_PXP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out. More... | |
#define | APP_PXP_FAST_ADV (1600) |
APP_PXP_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s). More... | |
#define | IAL_ADV_DATA_UUID_LEN (2) |
IAL_ADV_DATA_UUID_LEN the size of IAL service uuid. More... | |
#define | IAL_ADV_DATA_UUID_TYPE (0x3) |
IAL_ADV_DATA_UUID_TYPE the total sizeof IAL service uuid. More... | |
#define | LL_ADV_DATA_UUID_LEN (2) |
LL_ADV_DATA_UUID_LEN the size of LL service uuid. More... | |
#define | LL_ADV_DATA_UUID_TYPE (0x3) |
LL_ADV_DATA_UUID_TYPE the total sizeof LL service uuid. More... | |
#define | PATHLOSS |
#define | PATHLOSS_VALUE 1 |
PATHLOSS which defines if the user wants pathloss functionality. More... | |
#define | PXP_ADV_DATA_NAME_DATA ("ATMEL-PXP") |
#define | PXP_ADV_DATA_NAME_LEN (9) |
PXP_ADV_DATA_NAME_LEN the length of the device name. More... | |
#define | PXP_ADV_DATA_NAME_TYPE (0x9) |
PXP_ADV_DATA_NAME_TYPE the gap ad data type. More... | |
#define | SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data More... | |
#define | TXP_ADV_DATA_UUID_LEN (2) |
TXP_ADV_DATA_UUID_LEN the size of TXP service uuid. More... | |
#define | TXP_ADV_DATA_UUID_TYPE (0x3) |
TXP_ADV_DATA_UUID_TYPE the total sizeof TXP service uuid. More... | |
Typedefs | |
typedef void(* | reporter_callback_t )(uint8_t) |
typedef void(* | reporter_state_callback_t )(bool) |
Functions | |
void | pxp_reporter_adv (void) |
sets the advertisement data and starts advertisement More... | |
at_ble_status_t | pxp_reporter_char_changed_handler (void *params) |
character changed handler More... | |
at_ble_status_t | pxp_reporter_connected_state_handler (void *params) |
connection state handler More... | |
at_ble_status_t | pxp_reporter_disconnect_event_handler (void *params) |
disconnection event handler More... | |
void | pxp_reporter_init (void *param) |
Initialize the profile, includes all initializations and start up routines of the profiles. More... | |
at_ble_status_t | pxp_service_define (void) |
profile services definition to the attribute data base More... | |
void | pxp_service_init (void) |
Initialize the services of the profile. More... | |
void | register_linkloss_handler (reporter_callback_t linkloss_fn) |
function which register the application alerting function for linkloss to the profile More... | |
void | register_pathloss_handler (reporter_callback_t pathloss_fn) |
function which register the application alerting function for pathloss to the profile More... | |
void | register_state_handler (reporter_state_callback_t state_fn) |
function which register the application state call back handler More... | |
#define ADV_DATA_LEN (18) |
ADV_DATA_LEN.
#define ADV_TYPE_LEN (0x1) |
ADV_TYPE_LEN.
#define APP_PXP_ADV_TIMEOUT (655) |
APP_PXP_ADV_TIMEOUT Advertising time-out between 0x0001 and 0x028F in seconds, 0x0000 disables time-out.
Referenced by pxp_disconnect_event_handler(), pxp_reporter_adv(), and pxp_reporter_disconnect_event_handler().
#define APP_PXP_FAST_ADV (1600) |
APP_PXP_FAST_ADV between 0x0020 and 0x4000 in 0.625 ms units (20ms to 10.24s).
Referenced by pxp_disconnect_event_handler(), pxp_reporter_adv(), and pxp_reporter_disconnect_event_handler().
#define IAL_ADV_DATA_UUID_LEN (2) |
IAL_ADV_DATA_UUID_LEN the size of IAL service uuid.
Referenced by pxp_reporter_adv().
#define IAL_ADV_DATA_UUID_TYPE (0x3) |
IAL_ADV_DATA_UUID_TYPE the total sizeof IAL service uuid.
#define LL_ADV_DATA_UUID_LEN (2) |
LL_ADV_DATA_UUID_LEN the size of LL service uuid.
Referenced by pxp_reporter_adv().
#define LL_ADV_DATA_UUID_TYPE (0x3) |
LL_ADV_DATA_UUID_TYPE the total sizeof LL service uuid.
Referenced by pxp_reporter_adv().
#define PATHLOSS |
#define PATHLOSS_VALUE 1 |
PATHLOSS which defines if the user wants pathloss functionality.
#define PXP_ADV_DATA_NAME_DATA ("ATMEL-PXP") |
Referenced by pxp_reporter_adv().
#define PXP_ADV_DATA_NAME_LEN (9) |
PXP_ADV_DATA_NAME_LEN the length of the device name.
Referenced by pxp_reporter_adv().
#define PXP_ADV_DATA_NAME_TYPE (0x9) |
PXP_ADV_DATA_NAME_TYPE the gap ad data type.
Referenced by pxp_reporter_adv().
#define SCAN_RESP_LEN (10) |
scan_resp_len is the length of the scan response data
#define TXP_ADV_DATA_UUID_LEN (2) |
TXP_ADV_DATA_UUID_LEN the size of TXP service uuid.
Referenced by pxp_reporter_adv().
#define TXP_ADV_DATA_UUID_TYPE (0x3) |
TXP_ADV_DATA_UUID_TYPE the total sizeof TXP service uuid.
typedef void(* reporter_callback_t)(uint8_t) |
typedef void(* reporter_state_callback_t)(bool) |
void pxp_reporter_adv | ( | void | ) |
sets the advertisement data and starts advertisement
[in] | void |
sets the advertisement data and starts advertisement
at_ble_status_t pxp_reporter_char_changed_handler | ( | void * | params | ) |
character changed handler
[in] | at_ble_characteristic_changed_t | which includes handle,new value |
character changed handler
References AT_BLE_SUCCESS, ias_set_alert_value(), INVALID_IAS_PARAM, INVALID_LLS_PARAM, linkloss_current_alert_level, lls_set_alert_value(), pathloss_alert_value, and pathloss_cb.
at_ble_status_t pxp_reporter_connected_state_handler | ( | void * | params | ) |
connection state handler
[in] | at_ble_connected_t | which includes the connection parameters like handle |
connection state handler
References ALL_UNUSED, at_ble_characteristic_value_get(), AT_BLE_SUCCESS, connected_cb, DBG_LOG, linkloss_current_alert_level, pathloss_alert_value, and status.
at_ble_status_t pxp_reporter_disconnect_event_handler | ( | void * | params | ) |
disconnection event handler
[in] | at_ble_disconencted_t | which includes the connection parameters like handle,reason for disconnection |
disconnection event handler
References ALL_UNUSED, APP_PXP_ADV_TIMEOUT, APP_PXP_FAST_ADV, AT_BLE_ADV_FP_ANY, AT_BLE_ADV_GEN_DISCOVERABLE, at_ble_adv_start(), AT_BLE_ADV_TYPE_UNDIRECTED, AT_BLE_SUCCESS, DBG_LOG, linkloss_cb, linkloss_current_alert_level, and NULL.
void pxp_reporter_init | ( | void * | param | ) |
Initialize the profile, includes all initializations and start up routines of the profiles.
[in] | void |
Initialize the profile, includes all initializations and start up routines of the profiles.
at_ble_status_t pxp_service_define | ( | void | ) |
profile services definition to the attribute data base
[in] | void |
profile services definition to the attribute data base
void pxp_service_init | ( | void | ) |
Initialize the services of the profile.
[in] | void |
Initialize the services of the profile.
Initializing the mandatory linkloss service of proximity reporter
Initializing the optional services for pathloss feature of proximity reporter
Initializing the mandatory linkloss service of proximity reporter
Initializing the optional services for pathloss feature of proximity reporter
void register_linkloss_handler | ( | reporter_callback_t | linkloss_fn | ) |
function which register the application alerting function for linkloss to the profile
[in] | call | back function of the application for linkloss |
function which register the application alerting function for linkloss to the profile
void register_pathloss_handler | ( | reporter_callback_t | pathloss_fn | ) |
function which register the application alerting function for pathloss to the profile
[in] | call | back function of the application for pathloss |
function which register the application alerting function for pathloss to the profile
void register_state_handler | ( | reporter_state_callback_t | state_fn | ) |
function which register the application state call back handler
[in] | call | back function of the application for connection state |
References connected_cb.
Referenced by main().