Functions | |
int | MQTTDeserialize_unsuback (unsigned short *packetid, unsigned char *buf, int buflen) |
Deserializes the supplied (wire) buffer into unsuback data. More... | |
int | MQTTSerialize_unsubscribe (unsigned char *buf, int buflen, unsigned char dup, unsigned short packetid, int count, MQTTString topicFilters[]) |
Serializes the supplied unsubscribe data into the supplied buffer, ready for sending. More... | |
int | MQTTSerialize_unsubscribeLength (int count, MQTTString topicFilters[]) |
Determines the length of the MQTT unsubscribe packet that would be produced using the supplied parameters. More... | |
int MQTTDeserialize_unsuback | ( | unsigned short * | packetid, |
unsigned char * | buf, | ||
int | buflen | ||
) |
Deserializes the supplied (wire) buffer into unsuback data.
packetid | returned integer - the MQTT packet identifier |
buf | the raw buffer data, of the correct length determined by the remaining length field |
buflen | the length in bytes of the data in the supplied buffer |
References FUNC_ENTRY, FUNC_EXIT_RC, MQTTDeserialize_ack(), and UNSUBACK.
Referenced by MQTTFormat_toClientString(), and MQTTUnsubscribe().
int MQTTSerialize_unsubscribe | ( | unsigned char * | buf, |
int | buflen, | ||
unsigned char | dup, | ||
unsigned short | packetid, | ||
int | count, | ||
MQTTString | topicFilters[] | ||
) |
Serializes the supplied unsubscribe data into the supplied buffer, ready for sending.
buf | the raw buffer data, of the correct length determined by the remaining length field |
buflen | the length in bytes of the data in the supplied buffer |
dup | integer - the MQTT dup flag |
packetid | integer - the MQTT packet identifier |
count | - number of members in the topicFilters array |
topicFilters | - array of topic filter names |
References MQTTHeader::bits, buf, MQTTHeader::byte, count, MQTTHeader::dup, FUNC_ENTRY, FUNC_EXIT_RC, header, i, MQTTPACKET_BUFFER_TOO_SHORT, MQTTPacket_encode(), MQTTPacket_len(), MQTTSerialize_unsubscribeLength(), ptr, MQTTHeader::qos, MQTTHeader::type, UNSUBSCRIBE, writeChar(), writeInt(), and writeMQTTString().
Referenced by MQTTUnsubscribe().
int MQTTSerialize_unsubscribeLength | ( | int | count, |
MQTTString | topicFilters[] | ||
) |
Determines the length of the MQTT unsubscribe packet that would be produced using the supplied parameters.
count | the number of topic filter strings in topicFilters |
topicFilters | the array of topic filter strings to be used in the publish |
References count, i, len, and MQTTstrlen().
Referenced by MQTTSerialize_unsubscribe().