AT30TSE75X driver.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
|
void | at30tse_eeprom_read (uint8_t *data, uint8_t length, uint8_t word_addr, uint8_t page) |
| Reads data from the EEPROM. More...
|
|
void | at30tse_eeprom_write (uint8_t *data, uint8_t length, uint8_t word_addr, uint8_t page) |
| Writes the EEPROM with data provided. More...
|
|
void | at30tse_init (void) |
| Configures the TWHIS master to be used with the AT30TSE75X device. More...
|
|
uint16_t | at30tse_read_register (uint8_t reg, uint8_t reg_type, uint8_t reg_size) |
| Reads the value from the register reg. More...
|
|
double | at30tse_read_temperature () |
| Reads the temperature value. More...
|
|
void | at30tse_set_register_pointer (uint8_t reg, uint8_t reg_type) |
| Sets the register pointer with specified reg value. More...
|
|
void | at30tse_write_config_register (uint16_t value) |
| Writes the configuration register reg with the value passed. More...
|
|
void | at30tse_write_register (uint8_t reg, uint8_t reg_type, uint8_t reg_size, uint16_t reg_value) |
| Writes the specified register reg with the reg_value passed. More...
|
|