Declaration of main function used by HID generic example.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_generic_disable (void) |
Called by HID interface Callback running when USB Host disable generic interface. More... | |
bool | main_generic_enable (void) |
Called by HID interface Callback running when USB Host enable generic interface. More... | |
void | main_hid_set_feature (uint8_t *report) |
Called by UDI HID generic when USB Host send a feature request. More... | |
void | main_remotewakeup_disable (void) |
Called by UDC when USB Host request to disable remote wakeup. More... | |
void | main_remotewakeup_enable (void) |
Called by UDC when USB Host request to enable remote wakeup. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void main_generic_disable | ( | void | ) |
Called by HID interface Callback running when USB Host disable generic interface.
References main_b_generic_enable.
bool main_generic_enable | ( | void | ) |
Called by HID interface Callback running when USB Host enable generic interface.
true | if generic startup is ok |
References main_b_generic_enable.
void main_hid_set_feature | ( | uint8_t * | report | ) |
Called by UDI HID generic when USB Host send a feature request.
References udc_stop(), and ui_powerdown().
void main_remotewakeup_disable | ( | void | ) |
Called by UDC when USB Host request to disable remote wakeup.
References ui_wakeup_disable().
void main_remotewakeup_enable | ( | void | ) |
Called by UDC when USB Host request to enable remote wakeup.
References ui_wakeup_enable().
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Called by UDD when the USB line exit of suspend state.
References main_b_suspend_event, and ui_wakeup().
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Called when a start of frame is received on USB line.
References main_b_cdc_enable, main_b_generic_enable, main_b_kbd_enable, main_b_keyboard_enable, main_b_mouse_enable, main_b_msc_enable, main_b_phdc_enable, main_b_sof_event, main_b_vendor_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
References main_b_resume_event, and ui_powerdown().