Declaration of main function used by MSC example.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_msc_notify_trans (void) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called. More... | |
void | main_resume_action (void) |
Called by UDD when the USB line exit of suspend state. More... | |
void | main_sof_action (void) |
Called when a start of frame is received on USB line. More... | |
void | main_suspend_action (void) |
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state. More... | |
void | memories_initialization (void) |
Initialize the memories used by examples. More... | |
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
void main_msc_notify_trans | ( | void | ) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called.
References pdFALSE, and xSemaphoreGiveFromISR.
void main_resume_action | ( | void | ) |
Called by UDD when the USB line exit of suspend state.
Called by UDD when the USB line exit of suspend state.
void main_sof_action | ( | void | ) |
Called when a start of frame is received on USB line.
Called when a start of frame is received on USB line.
void main_suspend_action | ( | void | ) |
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
void memories_initialization | ( | void | ) |
Initialize the memories used by examples.