White-list structure.
#include <at_ble_api.h>
Data Fields | |
uint8_t | addrCount |
Count of device addresses in array, up to AT_BLE_GAP_WHITELIST_ADDR_MAX_COUNT. More... | |
uint8_t | irkCount |
Count of IRKs in array, up to AT_BLE_GAP_WHITELIST_IRK_MAX_COUNT. More... | |
at_ble_addr_t ** | ppAddrs |
Pointer to array of device address pointers, pointing to addresses to be used in white-list. More... | |
at_ble_gap_irk_t ** | ppIrks |
Pointer to array of Identity Resolving Key (IRK) pointers, each pointing to an IRK in the white-list. More... | |
uint8_t at_ble_gap_whitelist_t::addrCount |
Count of device addresses in array, up to AT_BLE_GAP_WHITELIST_ADDR_MAX_COUNT.
uint8_t at_ble_gap_whitelist_t::irkCount |
Count of IRKs in array, up to AT_BLE_GAP_WHITELIST_IRK_MAX_COUNT.
at_ble_addr_t** at_ble_gap_whitelist_t::ppAddrs |
Pointer to array of device address pointers, pointing to addresses to be used in white-list.
NULL if none are given.
at_ble_gap_irk_t** at_ble_gap_whitelist_t::ppIrks |
Pointer to array of Identity Resolving Key (IRK) pointers, each pointing to an IRK in the white-list.
NULL if none are given.