Microchip® Advanced Software Framework

mem Struct Reference

The heap is made up as a list of structs of this type.

This does not have to be aligned since for getting its size, we only use the macro SIZEOF_STRUCT_MEM, which automatically alignes.

Data Fields

mem_size_t next
 index (-> ram[next]) of the next struct More...
 
mem_size_t prev
 index (-> ram[prev]) of the previous struct More...
 
u8_t used
 1: this area is used; 0: this area is unused More...
 

mem_size_t mem::next

index (-> ram[next]) of the next struct

Referenced by mem_free(), mem_init(), mem_malloc(), mem_trim(), and plug_holes().

mem_size_t mem::prev

index (-> ram[prev]) of the previous struct

Referenced by mem_init(), mem_malloc(), mem_trim(), and plug_holes().

u8_t mem::used

1: this area is used; 0: this area is unused

Referenced by mem_free(), mem_init(), mem_malloc(), mem_trim(), and plug_holes().