Microchip® Advanced Software Framework

tstrM2MBLEInfo Struct Reference

BLE Result.

This struct is passed to the application in response to a BLE request. If the BLE session is completed successfully, the
structure will have Non-ZERO authentication type. If the BLE Session fails (due to error or timeout) the authentication type
is set to ZERO.
See Also
tenuM2mSecType

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [__PADDING_tstrM2MBLEInfo_]
 
uint8 au8PSK [M2M_MAX_PSK_LEN]
 
uint8 au8SSID [M2M_MAX_SSID_LEN]
 
uint8 u8AuthType
 
uint8 u8Ch
 

uint8 tstrM2MBLEInfo::__PAD__[__PADDING_tstrM2MBLEInfo_]
uint8 tstrM2MBLEInfo::au8PSK[M2M_MAX_PSK_LEN]

PSK for the network obtained from BLE provisioning.

uint8 tstrM2MBLEInfo::au8SSID[M2M_MAX_SSID_LEN]

SSID obtained from BLE provisioning.

uint8 tstrM2MBLEInfo::u8AuthType

Network authentication type.

uint8 tstrM2MBLEInfo::u8Ch

RF Channel for the AP.