This struct contains the static IP configuration.
IP configuration (static/DHCP). The same structure is used for DCHP callback as well as static IP configuration.
#include <m2m_types.h>
Data Fields | |
uint32 | u32AlternateDNS |
uint32 | u32DhcpLeaseTime |
uint32 | u32DNS |
uint32 | u32Gateway |
uint32 | u32StaticIP |
uint32 | u32SubnetMask |
uint32 tstrM2MIPConfig::u32AlternateDNS |
IP for the secondary DNS server (if any). Must set to zero if not provided in static IP configuration from the application.
uint32 tstrM2MIPConfig::u32DhcpLeaseTime |
DHCP Lease Time in sec. This field is is ignored in static IP configuration.
uint32 tstrM2MIPConfig::u32DNS |
IP for the DNS server.
Referenced by m2m_wifi_set_static_ip().
uint32 tstrM2MIPConfig::u32Gateway |
IP of the default internet gateway.
Referenced by m2m_wifi_set_static_ip().
uint32 tstrM2MIPConfig::u32StaticIP |
The static IP assigned to the device.
If DHCP callback, this is the IP address obtained from the DHCP. In static IP config, this is the assigned to the device from the application.
Referenced by app_wifi_handle_event(), iperf_wifi_cb(), and m2m_wifi_set_static_ip().
uint32 tstrM2MIPConfig::u32SubnetMask |
Subnet mask for the local area network.
Referenced by m2m_wifi_set_static_ip().