Microchip® Advanced Software Framework

tstrM2MProvisionModeConfig Struct Reference

This struct contains the provisioning mode configuration.

M2M Provisioning Mode Configuration.

#include <m2m_types.h>

Data Fields

uint8 __PAD24__ [3]
 
char acHttpServerDomainName [64]
 
tstrM2MAPConfig strApConfig
 
tstrM2MAPConfigExt strApConfigExt
 
uint8 u8EnableRedirect
 

uint8 tstrM2MProvisionModeConfig::__PAD24__
char tstrM2MProvisionModeConfig::acHttpServerDomainName

The device domain name for HTTP provisioning.

Referenced by m2m_wifi_start_provision_mode_ext().

tstrM2MAPConfig tstrM2MProvisionModeConfig::strApConfig

Configuration parameters for the WiFi AP.

Referenced by m2m_wifi_start_provision_mode_ext().

tstrM2MAPConfigExt tstrM2MProvisionModeConfig::strApConfigExt

Additional configuration parameters for the WiFi AP.

Referenced by m2m_wifi_start_provision_mode_ext().

uint8 tstrM2MProvisionModeConfig::u8EnableRedirect

A flag to enable/disable HTTP redirect feature for the HTTP provisioning server. If the redirect is enabled, all HTTP traffic (http://URL) from the device associated with WINC AP will be redirected to the HTTP Provisioning web page.

  • 0 : Disable HTTP Redirect.
  • 1 : Enable HTTP Redirect.

A flag to enable/disable HTTP redirect feature for the HTTP Provisioning server. If the Redirect is enabled, all HTTP traffic (http://URL) from the device associated with WINC AP will be redirected to the HTTP Provisioning Web page.

  • 0 : Disable HTTP Redirect.
  • 1 : Enable HTTP Redirect.

Referenced by m2m_wifi_start_provision_mode_ext().