Microchip® Advanced Software Framework

tstrM2MScan Struct Reference

This struct contains the Wi-Fi scan request.

Wi-Fi Scan Request.

See Also
tenuM2mScanCh
tenuM2mScanCh tstrM2MScanOption

#include <m2m_types.h>

Data Fields

uint8 __PAD24__ [3]
 
uint8 __RSVD8__ [1]
 
uint16 u16PassiveScanTime
 
uint8 u8ChNum
 

uint8 tstrM2MScan::__PAD24__[3]

Padding bytes for forcing 4-byte alignment

uint8 tstrM2MScan::__RSVD8__[1]

Reserved for future use.

uint16 tstrM2MScan::u16PassiveScanTime

The length of each scan slot in milliseconds. Refers to passive scan only. The device listens for beacons during this time. Valid settings are in the range 10<=PassiveScanTime<=1200. Default setting is M2M_SCAN_DEFAULT_PASSIVE_SLOT_TIME.

Referenced by m2m_wifi_request_scan_passive().

uint8 tstrM2MScan::u8ChNum

The Wi-Fi RF channel number

The Wi-Fi RF Channel number

Referenced by m2m_wifi_request_scan(), m2m_wifi_request_scan_passive(), and m2m_wifi_request_scan_ssid_list().