Microchip® Advanced Software Framework

tstrM2mWifiApId Struct Reference

Specify an access point (by SSID)

#include <m2m_types.h>

Data Fields

uint8 __PAD__ [3]
 
uint8 au8SSID [M2M_MAX_SSID_LEN]
 

uint8 tstrM2mWifiApId::__PAD__

Padding bytes for forcing 4-byte alignment

uint8 tstrM2mWifiApId::au8SSID

SSID of the desired AP, prefixed by length byte. First byte 0xFF used to mean all access points.

Referenced by m2m_wifi_delete_sc().