Host File OTA Information.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD8__ |
uint8 | pFileBuf [MAX_FILE_READ_STEP] |
uint16 | u16FileBlockSz |
uint8 | u8OtaFileReadStatus |
uint8 tstrOtaHostFileReadStatusResp::__PAD8__ |
Padding byte for forcing 4-byte alignment
uint8 tstrOtaHostFileReadStatusResp::pFileBuf[MAX_FILE_READ_STEP] |
Pointer to the temporary buffer containing the data just read. Max size is MAX_FILE_READ_STEP
Referenced by m2m_ota_cb().
uint16 tstrOtaHostFileReadStatusResp::u16FileBlockSz |
Reports the size of the block of data read via HIF. Valid if u8OtaFileReadStatus=OTA_STATUS_SUCCESS .
Referenced by m2m_ota_cb().
uint8 tstrOtaHostFileReadStatusResp::u8OtaFileReadStatus |
The status of the File Read operation. See tenuOtaUpdateStatus.
Referenced by m2m_ota_cb().