Microchip® Advanced Software Framework

usb_phdc_fnctext_desc_t Struct Reference

PHDC Function Extension Descriptor Note: The wDevSpecializations fields must follow this struct.

#include <usb_protocol_phdc.h>

Data Fields

uint8_t bDescriptorType
 PHDC descriptor type. More...
 
uint8_t bLength
 Size of this descriptor in bytes. More...
 
uint8_t bNumDevSpecs
 Number of wDevSpecializations below. More...
 
uint8_t bReserved
 Reserved for future use, must be zero. More...
 

uint8_t usb_phdc_fnctext_desc_t::bDescriptorType

PHDC descriptor type.

uint8_t usb_phdc_fnctext_desc_t::bLength

Size of this descriptor in bytes.

uint8_t usb_phdc_fnctext_desc_t::bNumDevSpecs

Number of wDevSpecializations below.

uint8_t usb_phdc_fnctext_desc_t::bReserved

Reserved for future use, must be zero.