Microchip® Advanced Software Framework

usb_phdc_qos_desc_t Struct Reference

PHDC QoS Descriptor.

#include <usb_protocol_phdc.h>

Data Fields

uint8_t bDescriptorType
 PHDC descriptor type. More...
 
uint8_t bLength
 Size of this descriptor in bytes. More...
 
uint8_t bmLatencyReliability
 If bQoSEncodingVersion = 01h,. More...
 
uint8_t bQoSEncodingVersion
 01h = version 1 QoS information encoding More...
 

uint8_t usb_phdc_qos_desc_t::bDescriptorType

PHDC descriptor type.

uint8_t usb_phdc_qos_desc_t::bLength

Size of this descriptor in bytes.

uint8_t usb_phdc_qos_desc_t::bmLatencyReliability

If bQoSEncodingVersion = 01h,.

then this bitmap refers to the latency/reliability bin for the QoS data

uint8_t usb_phdc_qos_desc_t::bQoSEncodingVersion

01h = version 1 QoS information encoding