Microchip® Advanced Software Framework

winc3400/wifi_drv/driver/source/m2m_ssl.c File Reference

WINC SSL Interface.

Copyright (c) 2017-2021 Microchip Technology Inc. and its subsidiaries.

#include "driver/include/m2m_ssl.h"
#include "driver/source/m2m_hif.h"
#include "driver/source/nmasic.h"

Macros

#define CHUNKHDRSZ   (sizeof(tstrTlsSrvChunkHdr))
 
#define CHUNKSZ   (TXLIMIT - 256)
 
#define TXLIMIT   (256 * 6)
 

Functions

static void m2m_ssl_cb (uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr)
 Internal SSL callback function. More...
 
NMI_API void m2m_ssl_ecc_process_done (void)
 Allow SSL driver to tidy up after application has finished processing ECC message. More...
 
NMI_API sint8 m2m_ssl_handshake_rsp (tstrEccReqInfo *strECCResp, uint8 *pu8RspDataBuff, uint16 u16RspDataSz)
 Sends ECC responses to the WINC. More...
 
NMI_API sint8 m2m_ssl_init (tpfAppSSLCb pfAppSSLCb)
 Initializes the SSL layer. More...
 
NMI_API sint8 m2m_ssl_retrieve_cert (uint16 *pu16Curve, uint8 *pu8Value, uint8 *pu8Sig, tstrECPoint *pstrKey)
 Retrieve the next set of information from the WINC for ECDSA verification. More...
 
NMI_API sint8 m2m_ssl_retrieve_hash (uint8 *pu8Value, uint16 u16ValueSz)
 Retrieve the value from the WINC for ECDSA signing. More...
 
NMI_API sint8 m2m_ssl_retrieve_next_for_verifying (tenuEcNamedCurve *penuCurve, uint8 *pu8Value, uint16 *pu16ValueSz, uint8 *pu8Sig, uint16 *pu16SigSz, tstrECPoint *pstrKey)
 Retrieve the next set of information from the WINC for ECDSA verification. More...
 
NMI_API sint8 m2m_ssl_send_certs_to_winc (uint8 *pu8Buffer, uint32 u32BufferSz)
 Sends certificates to the WINC. More...
 
NMI_API sint8 m2m_ssl_set_active_ciphersuites (uint32 u32SslCsBMP)
 Sets the active ciphersuites. More...
 
NMI_API void m2m_ssl_stop_processing_certs (void)
 Allow SSL driver to tidy up in case application does not read all available certificates. More...
 
NMI_API void m2m_ssl_stop_retrieving (void)
 Allow SSL driver to tidy up when the application chooses not to retrieve all available information. More...
 

Variables

static tenuTlsFlashStatus genuStatus = TLS_FLASH_ERR_UNKNOWN
 
static tpfAppSSLCb gpfAppSSLCb = NULL
 
static uint32 gu32HIFAddr = 0
 

#define CHUNKHDRSZ   (sizeof(tstrTlsSrvChunkHdr))
#define CHUNKSZ   (TXLIMIT - 256)
#define TXLIMIT   (256 * 6)

void m2m_ssl_cb ( uint8  u8OpCode,
uint16  u16DataSize,
uint32  u32Addr 
)
static

Referenced by m2m_ssl_cb(), and m2m_ssl_init().

tpfAppSSLCb gpfAppSSLCb = NULL
static

Referenced by m2m_ssl_cb(), and m2m_ssl_init().